Part Number: LM5156
Hello,
I'm evaluating to make isolated dc/dc converter with following characteristics:
MANDATORY:
Vin = 24V
Vout = variable from 0 (near 0) to 100V
Load will be RC, 7-8W
It have to be isolated
IF POSSIBLE:
Vin = 24 or 48Vdc
Vout1 = variable from 0 (near 0) to 100V
Vout2 = 12Vdc (0,5W)
There is a design that I can use as reference?
Thank you