Other Parts Discussed in Thread: TCA9546A, SN74LV4052A, TMUX1309, TMUX1574, SN74CBT3257C, SN74CBTLV3257, TMUX1121, TMUX1122, TMUX1112, TMUX1111, TCA9548A
Hello,
I have two bus masters and one slave device so I need a demux to allow either of them to talk to the slave. I can either use 4 such parts or if you have a dual or quad I can lower the IC count. I would also like to connect one of the bus masters to TCA9546APWR and one of the outputs of that to the demux and then to slave
Bus master --> TCA9546APWR --> 2 : 1 demux --> I2C Slave
Can you suggest a part?
Thanks,
Divakar