If the R4 and R5 must be 60.4 kOhm, and why? Can I change them to 80 kOhm?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
R4 and R5 do not necessarily have to be 60.4kOhm - in fact, they are different values in the non-tracking application further down in the datasheet:

80k resistors are suitable for this device as well.
Thanks,
Kadeem
Hello,
There is no issue to choose 80K. The 60.4K may be selected for resistor tolerance.
Regards, Mahmoud