Part Number: UCC28220
Hi.
I am developing an interleaved 3 switch forward convertor using IC UCC28220
* Topology: 3 switch forward
* Input: 380VDC(PFC Output)
* Ouput: 12VDC, 84A, 1000W
The problem is the overcurrent protection circuit.
The circuit design used a current transformer. Also,UCC28220 is controlled from the secondary side.
Under overcurrent conditions, the output voltage gradually decreases. However, the load current continues to increase.
(See picture below: Vertical axis voltage / horizontal axis current)
I think that under overcurrent conditions, the UCC28220 limits the duty, so the output current continues to increase, causing the output voltage to drop.
The problem is overheating of the output circuit.
I want to design the overcurrent protection characteristic curve to be like one of the two pictures below.
Please check if my circuit design is incorrect.
Also, Please let me know if there is a way to make ocp hiccup work.
Attatchment: Schematic - 3 Switch Forward - Output 1000W (12V, 84A).pdf
Schematic - 3 Switch Forward - Output 1000W (12V, 84A).pdf