Other Parts Discussed in Thread: DRA752, PMP, BEAGLEBOARD-X15, TMDSEVM572X, DRA742
Hi,
my custom board is not booting it is stuck at SPL as shown below
U-Boot SPL 2019.01 (Mar 27 2024 - 12:04:44 +0530)
DRA752-GP ES2.0
no pinctrl state for default mode
after the above nothing happens,
iam trying to boot my custom board ,which has Am5728 ,2GB ddr, Iam using SDK linux version ti-processor-sdk-linux-am57xx-evm-06.03.00.106.iam using SD card for booting
My custom board has
PMIC
eeprom with AM5728 EVM data
1nos of ethernet interface
sata interface
sdcard interface
rtc
USB 3.0 HUB,
can some one help me about what iam missing,
should i do any changes in pinmux config or should i do something to disable it to check mmc1 which is Emmc,