Part Number: BQ25672EVM
Other Parts Discussed in Thread: BQ25672, TI-CHARGER-GUI, BQ25798
Tool/software:
Hello,
I am using the BQ25672EVM and have a question regarding the test setup.
In the EVM documentation, a battery simulator is recommended to be connected to the BAT pin of the charger IC. However, I don't have a battery simulator or DC load available. Can I connect a discharged battery pack from my lab instead, and would it work?
Here's what I've done so far:
1. Connected PS1 (5V @ 3A) to the J1 connector.
2. Connected the battery pack to the J5 connector.
3. Launched the TI-CHARGER-GUI software and selected BQ25672 as mentioned in the initial EVM documentation.
4. At step #4, when I turn on PS1 and connect the battery pack as load 1, I am unable to measure 8.55V at VSYS on the J3 connector. Instead, I measure 7.61V.
Could you please guide me on what might be missing in this setup that is preventing the correct voltage measurement?