Part Number: TPS54202
Other Parts Discussed in Thread: TPS62932, TPS62933
Tool/software:
Dear Sir,
What converter can I use to have 3 voltage outputs?
We would suggest using a single DC/DC converter for the 3 power supplies (12V, 5V and 3.3V) since components cost lower at high volume.
{Edit by Peter Miller} - Maxim is looking for a converter (integrated FET) recommendation for 3-rails from a 24V (20-25V) input:
12V @ 1.5A
5V @ 0.4A
3.3V @ 0.5A
For increased volume and inventory control, he would like a single device which can support all 3 applications, not necessarily a triple-output converter.