This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202: 24V input to 12V, 5V, and 3.3V part recommendations.

Part Number: TPS54202
Other Parts Discussed in Thread: TPS62932, TPS62933

Tool/software:

Dear Sir,

What converter can I use to have 3 voltage outputs?

We would suggest using a single DC/DC converter for the 3 power supplies (12V, 5V and 3.3V) since components cost lower at high volume. 

{Edit by Peter Miller} - Maxim is looking for a converter (integrated FET) recommendation for 3-rails from a 24V (20-25V) input:

12V @ 1.5A

5V @ 0.4A

3.3V @ 0.5A 

For increased volume and inventory control, he would like a single device which can support all 3 applications, not necessarily a triple-output converter.