Other Parts Discussed in Thread: BQ25730EVM
Tool/software:
Hello,
We've used the BQ257x family of parts in some of our other products using batteries, but I'd now like to use it with a supercapacitor instead. The features which I particularly like about this family is
- Input current limiting - Power will be sourced from a USB-C PD supply, where the current/voltage will be negotiated
- Battery (supercap) current limiting - Current going into the supercaps can be limited for a safe temp rise
- Battey (supercap) supplement mode - When the external supply is disconnected, the supercap can immediately supplement and power the system from its functional voltage range of ~6V to 10V
In my application, I want the supercap to fully charge before the VSYS load is connected, and in my testing I've been able to demonstrate my desired behavior with the following register configurations
- Charge Option 0 > EN_LDO = 0
- Charge Current Register = 1024mA
- Charge Voltage Register = 10000mV
- Input Current Limit= 3000mA
- Minimum System Voltage = 0mV
This successfully charges my supercap from 0V to 10V, after which VSYS=10V and I can use it to power my system. My question is that according to the datasheet, Minimum System Voltage = 0mV is not supposed to be valid (see image below). Can someone from TI answer whether this Min System Voltage behavior is expected? If it is not expected, can it be captured in the errata as a valid input because I would like to use it and think it would be a useful use-case? Also is there any risk of parts in the field, or planned silicon changes causing this behavior to change?
Thanks
Hale