Other Parts Discussed in Thread: UCC27301A
Tool/software:
Hi Team,
Want to know if the device can be used similar to Infineon 1EDNx550 when used as high-side driver. Can I used as same way as the circled area in the pic below?

-A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Albert,
Thank you for reaching out regarding your questions about the UCC27511A. There are a few options for a high-side driver.
The UCC27511A is a low-side driver, so provisions would need to be made to use it on the high side. This is highlighted in the following FAQ:
[FAQ] Can I use a Low Side driver as a High Side driver?
The Infineon part is listed as a high-side and low-side driver, so it can be used in either setup it appears. Another option here would be to use a single channel isolated driver such as the UCC23525.
Another option would be to use a half-bridge driver such as the UCC27301A. If only a high-side is needed, then this can be used as a high-side driver with the provisions discussed in the following FAQ:
[FAQ] How to bias the high side of a half-bridge gate driver and why
Let me know if there are any questions.
Thank you,
William Moore