Part Number: UCC2818-EP
Other Parts Discussed in Thread: UCC28180, PMP31164, UCC25640EVM-020
Tool/software:
Hi TI team
We have build a PFC board using UCC2818-EP PFC IC.
Following is our requirement
Vin :100Vrms to 134Vrms (360Hz to 800Hz)
Vout : 400V (100W)
Previously we tested UCC28180 IC using Eval board as per PMP31164 reference design following link we had discussed the problem we have faced.
Now we build a PFC board using UCC2818-EP following is the schematic and we are seeing some issues in the input current. Current loop is set to be around cutoff frequency of 20KHz and voltage loop is set to be around 68Hz. Is it a problem with Compensation? Current is peaking only on positive side of voltage and duty seems to be normal in all the cases, as i increase the load the current also starts peaking more.