Other Parts Discussed in Thread: LP5812

Tool/software:
I have a LP5012 on my board and can write and readback registers via i2c, but no matter what I set I don't seem to be able to get any output. My understanding is that from a default state (and I have tried setting the reset to defaults register) the only requirements to get a light would be to enable bit6 of register 0 and pull the EN pin high. my EN pin is tied to VCC (5V). When I write and readback register 0 it changes from an initial 0x00 to 0x40 (seems correct)
I have tried setting all the brightness to 0x80 to try and get some output, I tried changing all the setting in register 1 and 2 but never get any output.
R-iref is 4.7K ohms, but I tried bypassing it to use the internal current limit
measuring the voltage on the output pin I get with on an oscilloscope with an LED to VCC shows 3.5V but no waveform and the LED does not light (looks like about the voltage drop of the LED I guess)
my i2c pullups are 4.7K, but i2c is working anyway so that seems irrelevant
I tried replacing the IC, but no change
I have tested my LEDs themselves