Other Parts Discussed in Thread: AM2431, AM623, CC3551E, , SK-AM64B
Tool/software:
I understand that this industrial networking oriented family of sitara processors have no low power mode designed as other general purpose sitara processors have, such as AM623/625. But in our application, which requires pcie and high-speed parallel communication (could be perfectivly implemented by PRU-ICSSG) when powered by wall adapter, the system must also be kept to consume as little power as possible when powered by batteries. In this mode, the AM6411 (or AM2431) may be powered on by a BLE/WiFi processor (probably CC3551e), then stay in an active idle mode for a while and write a few mega bytes of data into pcie SSD intermittently. Both AM6411 and R52 processors could be put into stop mode (or some non-functional mode with even lower power consumption), a wait-for-interrupt cortex M4 is sufficient for this task.
I have played with the Power Estimation Tool. If everything is put into OFF state, there is still a power consumption of around 250mW. My question is, if this is the absolute minimal power consumption that can be achieved for this processor? Or, the tool is not quite accurate in this extreme case. With everyting OFF and only M4 core is waiting for interrupt, the power consumption can go even lower. We do hope it could be below 100mW to extend battery life, is this possible?