Part Number: TPS563300
Other Parts Discussed in Thread: LM317, TPS564252, TPS54531
Tool/software:
Hi,
I am facing issue of TPS563300 blowing up (burn out with smoke) as soon as 24V input is either switched ON or it is hot plugged in. Output voltage is 12V, 2A. However, when it blows up there is no output load connected and hence output current is 0. This problem was observed with this chip on multiple boards. However, after it starts there is no problem even with load of 1.7A as per my testing for hours.
I have designed power supply circuit using webbench. Below is the design output of webbench:

Also BOM generated by webbench tool:

Below is the schematic of power supply on my custom board. I have connected potential divider on EN pin so that chip starts only when input voltage increases above 19V. One capacitor on input and output are DNP (Do not populate) so as to connect more caps if required for stability. I have observed chip blow up when these capacitors were connected or not connected.

Below is the BOM of passive components in my design. Active components part nos. are as mentioned in schematics.

PCB layout was done following the guidelines given in datasheet.

Board images:


Please help me locate the issue.
Thanks,
Pradeep