I'm not sure if I'm posting this to the correct forum. None of the Application forums covers the SensorEval app so I'm trying this forum.
I'm unable to run SensorEval v1.2.1 under Windows XP 5.1 (Build 2600, SP3). The error I get is:
comdlg32.ocx is a CMDialog ActiveX Control required to run Visual Basic apps. The file was not bundled with the SensorEval installation package. Nor does is exist anywhere on my drive, unfortunately. Since TI is the application developer, I believe you're required to distribute this with builds. It's not available for download on Microsoft.com nor apparently anywhere on ti.com. There are bootleg copies on a few shady websites, however, I'm 100% unwilling to go that route. Could someone please send me the required file? Thanks.