Part Number: DS90UB933-Q1
Hi there,
I am trying to understand how the high speed data is flowing through the FPD III link in the SERDES pair. Using DS90UB933/934 pair as example.
I am assuming the differential driver is similar to the typical LVDS driver (in a high level sense ignoring details). See picture below (obtained from TI LVDS owner manual),
Q: can this be confirmed?
In differential mode, it is straightforward in that high speed current will flow from DOUT+ of serializer through the STP cable to RIN-, go through the internal 100 ohm termination (following picture below regarding the differential mode, obtained from TI FPD3 training) in the deserializer, then exit out of RIN- of deserializer and flow back to DOUT- of serializer and back to GND, thus completing the current loop.
Q: However, what is the path that the high speed current takes in the single ended coxial mode case (FIgure 30 in pg 37 of DS90UB933 datasheet)?
- Is it that high speed current flows out from DOUT+ (serializer, goes through the coaxial cable, reaches RIN+ of the deserializer), gets terminated by the 50 ohm termination, goes through to the VBIAS (which would be GND in AC) and then flow back out via GND of the deserializer, back to coaxial cable's GND, and back to the serializer?
- Why is the external 50 ohm needed for the RIN- port in this single ended case? What is its significance?
Thanks.
Shaun.