Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137
Hi,
We are developing a system with TMS570LS2135 and we need to use CAN to communicate with other systems. When we test the products, we found the CAN interface doesn't work and there is no signal output from pins of CAN high/low.
The detailed information is following:
1. The problem:
Can't send CAN message out and there is no signal can be captured from the pin of CAN Interface with a scope.
2. MCU model: TMS570LS2135 PGE
3. The logic diagram of MCU and CAN1 pins:
3. The logic diagram of MCU with CAN Transceiver (here is the CAN2 pins (it is the same as CAN1)
4. The configuration of Halcogen:
5. Test code( almost the same as sample code)
6. Execute the code above step by step, after sending the message out, the value of registers are the following: