Part Number: TPS65720
We are using TPS657201YFFR as a single PMIC in a battery driven product. It handles all power management in the design. We have a problem with the standby current (that is when HOLD_DCDC1 is low and PB_IN is pulled high using VSYS). We see a current being drained from the battery (3.7 volt) of about 1 mA going into BAT1/BAT2. My measurements show that there is no significant current being sourced by L1, VLDO1 and SYS1/SYS2. This makes me believe that the current is being drawn by an internal circuit of the TPS657201.
I have noticed that if we remove and then reinsert the battery the standby current is instead around 0.01 mA which is much more reasonable.
Do you have any idea why turning off the PMIC using HOLD_DCDC1 and PB_IN results in such a high standby current?