Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: TIDA-01130, ALP
Hi, Ti partner:
I have a camera system: TIDA-01130 (ov2775 + UB953 ) link to Nvidia TX2 Board(UB9534 + TX2 )
The Nvidia TX2 Board runs a linux system, with kernel-4.4 Version.
Now, I need to develop the TIDA-01130 driver that the camera can run in the TX2.
I have add the driver to suit TX2, but when i run v4l2-ctl tool to capture a RAM image from TIDA-01130, cat not get a valid RAM image.
About the TX2 log show, it indicate TX2 do not get a Frame Start from the ub954.
I have measure the MIPI CLK/DATA wave of the ov2775 and UB953 TXout, the wave is exited. But am not sure they are really correct.
I double it most be the UB953 TXout not correct.
Here is my UB954, UB953 register configures:
// UB954 init:
UB954_write_reg(s_data, 0x4c, 0x01);
UB954_write_reg(s_data, 0x58, 0x5e);
UB954_write_reg(s_data, 0x5b, 0x30);
UB954_write_reg(s_data, 0x5c, 0x30);
UB954_write_reg(s_data, 0x5d, 0x6c); //sensor i2c addr
UB954_write_reg(s_data, 0x65, 0x6c); //sensor i2c addr alias
UB954_write_reg(s_data, 0x6d, 0x7c);
UB954_write_reg(s_data, 0x32, 0x01);
UB954_write_reg(s_data, 0x33, 0x01);
UB954_write_reg(s_data, 0x21, 0x01);
UB954_write_reg(s_data, 0x20, 0x00)
// UB953 init:
// Sensor Mclk in: 24Mhz
UB953_write_reg(s_data, 0x06, 0x41);
UB953_write_reg(s_data, 0x07, 0x28);
//Sensor PWDN and RESET pins setting
UB953_write_reg(s_data, 0x0e, 0xf0);
UB953_write_reg(s_data, 0x0d, 0x00);
usleep_range(2000, 2010);
UB953_write_reg(s_data, 0x0d, 0x04);
usleep_range(2000, 2010);
UB953_write_reg(s_data, 0x0d, 0x0c);
usleep_range(2000, 2010);
Above these setting , my purpose :
1. TX2 supplied a 24Mhz MCLK to ub954, ub953 with the ub954 CLKin, that can supply a 24Mhz to ov2775 sensor
2. ov2775 with 4-lane MIPI output,link to the ub954 RX0, and ub954 RX1 are disabbled.
3. ub954 TX out with 4-lane to TX2-Board.
Please help me check if there registers setting are okay?
This issue troubled me a long time, thanks a lot!