This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3550: BAL pin vs no or single supercap

Part Number: LM3550


Section 7.3.5 read as follow:

The Balance pin (BAL), when connected to a super-capacitor (if needed), regulates the two sections of the
super-capacitor so that voltage on either cell is equal to ½ the output voltage.

What should we do with this pin if no supercap is present or if a single hjgh voltage (>5.5V) supercapacitor is used?