Section 7.3.5 read as follow:
The Balance pin (BAL), when connected to a super-capacitor (if needed), regulates the two sections of the
super-capacitor so that voltage on either cell is equal to ½ the output voltage.
What should we do with this pin if no supercap is present or if a single hjgh voltage (>5.5V) supercapacitor is used?