Part Number: DCP011512DB
Hi, Do I need t have equal caps and resistors on Vout+ and Vout-. ? What happened if for example I install 1K on Vout- and 100 Ohms on Vout+ ? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DCP011512DB
Hi, Do I need t have equal caps and resistors on Vout+ and Vout-. ? What happened if for example I install 1K on Vout- and 100 Ohms on Vout+ ? Thanks
Nader:
I recommend equal preloading on each ± output with equal value capacitors and resistors for equal Vout . The maximum load current for each output voltage is 33 mA (milli-Amps) .. A fixed 2000Ω resistor per channel preloading each channel with about 7.5mA.
Question?
What is the end application output circuitry? Is it a pre-driver for power application power FET pre-driver??
Tom
Nader:
Thanks for the schematic and op-amp to drive pressure sensors. Is the pressure sensor controlling another higher voltage circuit?
What is the output average ground voltage secondary as compared to the DCP011512D primary side ground ?
Why are there series resistors ( 1kΩ (-) 12V and 12.5Ω(+12V) between each DCP011512D output polarity and their output circuitry..
Tom
Nader:
Thanks for the update. Each +12V or (-) 12Voutput voltage level is directly affected by the output current. .Any load current variation or impedance loading on either bus will independently have different Vout level .
Tom