Hello guys,
One of my customers is looking for a PSE device of PoE.
They want to use a device which meets to the follwoing spec.
----------------
[Spec]
Input : 24V
Output : 48V/350mA
Meet to IEEE802.3af standard.
PSE side device.
------------------
If you don't have any other device, can I recommend TPS23841 to them?
Also when they use the device, they may need some support for software to control it.
Do you have any capability of software support for them to control TPS23841?
Your reply would be much appreciated.
Best regards,
Kazuya Nakai.