Other Parts Discussed in Thread: TPS562219A
Hi,
I'm using the TPS562210A in a project to generate 5V from 12V (also tried 15V, the result is the same), which is used to power a Raspberry Pi 3 model A+.
The system is working, but Ive got a very annoying noise coming from the power management stage, and I think that I found the source of this noise, which must probably be the inductor. This is the waveform on SW: 
The problem is that I don't know what is causing this issue, as I followed the guidances from the datasheet and the EVM User Guide. Any advice on this will be more than helpfull!
Attached are the schematic and the layout of the circuit.
Thanks for reading me,
Yoann