Other Parts Discussed in Post: OPA363

In the last few months, I’ve seen at least four cases of the wrong understanding of the “real Vos” of an op amp.

Figure 1 shows the specs for the OPA363 op amp, a single supply 1.8V to 5.5V op amp with 7MHz of unity gain bandwidth and a 5V/us slew rate. I’ve put a box around the real Vos of the OPA363 in the table below.

NOT! The real Vos of the OPA363 is directly dependent on how it is used in your application! 


Figure 1

Let’s look at how to calculate the real Vos for your application and keep your designs meeting their specification.

The key contributors to DC Offset voltage are:

     1)    Vos_drift (Vos change with temperature)

     2)    Vos_PSRR (Vos due to power supply rejection ratio)

     3)    Vos_CMRR (Vos due to common mode rejection ratio)

     4)    Vos_initial (Vos under factory test conditions)

Each of these individual contributors to Vos can have a positive or negative magnitude. We’ll do our initial computation assuming they all have a positive polarity.

Figure 2 uses information from Figure 1 to compute the individual contributors of offset due to the end application. It’s important to decipher the factory test conditions for Vos_initial, as listed in Figure 2.

Vos_drift is calculated by using the temperature difference between 25C and the end application.

Vos_PSRR is computed by noting the difference between the supply used in the end application and the supply used for Vos_initial test. 

Vos_CMRR requires a conversion of the CMRR specification, given in dB, to a linear attenuation specification given in uV/V. 

Now we have all of the contributing factors to the real Vos based on our end application.


Figure 2

So now what do we do with the individual contributors to Vos? 

All data sheet specs are usually obtained using a +/-3 sigma truncation of a typically Gaussian distribution of parts over process variations. So we can obtain the Vos_total _RSS by taking the root sum of squares of each individual contributor.

This RSS total implies a +/- 3 sigma coverage, or that 99.7% of all devices used in our application will be less than or equal to our computed Vos_total_RSS. This also means that 0.3% of parts can be larger than our Vos_total_RSS. 

If we want a conservative design margin, we can add all of the errors to yield Vos_total_max.


Figure 3

Figure 4 shows the summary of our real Vos investigation. Whether you decide to use Vos_total_RSS or Vos_total_max, remember that the totals can be positive or negative in polarity, as shown in Figure 4. 

Figure 4

Hopefully, you’ll consider the real Vos in your next application and avoid any unwanted surprises when your product goes to production.

And if you want to learn more about statistics and op amp noise, you might want to check out the book written by my boss, Art Kay (Kay, A., Operational Amplifier Noise, Newnes, 2012).

  • You are correct that the output of the op map will display a 9.12mV offset for a gain of 10 with a 912uV input offset voltage.  The only way I know of is to use a lower input offset voltage op amp or to trim the offset out with a potentiometer voltage summed into the input.  The problem with nulling the input offset voltage with a potentiometer is that over temperature and power supply fluctuations the initial offset you trim will change.  Consider an Auto-Zero or Chopper op amp such as OPA333.....

  • If the offset voltage is 912uV and the if the gain is 10 then whether the output of the op-amp will have a Dc offset of 9.12mV? How can I educe this offset voltage is there any method that can reduce the offset voltage other than trim pot offset correction correction

  • Please see link below to zip files that contain all of the old Burr-Brown Application Notes we are aware of.  Happy Analog-ing!

    e2e.ti.com/.../2573.burr-brown-application-notes.aspx

  • Tim,

    You mentioned in one of your replies to a comment that the Burr-Brown App Notes were available in the pdf format.  How might I access these files?

    Thanks,

    Bill Nurnberger

  • Howard:

    You are so right regarding the Burr-Brown App notes.  Most of op amp theory has not changed in the last 30 years (maybe longer but that's as far back as I can personally go for recollection).  Parts have gotten smaller, features enhanced and cost reduced.  We do have a collection of all of the Burr-Brown app notes in pdf format if you ever need one.  We are also working on continuous expansion of the TI Precision Designs landing page to offer all relevant collateral such as the old BB App Notes.  It is surprising to me that when I run into a subject I do not know in analog how little useful help I find on the web.  Like most engineers today, time is precious and I just want a quick and exact definition by example so I can figure stuff out and move on. Much of the old literature has not been scanned or readily avaialble on analog.  I guess we will just have to re-invent the wheel and hope it will last for a while.  Thanks for your comments and let us know how we can help you succeed in your applications.