This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Can I switch bewteen 2.4G 15.4 and Sub-G 15.4 in runtime?

Part Number: CC1352P

Hi, I use CC1352P, simplelink_cc13x2_26x2_sdk_5_10_00_48.


In SDK 15.4 examples, there are sub-g example and 2.4g example as below:

I have tested these two examples, and they can work normal.

Now I want to ask, can I use sub-g and 2.4g both in my application Or can I switch between sub-g and 2.4g in program runtime?