This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Can I switch between 2.4G and Sub-1G(915MHz) of TI 15.4 stack in runtime?

Part Number: CC1352P


Hi, I use CCC1352P, simplelink_cc13x2_26x2_sdk_4_40_04_04, CCS10.2.

I know CC1352P supports 2.4G and Sub-1G RF front end.

And I also know SDK provides DMM to support 15.4 and BLE two stacks runing in one single chip.

As for 15.4, I can choose 2.4G or Sub-1G.

| want to ask, can I use 2.4G AND Sub-1G both in 15.4 stack which means I have only one stack -- 15.4, but two RF front.

For example, I tx data on 2.4G 15.4 some time, and other time, I may tx data on Sub-1G 15.4.

So, based on the situation above, does SDK support this kind of feature?

Thanks.