Tool/software:
Similar schematics for LLC converter as Alex Drobyshev posted recently except that I use a separate source for AC voltage for HV startup but nonetheless my UCC256601 never started. What I can see is 7.9 to 8 VDC on pin12 for VCC (EVM shows 12VDC) and no 5VDC on pin 8 for V5P. With an oscilloscope I can only see there 1volt square shape pulses, 120ms long with a period of about 1200ms on pin8 for V5P. When I tried to reduce AC voltage supplied from an isolated transformer to pin1 for HV, the frequency for those pulses increases also but their magnitude remains the same at 1V level. VCC voltage does not change, it stays at about 8VDC level. When the power was turned off surprisingly those pulses stay for a very long time, about 10-20 minutes. Some large capacity discharging at very low consumption rate? I checked all components connected to V5P, nothing that can overload it during start up. TSET resistors are 1000K/200K for Upper/Lower. LL resistors are 600K/150K respectively. C10 is 4.7uF. C13 is 1uF ceramic capacitor. OTP programming circuit connected not to Vin as Alex shows but to Vcc as suggested in EVM schematics. What could be wrong that prevents the HV startup?