Part Number: TPS25854-Q1
Other Parts Discussed in Thread: TPS25846-Q1, , TPS25830A-Q1, TPS25772-Q1, TPS55289-Q1
Tool/software:
Dear TI experts,
My customer prepare the project of wired USB charging solution for car.
I suggested some parts based on TI's roadmap.
1. In the roadmap, I can see the logo of Apple carplay beside TPS25846-Q1. -> Can I expect that there is no issue along the process of MFI certification like OCP(Over Current Protection)?
2. On the other hand, I cannot see the logo of Apple Carplay beside TPS25854-Q1. It is recommended as USB charging box solution. -> Can I expect that I cannot use it in the position which need MFI certification?
-> If so, Could you suggest other IC which have no problem with MFI certification fo USB charging box?
3. Could you recommend dual USB-C PD solution (single port 45W, dual port 30+30W) for Apple carplay?
Please check this issue. Thanks.
Best regards,
Chase