This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6754-Q1: Audio stops due to DC fault detection with 2ohm speaker and big volume

Part Number: TAS6754-Q1
Other Parts Discussed in Thread: TAS67524-Q1,

Tool/software:

Hello experts,

My customer sees audio output stopping with 2ohm speaker and big volume. They use TAS6754-Q1 EVM and they will use TAS67524-Q1 in MP.

Temperature: Room temp
PVDD/VBAT: 15V
Input: Pink noise
Load: 2ohm speaker
Result: When they use 2ohm speaker, audio output stops in 0dB ~ -3dB volume. When they use 4ohm speaker, no stop in all volume range.

After the audio stop, they see DC fault detection. What is the root cause and workaround for this? Their target is no audio shutdown in 9~16V PVDD/VBAT, 2ohm speaker, and 10% THD.

Please refer to below waveform for 4ohm speaker case. Audio does not stop in this case.

Regards,

Kento