Other Parts Discussed in Thread: LMZ21700
Hello,
I have a design using a LMZ21700 to buck voltage from 4.2V (from a battery) down to 3.6V. The load is able to operate from 3.8V down to 3.1V. The expectation was that below 3.6V the output would drop with the input and the load can measure the incoming voltage and sense when the battery voltage is getting too low.
The circuit works fine but once the battery voltage falls below 3.6V then it seems to draw 1mA quiescent current.
Am I missing something in the datasheet? I have looked it over and I just expected the High Side Driver to simply go on but maybe I missed something. Can the PWM mode it 100%?
I am not using Power Good (It just goes out to a test point).
Thanks in advance!