Part Number: TMS320DM8127
Other Parts Discussed in Thread: IPNC-RDK-CSK, AM5728
Hello,
we are planning to buy an eval board for the DM8127 (TMDSCSK8127-CSKCC-BNDL).
And we have some questions before:
1. We want to stream 1920x1080p30 video via network and do parallel recording to USB stick. Configuration of streaming and recording should be done via Web Interface. Access to video files via file server should be possible. Is this already available in example application (especially video file server)? Can this be realized?
2. Are video input formats BT1120 and BT656 supported?
3. Does the device support frame rate and resolution up/down conversion?
4. Is the required functionality available and tested in the IPNC-RDK-CSK?
5. We have a VIP subdevice driver for the sitara AM5728, can we reuse it for video input on the DM8127? Or has the IPNC-RDK-CSK another software architecture? Do you use V4L2? Is there example code on how to write video input drivers for UART and I2C camera devices?
6. What does the TMDSCSK8127-CSKCC-BNDL include (carrier board, processor board, camera module, power supply,...)? What do we have to purchase extra?
Thanks in advance for your efforts
Marc