Part Number: CC1312R
Other Parts Discussed in Thread: SYSCONFIG
I have a CC1312R application based on SimpleLink CC13x2 SDK.
I have nothing special in the ccfg.c file regarding the GPRAM.
In the memory allocation tab of Code Composer, GPRAM appears as 0% usage of 8k.

Is by default GPRAM in "off mode" and not used at all? If I want to use GPRAM as a cache of the SYS flash, should I add the following in my main file:
VIMSConfigure(VIMS_BASE, TRUE, TRUE);
VIMSModeSet(VIMS_BASE, VIMS_MODE_ENABLED);
How can I know if GPRAM is used in cache mode?
Let's say that now I want to "merge" the GPRAM into the SRAM. Is that possible or will they ever stay separate? Can it appear merged in the memory allocation? For such objective, I tried to add:
#define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM 0x0
in the ccfg.c file. In main.c I have put:
Power_setConstraint(PowerCC26XX_SB_VIMS_CACHE_RETAIN); Power_setConstraint(PowerCC26XX_NEED_FLASH_IN_IDLE);
What else do I need to do? Am I going to see 88kB of SRAM after or do I need to decide which global variables go into the GPRAM and how to do that? Is GPRAM access time similar to SRAM?
Here is the content of my TIRTOS.cmd file:
--stack_size=1024 /* C stack is also used for ISR stack */
HEAPSIZE = 0x1000; /* Size of heap buffer used by HeapMem */
/* Retain interrupt vector table variable */
--retain=g_pfnVectors
/* Override default entry point. */
--entry_point ResetISR
/* Allow main() to take args */
--args 0x8
/* Suppress warnings and errors: */
/* - 10063: Warning about entry point not being _c_int00 */
/* - 16011, 16012: 8-byte alignment errors. Observed when linking in object */
/* files compiled using Keil (ARM compiler) */
--diag_suppress=10063,16011,16012
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M3_T_le_eabi.lib */
/* The starting address of the application. Normally the interrupt vectors */
/* must be located at the beginning of the application. */
#define FLASH_BASE 0x0
#define FLASH_SIZE 0x58000
#define RAM_BASE 0x20000000
#define RAM_SIZE 0x14000
#define GPRAM_BASE 0x11000000
#define GPRAM_SIZE 0x2000
/* System memory map */
MEMORY
{
/* Application stored in and executes from internal flash */
FLASH (RX) : origin = FLASH_BASE, length = FLASH_SIZE
/* Application uses internal RAM for data */
SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE
/* Application can use GPRAM region as RAM if cache is disabled in the CCFG
(DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */
GPRAM (RWX): origin = GPRAM_BASE, length = GPRAM_SIZE
}
/* Section allocation in memory */
SECTIONS
{
.intvecs : > FLASH_BASE
.text : >> FLASH
.TI.ramfunc : {} load=FLASH, run=SRAM, table(BINIT)
.const : >> FLASH
.constdata : >> FLASH
.rodata : >> FLASH
.binit : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.emb_text : >> FLASH
.ccfg : > FLASH (HIGH)
.vtable : > SRAM
.vtable_ram : > SRAM
vtable_ram : > SRAM
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM (HIGH)
.nonretenvar : > SRAM
/* Heap buffer used by HeapMem */
.priheap : {
__primary_heap_start__ = .;
. += HEAPSIZE;
__primary_heap_end__ = .;
} > SRAM align 8
.gpram : > GPRAM
}