Part Number: TDA4VM
How do I port an R5F RTOS Ethernet client running on MCU2_1 to other R5F cores (ex: MCU3_0 core) in SoCs with multiple R5F cores?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
How do I port an R5F RTOS Ethernet client running on MCU2_1 to other R5F cores (ex: MCU3_0 core) in SoCs with multiple R5F cores?
This requires porting efforts on top of Enet LLD and Ethernet Firmware provided in the standard TI SDK.
The above list summarizes the software changes needed to run an RTOS client on mcu3_0 instead of mcu2_1.
The attached patch provides a reference to illustrate the software changes corresponding to the summary shown above. The patch was based on SDK 8.6.
From 03a33c9a2d8dbbcb6f1564d671426e20a7ead6c7 Mon Sep 17 00:00:00 2001
From: sudheer <s-doredla@ti.com>
Date: Wed, 29 Mar 2023 19:40:51 +0530
Subject: [PATCH] ethfw: client: MCU_3_0 support
Reference code to enable RTOS client support on mcu3_0 core in J721E
device as a replacement for mcu2_1 core which is supported by default.
It does NOT aim at adding suppor tmcu3_0 in addition to mcu2_1.
The changes are summarized below:
- Replace IPC id of the RTOS client (IPC_MCU2_1 -> IPC_MCU3_0) in
EthFw library, CpswProxy server and client, as well as EthFw server
app.
- Replace IPC core id where virtual switch port and virtual MAC port
interfaces are enabled on.
- Update memory addresses used for MCU3_0 IPC (0xA3000000 -> 0xA4000000).
- Rename intercore macros as per corresponding changes in Enet LLD
for mcu3_0 support.
- Enabling mcu3_0 core in driver's CORELIST
* Core Enet LLD driver support only
* No examples are being enabled
- Replace mcu2_1 with mcu3_0 in intercore and lwipific libraries
* Meant for cases where RTOS client core is mcu3_0, not mcu2_1
* No intention to support mcu3_0 in addition to mcu2_1
Signed-off-by: sudheer <s-doredla@ti.com>
---
.../{mcu_2_1 => mcu_3_0}/concerto.mak | 4 +-
.../j7200/linker_mem_map.cmd | 12 ++--
.../j721e/linker_mem_map.cmd | 12 ++--
.../j784s4/linker_mem_map.cmd | 12 ++--
.../{mcu_2_1 => mcu_3_0}/linker_freertos.cmd | 56 +++++++++----------
.../{mcu_2_1 => mcu_3_0}/linker_safertos.cmd | 30 +++++-----
.../linker_safertos_j7200.cmd | 30 +++++-----
.../{mcu_2_1 => mcu_3_0}/main.c | 10 ++--
.../app_remoteswitchcfg_server/mcu_2_0/main.c | 32 +++++------
ethfw/apps/common/r5f_mpu_j721e_default.c | 4 +-
ethfw/apps/common/r5f_mpu_j721e_safertos.c | 4 +-
ethfw/apps/common/r5f_mpu_j784s4_default.c | 4 +-
ethfw/apps/common/r5f_mpu_j784s4_safertos.c | 4 +-
ethfw/ethfw/src/ethfw.c | 2 +-
ethfw/ethfw_build_flags.mak | 4 +-
ethfw/ethremotecfg/client/src/cpsw_proxy.c | 2 +-
.../packages/ti/drv/enet/enet_component.mk | 4 +-
.../ti/drv/enet/intercore/include/ic_ipc.h | 2 +-
.../ti/drv/enet/intercore/include/ic_queue.h | 8 +--
.../ti/drv/enet/lwipific/inc/bufpool.h | 6 +-
.../ti/drv/enet/lwipific/inc/lwip2enet_ic.h | 12 ++--
.../ti/drv/enet/lwipific/src/lwip2enet_ic.c | 26 ++++-----
.../ti/drv/enet/soc/j7x/j721e/enet_soc.c | 22 +++++++-
23 files changed, 161 insertions(+), 141 deletions(-)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/concerto.mak (97%)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/j7200/linker_mem_map.cmd (92%)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/j721e/linker_mem_map.cmd (92%)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/j784s4/linker_mem_map.cmd (92%)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/linker_freertos.cmd (75%)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/linker_safertos.cmd (91%)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/linker_safertos_j7200.cmd (91%)
rename ethfw/apps/app_remoteswitchcfg_client/{mcu_2_1 => mcu_3_0}/main.c (99%)
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/concerto.mak b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/concerto.mak
similarity index 97%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/concerto.mak
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/concerto.mak
index 3a23e13e..58d9cb56 100755
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/concerto.mak
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/concerto.mak
@@ -2,10 +2,10 @@
include $(PRELUDE)
-ifeq ($(BUILD_CPU_MCU2_1),yes)
+ifeq ($(BUILD_CPU_MCU3_0),yes)
ifneq (,$(filter $(TARGET_CPU),R5F R5Ft))
-CPU_ID=mcu2_1
+CPU_ID=mcu3_0
TARGET := app_remoteswitchcfg_client
TARGETTYPE := exe
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j7200/linker_mem_map.cmd b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j7200/linker_mem_map.cmd
similarity index 92%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j7200/linker_mem_map.cmd
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j7200/linker_mem_map.cmd
index b2d88ddf..39e57c24 100644
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j7200/linker_mem_map.cmd
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j7200/linker_mem_map.cmd
@@ -71,12 +71,12 @@ MEMORY
R5F_TCMA ( X ) : ORIGIN = 0x00000100 , LENGTH = 0x00007F00
/* R5F_TCMB0 [ size 32.00 KB ] */
R5F_TCMB0 ( RWIX ) : ORIGIN = 0x41010000 , LENGTH = 0x00008000
- /* DDR for MCU2_1 for Linux IPC [ size 1024.00 KB ] */
- DDR_MCU2_1_IPC ( RWIX ) : ORIGIN = 0xA3000000 , LENGTH = 0x00100000
- /* DDR for MCU2_1 for Linux resource table [ size 1024 B ] */
- DDR_MCU2_1_RESOURCE_TABLE ( RWIX ) : ORIGIN = 0xA3100000 , LENGTH = 0x00000400
- /* DDR for MCU2_1 for code/data [ size 63.00 MB ] */
- DDR_MCU2_1 ( RWIX ) : ORIGIN = 0xA3100400 , LENGTH = 0x00EFFC00
+ /* DDR for MCU3_0 for Linux IPC [ size 1024.00 KB ] */
+ DDR_MCU3_0_IPC ( RWIX ) : ORIGIN = 0xA3000000 , LENGTH = 0x00100000
+ /* DDR for MCU3_0 for Linux resource table [ size 1024 B ] */
+ DDR_MCU3_0_RESOURCE_TABLE ( RWIX ) : ORIGIN = 0xA3100000 , LENGTH = 0x00000400
+ /* DDR for MCU3_0 for code/data [ size 63.00 MB ] */
+ DDR_MCU3_0 ( RWIX ) : ORIGIN = 0xA3100400 , LENGTH = 0x00EFFC00
/* Memory for remote core logging [ size 256.00 KB ] */
APP_LOG_MEM : ORIGIN = 0xB8000000 , LENGTH = 0x00040000
/* Memory for TI OpenVX shared memory. MUST be non-cached or cache-coherent [ size 31.75 MB ] */
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j721e/linker_mem_map.cmd b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j721e/linker_mem_map.cmd
similarity index 92%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j721e/linker_mem_map.cmd
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j721e/linker_mem_map.cmd
index b84ae5af..3e6fbf05 100644
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j721e/linker_mem_map.cmd
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j721e/linker_mem_map.cmd
@@ -71,12 +71,12 @@ MEMORY
R5F_TCMA ( X ) : ORIGIN = 0x00000100 , LENGTH = 0x00007F00
/* R5F_TCMB0 [ size 32.00 KB ] */
R5F_TCMB0 ( RWIX ) : ORIGIN = 0x41010000 , LENGTH = 0x00008000
- /* DDR for MCU2_1 for Linux IPC [ size 1024.00 KB ] */
- DDR_MCU2_1_IPC ( RWIX ) : ORIGIN = 0xA3000000 , LENGTH = 0x00100000
- /* DDR for MCU2_1 for Linux resource table [ size 1024 B ] */
- DDR_MCU2_1_RESOURCE_TABLE ( RWIX ) : ORIGIN = 0xA3100000 , LENGTH = 0x00000400
- /* DDR for MCU2_1 for code/data [ size 63.00 MB ] */
- DDR_MCU2_1 ( RWIX ) : ORIGIN = 0xA3100400 , LENGTH = 0x00EFFC00
+ /* DDR for MCU3_0 for Linux IPC [ size 1024.00 KB ] */
+ DDR_MCU3_0_IPC ( RWIX ) : ORIGIN = 0xA4000000 , LENGTH = 0x00100000
+ /* DDR for MCU3_0 for Linux resource table [ size 1024 B ] */
+ DDR_MCU3_0_RESOURCE_TABLE ( RWIX ) : ORIGIN = 0xA4100000 , LENGTH = 0x00000400
+ /* DDR for MCU3_0 for code/data [ size 63.00 MB ] */
+ DDR_MCU3_0 ( RWIX ) : ORIGIN = 0xA4100400 , LENGTH = 0x00EFFC00
/* Memory for remote core logging [ size 256.00 KB ] */
APP_LOG_MEM : ORIGIN = 0xB8000000 , LENGTH = 0x00040000
/* Memory for TI OpenVX shared memory. MUST be non-cached or cache-coherent [ size 31.75 MB ] */
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j784s4/linker_mem_map.cmd b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j784s4/linker_mem_map.cmd
similarity index 92%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j784s4/linker_mem_map.cmd
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j784s4/linker_mem_map.cmd
index c30d0c1c..a1c03b4d 100644
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/j784s4/linker_mem_map.cmd
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/j784s4/linker_mem_map.cmd
@@ -71,12 +71,12 @@ MEMORY
R5F_TCMA ( X ) : ORIGIN = 0x00000100 , LENGTH = 0x00007F00
/* R5F_TCMB0 [ size 32.00 KB ] */
R5F_TCMB0 ( RWIX ) : ORIGIN = 0x41010000 , LENGTH = 0x00008000
- /* DDR for MCU2_1 for Linux IPC [ size 1024.00 KB ] */
- DDR_MCU2_1_IPC ( RWIX ) : ORIGIN = 0xA3000000 , LENGTH = 0x00100000
- /* DDR for MCU2_1 for Linux resource table [ size 1024 B ] */
- DDR_MCU2_1_RESOURCE_TABLE ( RWIX ) : ORIGIN = 0xA3100000 , LENGTH = 0x00000400
- /* DDR for MCU2_1 for code/data [ size 63.00 MB ] */
- DDR_MCU2_1 ( RWIX ) : ORIGIN = 0xA3100400 , LENGTH = 0x00EFFC00
+ /* DDR for MCU3_0 for Linux IPC [ size 1024.00 KB ] */
+ DDR_MCU3_0_IPC ( RWIX ) : ORIGIN = 0xA4000000 , LENGTH = 0x00100000
+ /* DDR for MCU3_0 for Linux resource table [ size 1024 B ] */
+ DDR_MCU3_0_RESOURCE_TABLE ( RWIX ) : ORIGIN = 0xA4100000 , LENGTH = 0x00000400
+ /* DDR for MCU3_0 for code/data [ size 63.00 MB ] */
+ DDR_MCU3_0 ( RWIX ) : ORIGIN = 0xA4100400 , LENGTH = 0x00EFFC00
/* Memory for remote core logging [ size 256.00 KB ] */
APP_LOG_MEM : ORIGIN = 0xB8000000 , LENGTH = 0x00040000
/* Memory for TI OpenVX shared memory. MUST be non-cached or cache-coherent [ size 31.75 MB ] */
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_freertos.cmd b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_freertos.cmd
similarity index 75%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_freertos.cmd
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_freertos.cmd
index 9df357a3..6e8716eb 100644
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_freertos.cmd
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_freertos.cmd
@@ -64,66 +64,66 @@ SECTIONS
*(.text:Udma_ringDequeueRaw*)
*(.text:Udma_virtToPhyFxn*)
*/
- } > DDR_MCU2_1
+ } > DDR_MCU3_0
.text_rest{
_text_rest_begin = .;
*(.text)
_text_rest_end = .;
- } palign(32) > DDR_MCU2_1
+ } palign(32) > DDR_MCU3_0
- .const : {} palign(8) > DDR_MCU2_1
- .rodata : {} palign(8) > DDR_MCU2_1
- .cinit : {} palign(8) > DDR_MCU2_1
+ .const : {} palign(8) > DDR_MCU3_0
+ .rodata : {} palign(8) > DDR_MCU3_0
+ .cinit : {} palign(8) > DDR_MCU3_0
.pinit : {} palign(8) > R5F_TCMB0
- .bss : {} align(4) > DDR_MCU2_1
- .far : {} align(4) > DDR_MCU2_1
- .data : {} palign(128) > DDR_MCU2_1
- .sysmem : {} > DDR_MCU2_1
- .data_buffer : {} palign(128) > DDR_MCU2_1
- .bss.devgroup* : {} align(4) > DDR_MCU2_1
- .const.devgroup* : {} align(4) > DDR_MCU2_1
- .boardcfg_data : {} align(4) > DDR_MCU2_1
-
- ipc_data_buffer (NOINIT) : {} palign(128) > DDR_MCU2_1
+ .bss : {} align(4) > DDR_MCU3_0
+ .far : {} align(4) > DDR_MCU3_0
+ .data : {} palign(128) > DDR_MCU3_0
+ .sysmem : {} > DDR_MCU3_0
+ .data_buffer : {} palign(128) > DDR_MCU3_0
+ .bss.devgroup* : {} align(4) > DDR_MCU3_0
+ .const.devgroup* : {} align(4) > DDR_MCU3_0
+ .boardcfg_data : {} align(4) > DDR_MCU3_0
+
+ ipc_data_buffer (NOINIT) : {} palign(128) > DDR_MCU3_0
.resource_table :
{
__RESOURCE_TABLE = .;
- } > DDR_MCU2_1_RESOURCE_TABLE
+ } > DDR_MCU3_0_RESOURCE_TABLE
intercore_eth_desc_mem (NOLOAD) : {} palign(128) > INTERCORE_ETH_DESC_MEM
intercore_eth_data_mem (NOLOAD) : {} palign(128) > INTERCORE_ETH_DATA_MEM
- .tracebuf : {} align(1024) > DDR_MCU2_1
+ .tracebuf : {} align(1024) > DDR_MCU3_0
- .bss:ENET_DMA_DESC_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_RING_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_PKT_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_OBJ_MEM (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
+ .bss:ENET_DMA_DESC_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_RING_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_PKT_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_OBJ_MEM (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
.bss:app_log_mem (NOLOAD) : {} > APP_LOG_MEM
.bss:ipc_vring_mem (NOLOAD) : {} > IPC_VRING_MEM
- .bss:ddr_shared_mem (NOLOAD) : {} > DDR_MCU2_1
+ .bss:ddr_shared_mem (NOLOAD) : {} > DDR_MCU3_0
- .stack : {} align(4) > DDR_MCU2_1 (HIGH)
+ .stack : {} align(4) > DDR_MCU3_0 (HIGH)
- .irqStack : {. = . + __IRQ_STACK_SIZE;} align(4) > DDR_MCU2_1 (HIGH)
+ .irqStack : {. = . + __IRQ_STACK_SIZE;} align(4) > DDR_MCU3_0 (HIGH)
RUN_START(__IRQ_STACK_START)
RUN_END(__IRQ_STACK_END)
- .fiqStack : {. = . + __FIQ_STACK_SIZE;} align(4) > DDR_MCU2_1 (HIGH)
+ .fiqStack : {. = . + __FIQ_STACK_SIZE;} align(4) > DDR_MCU3_0 (HIGH)
RUN_START(__FIQ_STACK_START)
RUN_END(__FIQ_STACK_END)
- .abortStack : {. = . + __ABORT_STACK_SIZE;} align(4) > DDR_MCU2_1 (HIGH)
+ .abortStack : {. = . + __ABORT_STACK_SIZE;} align(4) > DDR_MCU3_0 (HIGH)
RUN_START(__ABORT_STACK_START)
RUN_END(__ABORT_STACK_END)
- .undStack : {. = . + __UND_STACK_SIZE;} align(4) > DDR_MCU2_1 (HIGH)
+ .undStack : {. = . + __UND_STACK_SIZE;} align(4) > DDR_MCU3_0 (HIGH)
RUN_START(__UND_STACK_START)
RUN_END(__UND_STACK_END)
- .svcStack : {. = . + __SVC_STACK_SIZE;} align(4) > DDR_MCU2_1 (HIGH)
+ .svcStack : {. = . + __SVC_STACK_SIZE;} align(4) > DDR_MCU3_0 (HIGH)
RUN_START(__SVC_STACK_START)
RUN_END(__SVC_STACK_END)
} /* end of SECTIONS */
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_safertos.cmd b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_safertos.cmd
similarity index 91%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_safertos.cmd
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_safertos.cmd
index 45dd05cf..84e52a52 100644
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_safertos.cmd
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_safertos.cmd
@@ -71,46 +71,46 @@ SECTIONS
{
.KERNEL_FUNCTION LOAD_START( lnkKernelFuncStartAddr ),
LOAD_END( lnkKernelFuncEndAddr ) : {} palign( 0x10000 )
- } > DDR_MCU2_1
+ } > DDR_MCU3_0
- .text : palign(32) > DDR_MCU2_1
- .rodata : palign(8) > DDR_MCU2_1
+ .text : palign(32) > DDR_MCU3_0
+ .rodata : palign(8) > DDR_MCU3_0
.text_fast {
- } > DDR_MCU2_1
+ } > DDR_MCU3_0
.text_rest{
_text_rest_begin = .;
*(.text)
_text_rest_end = .;
- } palign(32) > DDR_MCU2_1
+ } palign(32) > DDR_MCU3_0
- ipc_data_buffer (NOINIT) : {} palign(128) > DDR_MCU2_1
+ ipc_data_buffer (NOINIT) : {} palign(128) > DDR_MCU3_0
.resource_table :
{
__RESOURCE_TABLE = .;
- } > DDR_MCU2_1_RESOURCE_TABLE
+ } > DDR_MCU3_0_RESOURCE_TABLE
intercore_eth_desc_mem (NOLOAD) : {} palign(128) > INTERCORE_ETH_DESC_MEM
intercore_eth_data_mem (NOLOAD) : {} palign(128) > INTERCORE_ETH_DATA_MEM
- .tracebuf : {} align(1024) > DDR_MCU2_1
+ .tracebuf : {} align(1024) > DDR_MCU3_0
- .bss:ENET_DMA_DESC_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_RING_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_PKT_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_OBJ_MEM (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
+ .bss:ENET_DMA_DESC_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_RING_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_PKT_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_OBJ_MEM (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
/* Used in Switch configuration tool */
- .serialContext (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
+ .serialContext (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
.bss:app_log_mem (NOLOAD) : {} > APP_LOG_MEM
.bss:ipc_vring_mem (NOLOAD) : {} > IPC_VRING_MEM
- .bss:ddr_shared_mem (NOLOAD) : {} > DDR_MCU2_1
+ .bss:ddr_shared_mem (NOLOAD) : {} > DDR_MCU3_0
/* Data sections. */
GROUP palign( 0x10000 ), LOAD_START( lnkRamStartAddr ), LOAD_END( lnkRamEndAddr )
@@ -149,7 +149,7 @@ SECTIONS
.svcStack END( lnkStacksEndAddr ) : {. = . + __SVC_STACK_SIZE;} align(4)
RUN_START(__SVC_STACK_START)
RUN_END(__SVC_STACK_END)
- } > DDR_MCU2_1
+ } > DDR_MCU3_0
}
/*-------------------------------- END ---------------------------------------*/
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_safertos_j7200.cmd b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_safertos_j7200.cmd
similarity index 91%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_safertos_j7200.cmd
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_safertos_j7200.cmd
index 01948fe7..ada597ed 100644
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/linker_safertos_j7200.cmd
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/linker_safertos_j7200.cmd
@@ -71,46 +71,46 @@ SECTIONS
{
.KERNEL_FUNCTION LOAD_START( lnkKernelFuncStartAddr ),
LOAD_END( lnkKernelFuncEndAddr ) : {} palign( 0x10000 )
- } > DDR_MCU2_1
+ } > DDR_MCU3_0
- .text : palign(32) > DDR_MCU2_1
- .rodata : palign(8) > DDR_MCU2_1
+ .text : palign(32) > DDR_MCU3_0
+ .rodata : palign(8) > DDR_MCU3_0
.text_fast {
- } > DDR_MCU2_1
+ } > DDR_MCU3_0
.text_rest{
_text_rest_begin = .;
*(.text)
_text_rest_end = .;
- } palign(32) > DDR_MCU2_1
+ } palign(32) > DDR_MCU3_0
- ipc_data_buffer (NOINIT) : {} palign(128) > DDR_MCU2_1
+ ipc_data_buffer (NOINIT) : {} palign(128) > DDR_MCU3_0
.resource_table :
{
__RESOURCE_TABLE = .;
- } > DDR_MCU2_1_RESOURCE_TABLE
+ } > DDR_MCU3_0_RESOURCE_TABLE
intercore_eth_desc_mem (NOLOAD) : {} palign(128) > INTERCORE_ETH_DESC_MEM
intercore_eth_data_mem (NOLOAD) : {} palign(128) > INTERCORE_ETH_DATA_MEM
- .tracebuf : {} align(1024) > DDR_MCU2_1
+ .tracebuf : {} align(1024) > DDR_MCU3_0
- .bss:ENET_DMA_DESC_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_RING_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_PKT_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
- .bss:ENET_DMA_OBJ_MEM (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
+ .bss:ENET_DMA_DESC_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_RING_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_PKT_MEMPOOL (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
+ .bss:ENET_DMA_OBJ_MEM (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
/* Used in Switch configuration tool */
- .serialContext (NOLOAD) {} ALIGN (128) > DDR_MCU2_1
+ .serialContext (NOLOAD) {} ALIGN (128) > DDR_MCU3_0
.bss:app_log_mem (NOLOAD) : {} > APP_LOG_MEM
.bss:ipc_vring_mem (NOLOAD) : {} > IPC_VRING_MEM
- .bss:ddr_shared_mem (NOLOAD) : {} > DDR_MCU2_1
+ .bss:ddr_shared_mem (NOLOAD) : {} > DDR_MCU3_0
/* Data sections. */
GROUP palign( 0x10000 ), LOAD_START( lnkRamStartAddr ), LOAD_END( lnkRamEndAddr )
@@ -149,7 +149,7 @@ SECTIONS
.svcStack END( lnkStacksEndAddr ) : {. = . + __SVC_STACK_SIZE;} align(4)
RUN_START(__SVC_STACK_START)
RUN_END(__SVC_STACK_END)
- } > DDR_MCU2_1
+ } > DDR_MCU3_0
}
/*-------------------------------- END ---------------------------------------*/
diff --git a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/main.c b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/main.c
similarity index 99%
rename from ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/main.c
rename to ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/main.c
index 9598ffc4..3f47bc16 100644
--- a/ethfw/apps/app_remoteswitchcfg_client/mcu_2_1/main.c
+++ b/ethfw/apps/app_remoteswitchcfg_client/mcu_3_0/main.c
@@ -241,7 +241,7 @@ static uint8_t gCntrlBuf[CPSW_REMOTE_APP_IPC_DATA_SIZE] __attribute__ ((section(
static uint8_t g_vringMemBuf[IPC_VRING_MEM_SIZE] __attribute__ ((section(".bss:ipc_vring_mem"), aligned(8192)));
-static uint32_t selfProcId = IPC_MCU2_1;
+static uint32_t selfProcId = IPC_MCU3_0;
static uint32_t gRemoteProc[] =
{
#if defined(SOC_J721E)
@@ -262,8 +262,8 @@ static uint32_t gNumRemoteProc = sizeof(gRemoteProc) / sizeof(uint32_t);
static struct netif netif_ic;
static uint32_t netif_ic_state[IC_ETH_MAX_VIRTUAL_IF] =
{
- IC_ETH_IF_MCU2_0_MCU2_1,
- IC_ETH_IF_MCU2_1_MCU2_0,
+ IC_ETH_IF_MCU2_0_MCU3_0,
+ IC_ETH_IF_MCU3_0_MCU2_0,
IC_ETH_IF_MCU2_0_A72
};
@@ -1056,9 +1056,9 @@ static void EthApp_initNetif(CpswRemoteApp_VirtNetif *virtNetif)
NETIF_SET_CHECKSUM_CTRL(netif, chksumFlags);
#endif
- /* Create inter-core virtual ethernet interface: MCU2_1 <-> MCU2_0 */
+ /* Create inter-core virtual ethernet interface: MCU3_0 <-> MCU2_0 */
netif_add(&netif_ic, NULL, NULL, NULL,
- (void*)&netif_ic_state[IC_ETH_IF_MCU2_1_MCU2_0],
+ (void*)&netif_ic_state[IC_ETH_IF_MCU3_0_MCU2_0],
LWIPIF_LWIP_IC_init, tcpip_input);
/* Create bridge interface */
diff --git a/ethfw/apps/app_remoteswitchcfg_server/mcu_2_0/main.c b/ethfw/apps/app_remoteswitchcfg_server/mcu_2_0/main.c
index 75f18755..5cb4a469 100644
--- a/ethfw/apps/app_remoteswitchcfg_server/mcu_2_0/main.c
+++ b/ethfw/apps/app_remoteswitchcfg_server/mcu_2_0/main.c
@@ -214,7 +214,7 @@
#define ETHAPP_BRIDGEIF_CPU_PORT_ID BRIDGEIF_MAX_PORTS
/* Inter-core netif IDs */
-#define ETHAPP_NETIF_IC_MCU2_0_MCU2_1_IDX (0U)
+#define ETHAPP_NETIF_IC_MCU2_0_MCU3_0_IDX (0U)
#define ETHAPP_NETIF_IC_MCU2_0_A72_IDX (1U)
#define ETHAPP_NETIF_IC_MAX_IDX (2U)
@@ -224,8 +224,8 @@
/* Required size of the MAC address pool (specific to the TI EVM configuration):
* 1 x MAC address for Ethernet Firmware
* 2 x MAC address for mpu1_0 virtual switch and MAC-only ports (Linux, 1 for QNX)
- * 2 x MAC address for mcu2_1 virtual switch and MAC-only ports (RTOS)
- * 1 x MAC address for mcu2_1 virtual switch port (AUTOSAR) */
+ * 2 x MAC address for MCU3_0 virtual switch and MAC-only ports (RTOS)
+ * 1 x MAC address for MCU3_0 virtual switch port (AUTOSAR) */
#define ETHAPP_MAC_ADDR_POOL_SIZE (6U)
/* Define A72_QNX_OS if A72 is running Qnx. Qnx doesn't load resource table. */
@@ -444,7 +444,7 @@ static EthFw_VirtPortCfg gEthApp_virtPortCfg[] =
.portId = ETHREMOTECFG_SWITCH_PORT_0,
},
{
- .remoteCoreId = IPC_MCU2_1,
+ .remoteCoreId = IPC_MCU3_0,
.portId = ETHREMOTECFG_SWITCH_PORT_1,
},
#if defined(ENABLE_MAC_ONLY_PORTS)
@@ -453,7 +453,7 @@ static EthFw_VirtPortCfg gEthApp_virtPortCfg[] =
.portId = ETHREMOTECFG_MAC_PORT_1,
},
{
- .remoteCoreId = IPC_MCU2_1,
+ .remoteCoreId = IPC_MCU3_0,
.portId = ETHREMOTECFG_MAC_PORT_4,
},
#endif
@@ -462,7 +462,7 @@ static EthFw_VirtPortCfg gEthApp_virtPortCfg[] =
static EthFw_VirtPortCfg gEthApp_autosarVirtPortCfg[] =
{
{
- .remoteCoreId = IPC_MCU2_1,
+ .remoteCoreId = IPC_MCU3_0,
.portId = ETHREMOTECFG_SWITCH_PORT_1,
},
};
@@ -486,13 +486,13 @@ static uint8_t gEthAppVringMemBuf[IPC_VRING_MEM_SIZE] __attribute__ ((section(".
static uint32_t gEthAppRemoteProc[] =
{
#if defined(SOC_J721E)
- IPC_MPU1_0, IPC_MCU1_0, IPC_MCU1_1, IPC_MCU2_1,
+ IPC_MPU1_0, IPC_MCU1_0, IPC_MCU1_1, IPC_MCU3_0,
IPC_MCU3_0, IPC_MCU3_1, IPC_C66X_1, IPC_C66X_2,
IPC_C7X_1,
#elif defined(SOC_J7200)
- IPC_MPU1_0, IPC_MCU1_0, IPC_MCU1_1, IPC_MCU2_1,
+ IPC_MPU1_0, IPC_MCU1_0, IPC_MCU1_1, IPC_MCU3_0,
#elif defined(SOC_J784S4)
- IPC_MPU1_0, IPC_MCU1_0, IPC_MCU1_1, IPC_MCU2_1,
+ IPC_MPU1_0, IPC_MCU1_0, IPC_MCU1_1, IPC_MCU3_0,
IPC_MCU3_0, IPC_MCU3_1, IPC_MCU4_0, IPC_MCU4_1,
IPC_C7X_1, IPC_C7X_2, IPC_C7X_3, IPC_C7X_4,
#endif
@@ -504,8 +504,8 @@ static struct netif netif_ic[ETHAPP_NETIF_IC_MAX_IDX];
static uint32_t netif_ic_state[IC_ETH_MAX_VIRTUAL_IF] =
{
- IC_ETH_IF_MCU2_0_MCU2_1,
- IC_ETH_IF_MCU2_1_MCU2_0,
+ IC_ETH_IF_MCU2_0_MCU3_0,
+ IC_ETH_IF_MCU3_0_MCU2_0,
IC_ETH_IF_MCU2_0_A72
};
@@ -1043,9 +1043,9 @@ static void EthApp_initNetif(void)
NETIF_SET_CHECKSUM_CTRL(&netif, chksumFlags);
#endif
- /* Create inter-core virtual ethernet interface: MCU2_0 <-> MCU2_1 */
- netif_add(&netif_ic[ETHAPP_NETIF_IC_MCU2_0_MCU2_1_IDX], NULL, NULL, NULL,
- (void*)&netif_ic_state[IC_ETH_IF_MCU2_0_MCU2_1],
+ /* Create inter-core virtual ethernet interface: MCU2_0 <-> MCU3_0 */
+ netif_add(&netif_ic[ETHAPP_NETIF_IC_MCU2_0_MCU3_0_IDX], NULL, NULL, NULL,
+ (void*)&netif_ic_state[IC_ETH_IF_MCU2_0_MCU3_0],
LWIPIF_LWIP_IC_init, tcpip_input);
/* Create inter-core virtual ethernet interface: MCU2_0 <-> A72 */
@@ -1066,7 +1066,7 @@ static void EthApp_initNetif(void)
gEthApp_lwipBridgePortIdMap[IPC_MCU2_0] = ETHAPP_BRIDGEIF_CPU_PORT_ID;
bridgeif_add_port(&netif_bridge, &netif_ic[0]);
- gEthApp_lwipBridgePortIdMap[IPC_MCU2_1] = ETHAPP_BRIDGEIF_PORT1_ID;
+ gEthApp_lwipBridgePortIdMap[IPC_MCU3_0] = ETHAPP_BRIDGEIF_PORT1_ID;
bridgeif_add_port(&netif_bridge, &netif_ic[1]);
gEthApp_lwipBridgePortIdMap[IPC_MPU1_0] = ETHAPP_BRIDGEIF_PORT2_ID;
@@ -1087,7 +1087,7 @@ static void EthApp_initNetif(void)
#if defined(ETHAPP_ENABLE_INTERCORE_ETH)
netif_set_up(&netif);
- netif_set_up(&netif_ic[ETHAPP_NETIF_IC_MCU2_0_MCU2_1_IDX]);
+ netif_set_up(&netif_ic[ETHAPP_NETIF_IC_MCU2_0_MCU3_0_IDX]);
netif_set_up(&netif_ic[ETHAPP_NETIF_IC_MCU2_0_A72_IDX]);
netif_set_up(&netif_bridge);
#else
diff --git a/ethfw/apps/common/r5f_mpu_j721e_default.c b/ethfw/apps/common/r5f_mpu_j721e_default.c
index 1a3d40bf..d413e635 100644
--- a/ethfw/apps/common/r5f_mpu_j721e_default.c
+++ b/ethfw/apps/common/r5f_mpu_j721e_default.c
@@ -129,10 +129,10 @@ const CSL_ArmR5MpuRegionCfg gCslR5MpuCfg[CSL_ARM_R5F_MPU_REGIONS_MAX] =
.memAttr = 4U,
},
{
- /* Region 6 configuration: DDR_MCU2_1_IPC_ADDR as non-cache */
+ /* Region 6 configuration: DDR_MCU3_0_IPC_ADDR as non-cache */
.regionId = 6U,
.enable = 1U,
- .baseAddr = 0xA3000000,
+ .baseAddr = 0xA4000000,
.size = CSL_ARM_R5_MPU_REGION_SIZE_1MB,
.subRegionEnable = CSL_ARM_R5_MPU_SUB_REGION_ENABLE_ALL,
.exeNeverControl = 1U,
diff --git a/ethfw/apps/common/r5f_mpu_j721e_safertos.c b/ethfw/apps/common/r5f_mpu_j721e_safertos.c
index d868382a..924b6b6b 100644
--- a/ethfw/apps/common/r5f_mpu_j721e_safertos.c
+++ b/ethfw/apps/common/r5f_mpu_j721e_safertos.c
@@ -153,9 +153,9 @@ xMPU_CONFIG_PARAMETERS gMPUConfigParms[CSL_ARM_R5F_MPU_REGIONS_MAX] =
.ulSubRegionDisable = mpuREGION_ALL_SUB_REGIONS_ENABLED,
},
{
- /* Region 5 configuration: DDR_MCU2_1_IPC */
+ /* Region 5 configuration: DDR_MCU3_0_IPC */
.ulRegionNumber = 5U,
- .ulRegionBeginAddress = 0xA3000000,
+ .ulRegionBeginAddress = 0xA4000000,
{
.ulexeNeverControl = 1U,
.ulaccessPermission = CSL_ARM_R5_ACC_PERM_PRIV_USR_RD_WR,
diff --git a/ethfw/apps/common/r5f_mpu_j784s4_default.c b/ethfw/apps/common/r5f_mpu_j784s4_default.c
index 4bcf4224..c2861235 100644
--- a/ethfw/apps/common/r5f_mpu_j784s4_default.c
+++ b/ethfw/apps/common/r5f_mpu_j784s4_default.c
@@ -129,10 +129,10 @@ const CSL_ArmR5MpuRegionCfg gCslR5MpuCfg[CSL_ARM_R5F_MPU_REGIONS_MAX] =
.memAttr = 4U,
},
{
- /* Region 6 configuration: DDR_MCU2_1_IPC_ADDR as non-cache */
+ /* Region 6 configuration: DDR_MCU3_0_IPC_ADDR as non-cache */
.regionId = 6U,
.enable = 1U,
- .baseAddr = 0xA3000000,
+ .baseAddr = 0xA4000000,
.size = CSL_ARM_R5_MPU_REGION_SIZE_1MB,
.subRegionEnable = CSL_ARM_R5_MPU_SUB_REGION_ENABLE_ALL,
.exeNeverControl = 1U,
diff --git a/ethfw/apps/common/r5f_mpu_j784s4_safertos.c b/ethfw/apps/common/r5f_mpu_j784s4_safertos.c
index d41780d0..c9a2be77 100644
--- a/ethfw/apps/common/r5f_mpu_j784s4_safertos.c
+++ b/ethfw/apps/common/r5f_mpu_j784s4_safertos.c
@@ -153,9 +153,9 @@ xMPU_CONFIG_PARAMETERS gMPUConfigParms[CSL_ARM_R5F_MPU_REGIONS_MAX] =
.ulSubRegionDisable = mpuREGION_ALL_SUB_REGIONS_ENABLED,
},
{
- /* Region 5 configuration: DDR_MCU2_1_IPC */
+ /* Region 5 configuration: DDR_MCU3_0_IPC */
.ulRegionNumber = 5U,
- .ulRegionBeginAddress = 0xA3000000,
+ .ulRegionBeginAddress = 0xA4000000,
{
.ulexeNeverControl = 1U,
.ulaccessPermission = CSL_ARM_R5_ACC_PERM_PRIV_USR_RD_WR,
diff --git a/ethfw/ethfw/src/ethfw.c b/ethfw/ethfw/src/ethfw.c
index 3aa264ed..25756f4e 100644
--- a/ethfw/ethfw/src/ethfw.c
+++ b/ethfw/ethfw/src/ethfw.c
@@ -1063,7 +1063,7 @@ int32_t EthFw_initRemoteConfig(EthFw_Handle hEthFw)
/* Enable server-to-client notify service */
cfg.notifyServiceCpswType = gEthFwObj.enetType;
cfg.notifyServiceRemoteCoreId[0] = IPC_MPU1_0;
- cfg.notifyServiceRemoteCoreId[1] = IPC_MCU2_1;
+ cfg.notifyServiceRemoteCoreId[1] = IPC_MCU3_0;
/* Set CPSW Proxy shared multicast config.
* All parameters have already been checked. */
diff --git a/ethfw/ethfw_build_flags.mak b/ethfw/ethfw_build_flags.mak
index 3b7f3ff5..de01c222 100644
--- a/ethfw/ethfw_build_flags.mak
+++ b/ethfw/ethfw_build_flags.mak
@@ -14,12 +14,12 @@ BUILD_EMULATION_ARCH?=x86_64
BUILD_CPU_MPU1?=no
BUILD_CPU_MCU1_0?=no
BUILD_CPU_MCU2_0?=yes
-BUILD_CPU_MCU3_0?=no
+BUILD_CPU_MCU3_0?=yes
BUILD_CPU_C6x_1?=no
BUILD_CPU_C6x_2?=no
BUILD_CPU_C7x_1?=no
BUILD_CPU_MCU1_1?=no
-BUILD_CPU_MCU2_1?=yes
+BUILD_CPU_MCU2_1?=no
BUILD_CPU_MCU3_1?=no
BUILD_SOC_LIST ?= J721E J7200 J784S4
export BUILD_SOC_LIST
diff --git a/ethfw/ethremotecfg/client/src/cpsw_proxy.c b/ethfw/ethremotecfg/client/src/cpsw_proxy.c
index 057a10a9..59bfc3b6 100644
--- a/ethfw/ethremotecfg/client/src/cpsw_proxy.c
+++ b/ethfw/ethremotecfg/client/src/cpsw_proxy.c
@@ -1186,7 +1186,7 @@ static void CpswProxy_remoteDeviceInit(uint32_t masterCoreId,
#ifdef QNX_OS
System_printf("Remote device (core : mpu1_0) .....\r\n");
#else
- System_printf("Remote device (core : mcu2_1) .....\r\n");
+ System_printf("Remote device (core : mcu3_0) .....\r\n");
#endif
}
diff --git a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/enet_component.mk b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/enet_component.mk
index 848dc4cf..cd1d34fe 100644
--- a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/enet_component.mk
+++ b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/enet_component.mk
@@ -42,10 +42,10 @@ drvenet_RTOS_LIST = $(DEFAULT_RTOS_LIST)
drvenet_SOCLIST = am65xx j721e j7200 j721s2 j784s4
drvenet_BOARDLIST = am65xx_evm am65xx_idk j721e_evm j7200_evm j721s2_evm j784s4_evm
drvenet_am65xx_CORELIST = mpu1_0 mcu1_0
-drvenet_j721e_CORELIST = mpu1_0 mcu1_0 mcu2_0 mcu2_1
+drvenet_j721e_CORELIST = mpu1_0 mcu1_0 mcu2_0 mcu2_1 mcu3_0
drvenet_j7200_CORELIST = mpu1_0 mcu1_0 mcu2_0 mcu2_1
drvenet_j721s2_CORELIST = mpu1_0 mcu1_0 mcu2_0 mcu2_1
-drvenet_j784s4_CORELIST = mpu1_0 mcu1_0 mcu2_0 mcu2_1
+drvenet_j784s4_CORELIST = mpu1_0 mcu1_0 mcu2_0 mcu2_1 mcu3_0
# Temp SoC/board lists which excludes for libraries/apps which
# are not enabled yet
diff --git a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_ipc.h b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_ipc.h
index a1aeb290..7c577f6c 100644
--- a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_ipc.h
+++ b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_ipc.h
@@ -64,7 +64,7 @@ extern "C" {
#define ICETH_IPC_ENDPT_BASE 10
#define ICETH_IPC_ENDPT_MCU2_0_R5 (ICETH_IPC_ENDPT_BASE + 1)
#define ICETH_IPC_ENDPT_MCU2_0_A72 (ICETH_IPC_ENDPT_BASE + 2)
-#define ICETH_IPC_ENDPT_MCU2_1 (ICETH_IPC_ENDPT_BASE + 3)
+#define ICETH_IPC_ENDPT_MCU3_0 (ICETH_IPC_ENDPT_BASE + 3)
#define ICETH_IPC_ENDPT_MAX (ICETH_IPC_ENDPT_BASE + 4)
#define ICETH_ENDPT_NAME_LEN_MAX 128
diff --git a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_queue.h b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_queue.h
index 401ad6ba..4ca793ce 100644
--- a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_queue.h
+++ b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/intercore/include/ic_queue.h
@@ -66,10 +66,10 @@ extern "C" {
/*! Maximum no. of IcQ_Node objects in a queue */
#define ICQ_MAX_QUEUE_SIZE (2048)
-/*! MCU2_0 to MCU2_1 TX queue */
-#define ICQ_MCU2_0_TO_MCU2_1 (0U)
-/*! MCU2_1 to MCU2_0 TX queue */
-#define ICQ_MCU2_1_TO_MCU2_0 (1U)
+/*! MCU2_0 to MCU3_0 TX queue */
+#define ICQ_MCU2_0_TO_MCU3_0 (0U)
+/*! MCU3_0 to MCU2_0 TX queue */
+#define ICQ_MCU3_0_TO_MCU2_0 (1U)
/*! MCU2_0 to A72 TX queue */
#define ICQ_MCU2_0_TO_A72 (2U)
/*! A72 to MCU2_0 TX queue */
diff --git a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/bufpool.h b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/bufpool.h
index 064c213a..a6a95cd2 100644
--- a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/bufpool.h
+++ b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/bufpool.h
@@ -64,10 +64,10 @@ extern "C" {
/*! Total size of the Ethernet frame in bytes */
#define ETH_FRAME_SIZE (ETH_MAX_PAYLOAD + VLAN_TAG_SIZE)
-/*! MCU2_0 buffer pool for MCU2_0->MCU2_1 interface */
+/*! MCU2_0 buffer pool for MCU2_0->MCU3_0 interface */
#define BUFPOOL_MCU2_0_R5 (0)
-/*! MCU2_1 buffer pool */
-#define BUFPOOL_MCU2_1 (1)
+/*! MCU3_0 buffer pool */
+#define BUFPOOL_MCU3_0 (1)
/*! A72 buffer pool */
#define BUFPOOL_A72 (2)
/*! MCU2_0 buffer pool for MCU2_0->A72 interface */
diff --git a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/lwip2enet_ic.h b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/lwip2enet_ic.h
index 30c341d1..a2a34d82 100755
--- a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/lwip2enet_ic.h
+++ b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/inc/lwip2enet_ic.h
@@ -69,12 +69,12 @@ extern "C" {
/* Macros */
/* ========================================================================== */
-/*! Inter-core virtual driver object instance ID: MCU2_0->MCU2_1
- * This instance is created on MCU2_0 to interface with MCU2_1 */
-#define IC_ETH_IF_MCU2_0_MCU2_1 0
-/*! Inter-core virtual driver object instance ID: MCU2_0->MCU2_1
- * This instance is created on MCU2_1 to interface with MCU2_0 */
-#define IC_ETH_IF_MCU2_1_MCU2_0 1
+/*! Inter-core virtual driver object instance ID: MCU2_0->MCU3_0
+ * This instance is created on MCU2_0 to interface with MCU3_0 */
+#define IC_ETH_IF_MCU2_0_MCU3_0 0
+/*! Inter-core virtual driver object instance ID: MCU2_0->MCU3_0
+ * This instance is created on MCU3_0 to interface with MCU2_0 */
+#define IC_ETH_IF_MCU3_0_MCU2_0 1
/*! Inter-core virtual driver object instance ID: MCU2_0->A72
* This instance is created on MCU2_0 to interface with A72
*
diff --git a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/src/lwip2enet_ic.c b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/src/lwip2enet_ic.c
index fc18a09e..4c59c1cf 100755
--- a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/src/lwip2enet_ic.c
+++ b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/lwipific/src/lwip2enet_ic.c
@@ -102,26 +102,26 @@ Lwip2EnetIc_Object gLwip2EnetIcObj[IC_ETH_MAX_VIRTUAL_IF];
Lwip2EnetIc_Params gIcEnetParams[IC_ETH_MAX_VIRTUAL_IF]=
{
{
- .instId = IC_ETH_IF_MCU2_0_MCU2_1,
+ .instId = IC_ETH_IF_MCU2_0_MCU3_0,
.ownerId = IPC_MCU2_0,
- .txQId = ICQ_MCU2_0_TO_MCU2_1,
- .rxQId = ICQ_MCU2_1_TO_MCU2_0,
+ .txQId = ICQ_MCU2_0_TO_MCU3_0,
+ .rxQId = ICQ_MCU3_0_TO_MCU2_0,
.bufPoolId = BUFPOOL_MCU2_0_R5,
.reqEndPtId = ICETH_IPC_ENDPT_MCU2_0_R5,
- .remoteCoreId = IPC_MCU2_1,
+ .remoteCoreId = IPC_MCU3_0,
.endPtName = "ENDPT_ICETH_MCU2_0_R5",
- .remoteEndPtName = "ENDPT_ICETH_MCU2_1",
+ .remoteEndPtName = "ENDPT_ICETH_MCU3_0",
.macAddr = {0x00,0x01,0x02,0x03,0x04,0x05},
},
{
- .instId = IC_ETH_IF_MCU2_1_MCU2_0,
+ .instId = IC_ETH_IF_MCU3_0_MCU2_0,
.ownerId = IPC_MCU2_0,
- .txQId = ICQ_MCU2_1_TO_MCU2_0,
- .rxQId = ICQ_MCU2_0_TO_MCU2_1,
- .bufPoolId = BUFPOOL_MCU2_1,
- .reqEndPtId = ICETH_IPC_ENDPT_MCU2_1,
+ .txQId = ICQ_MCU3_0_TO_MCU2_0,
+ .rxQId = ICQ_MCU2_0_TO_MCU3_0,
+ .bufPoolId = BUFPOOL_MCU3_0,
+ .reqEndPtId = ICETH_IPC_ENDPT_MCU3_0,
.remoteCoreId = IPC_MCU2_0,
- .endPtName = "ENDPT_ICETH_MCU2_1",
+ .endPtName = "ENDPT_ICETH_MCU3_0",
.remoteEndPtName = "ENDPT_ICETH_MCU2_0_R5",
.macAddr = {0x00,0x01,0x02,0x04,0x05,0x06},
},
@@ -181,9 +181,9 @@ Lwip2EnetIc_Handle Lwip2EnetIc_open(uint32_t instId)
hIcObj->selfCoreId = EnetSoc_getCoreId();
- /* Only MCU2_0 and MCU2_1 supported for now */
+ /* Only MCU2_0 and MCU3_0 supported for now */
Lwip2EnetIc_assert( (hIcObj->selfCoreId == IPC_MCU2_0) ||
- (hIcObj->selfCoreId == IPC_MCU2_1) );
+ (hIcObj->selfCoreId == IPC_MCU3_0) );
hIcObj->remoteCoreId = gIcEnetParams[instId].remoteCoreId;
hIcObj->txQId = gIcEnetParams[instId].txQId;
diff --git a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/soc/j7x/j721e/enet_soc.c b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/soc/j7x/j721e/enet_soc.c
index ac05a59b..8386bf9f 100644
--- a/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/soc/j7x/j721e/enet_soc.c
+++ b/pdk_jacinto_08_06_00_31/packages/ti/drv/enet/soc/j7x/j721e/enet_soc.c
@@ -449,6 +449,22 @@ CpswSoc_Cfg gEnetSoc_cpsw9gSocCfg =
.coreIntNum = CSLR_R5FSS0_CORE1_INTR_CPSW0_MDIO_PEND_0,
.srcIdx = ENET_SOC_DIRECT_INTR_SRCIDX_INVALID,
},
+#elif defined(BUILD_MCU3_0)
+ { /* EVNT_PEND - Event pending interrupt (CPTS) */
+ .intrId = CPSW_INTR_EVNT_PEND,
+ .coreIntNum = CSLR_R5FSS1_CORE0_INTR_CPSW0_EVNT_PEND_0,
+ .srcIdx = ENET_SOC_DIRECT_INTR_SRCIDX_INVALID,
+ },
+ { /* STATS_PEND - Statistics pending interrupt */
+ .intrId = CPSW_INTR_STATS_PEND0,
+ .coreIntNum = CSLR_R5FSS1_CORE0_INTR_CPSW0_STAT_PEND_0,
+ .srcIdx = ENET_SOC_DIRECT_INTR_SRCIDX_INVALID,
+ },
+ { /* MDIO_PEND - MDIO interrupt */
+ .intrId = CPSW_INTR_MDIO_PEND,
+ .coreIntNum = CSLR_R5FSS1_CORE0_INTR_CPSW0_MDIO_PEND_0,
+ .srcIdx = ENET_SOC_DIRECT_INTR_SRCIDX_INVALID,
+ },
#elif defined(BUILD_MPU1_0)
{ /* EVNT_PEND - Event pending interrupt (CPTS) */
.intrId = CPSW_INTR_EVNT_PEND,
@@ -1015,6 +1031,8 @@ uint32_t EnetSoc_getCoreId(void)
coreId = IPC_MCU2_0;
#elif defined(BUILD_MCU2_1)
coreId = IPC_MCU2_1;
+#elif defined(BUILD_MCU3_0)
+ coreId = IPC_MCU3_0;
#else
#error "Enet J721E SOC: Core not supported!!"
#endif
@@ -1628,6 +1646,8 @@ static uint32_t EnetSoc_getCoreDevId(void)
coreDevId = TISCI_DEV_R5FSS0_CORE0;
#elif defined(BUILD_MCU2_1)
coreDevId = TISCI_DEV_R5FSS0_CORE1;
+#elif defined(BUILD_MCU3_0)
+ coreDevId = TISCI_DEV_R5FSS1_CORE0;
#else
#error "Enet J721E SOC: Core not supported!!"
#endif
@@ -1685,7 +1705,7 @@ int32_t EnetSoc_mapPort2QsgmiiId(Enet_Type enetType,
/* Translate portNum to QSGMII Id.
* In QSGMII mode, first QSGMII main port used is QSGMII ID 0 and next QSGMII ID 1.
- * For example – if MAC port 0 and port 3 are configured in QSGMII mode. Port 0 is QSMII 0
+ * For example <96> if MAC port 0 and port 3 are configured in QSGMII mode. Port 0 is QSMII 0
* and 3 QSGMII1. Software is transparent to this selection */
status = EnetSoc_getQsgmiiCfg(enetType, instId,
--
2.17.1