Part Number: TDA4VL-Q1
What are the changes required to be done in the Linux SDK support a DDR of size 4GB?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VL-Q1
What are the changes required to be done in the Linux SDK support a DDR of size 4GB?
The SDK offering for J721s2 currently supports 16GB DDR.
In order to make the SDK compatible to a 4GB DDR, please apply the below patch in ${PSDKLA}/board-support/u-boot-2021.01+gitAUTOINC+62a9e51344-g62a9e51344
/cfs-file/__key/communityserver-discussions-components-files/791/1323.DDR_5F00_4GB_5F00_Uboot.patch
Note:
1. The above patch is created on SDK 8.6.
2. Changes regarding the reduction in the DDR instance happens only in the u-boot.
After applying this patch, build the u-boot binaries and copy the same to the boot partition as shown below:
cd ${PSDKLA}
make u-boot_clean
make u-boot
sudo cp board-support/k3-image-gen-2022.01/tiboot3.bin /media/nikhil/BOOT/tiboot3.bin
sudo cp board-support/u-boot_build/a72/tispl.bin /media/nikhil/BOOT/tispl.bin
sudo cp board-support/u-boot_build/a72/u-boot.img /media/nikhil/BOOT/u-boot.img
Verification:
Check the u-boot logs as shown below
U-Boot 2021.01-00002-g7f1139c55f
(Apr 26 2023 - 15:38:23 +0530)
SoC: J721S2 SR1.0 GP
Model: Texas Instruments J721S2 EVM
Board: J721S2X-PM1-SOM rev E1
DRAM: 4 GiB
Flash: 0 Bytes
MMC: mmc@4f80000: 0, mmc@4fb0000: 1
In: serial@2880000
Regards,
Nikhil