Part Number: TDA4VM
Other Parts Discussed in Thread: DRA829, , TDA4VL, AM68, TDA4VH, AM69
What are the changes required to be done to JACINTO SDK in order to make it compatible for device variants
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Abstract
Jacinto7 TDA4 family consists of a large number of variants in its SoCs based on the usecase and applications.
The SDK for each family provides support for the superset device –
The SDK “out of the box” provides support for the a) fastest speed grades, and b) full feature set of the SoC.
For a given end application, it is the responsibility of the user to modify the SDK to configure the device in a way that matches the end application requirements and in a way that only takes advantage of the features/speeds that are available for the specific part number.
For example,
This FAQ highlights areas where a user may need to customize the SDK – either to save power for functions that aren’t needed in a given application (even if available for a part number) or where there are such differences between the devices in the SoC family and changes are required on the SDK to make the software offering compatible to these subset devices.
This would ease the process of SDK integration at customer's end.
Comparing the devices, below are the few differences/ modifications observed among the devices.
NOTE: The below mentioned changes are directly applicable on RTOS and LINUX SDK 8.6. For the other SDKs, please make the adaptations by referring the below changes.
1. Reduction in the number of DDR Instances
Some of the subset devices of J721s2 such as TDA4AL88, TDA4VL21 etc has only 1 DDR instance as compared to its superset device (which has 2). Hence the below modification shall be made in-order to make SDK compatible for 1 DDR instance.
Note: Changes regarding the reduction in the DDR instance happens only in the u-boot. Only a slight modification required on vision_apps
Boot tested on J721s2-EVM.
---
diff --git a/arch/arm/dts/k3-j721s2-ddr-evm-lp4-4266.dtsi b/arch/arm/dts/k3-j721s2-ddr-evm-lp4-4266.dtsi
index c91576bf09..8fbe202c75 100644
--- a/arch/arm/dts/k3-j721s2-ddr-evm-lp4-4266.dtsi
+++ b/arch/arm/dts/k3-j721s2-ddr-evm-lp4-4266.dtsi
@@ -14,7 +14,7 @@
#define MULTI_DDR_CFG_INTRLV_SIZE 11
#define MULTI_DDR_CFG_ECC_ENABLE 0
#define MULTI_DDR_CFG_HYBRID_SELECT 0
-#define MULTI_DDR_CFG_EMIFS_ACTIVE 3
+#define MULTI_DDR_CFG_EMIFS_ACTIVE 1
#define DDRSS0_CTL_00_DATA 0x00000B00
#define DDRSS0_CTL_01_DATA 0x00000000
diff --git a/arch/arm/dts/k3-j721s2-ddr.dtsi b/arch/arm/dts/k3-j721s2-ddr.dtsi
index 6a244fb7ac..7dabc2999b 100644
--- a/arch/arm/dts/k3-j721s2-ddr.dtsi
+++ b/arch/arm/dts/k3-j721s2-ddr.dtsi
@@ -2230,6 +2230,7 @@
};
memorycontroller1: memorycontroller@29b0000 {
+ status = "disabled";
compatible = "ti,j721s2-ddrss";
reg = <0x0 0x029b0000 0x0 0x4000>,
<0x0 0x0114000 0x0 0x100>;
diff --git a/arch/arm/dts/k3-j721s2-som-p0.dtsi b/arch/arm/dts/k3-j721s2-som-p0.dtsi
index f3080e948e..9e91110d90 100644
--- a/arch/arm/dts/k3-j721s2-som-p0.dtsi
+++ b/arch/arm/dts/k3-j721s2-som-p0.dtsi
@@ -13,9 +13,9 @@
/ {
memory@80000000 {
device_type = "memory";
- /* 16 GB RAM */
+ /* 8 GB RAM */
reg = <0x00 0x80000000 0x00 0x80000000>,
- <0x08 0x80000000 0x03 0x80000000>;
+ <0x08 0x80000000 0x01 0x80000000>;
};
/* Reserving memory regions still pending */
diff --git a/board/ti/j721s2/evm.c b/board/ti/j721s2/evm.c
index 90b7ca1150..51e50fa9c5 100644
--- a/board/ti/j721s2/evm.c
+++ b/board/ti/j721s2/evm.c
@@ -67,8 +67,8 @@ int dram_init_banksize(void)
#ifdef CONFIG_PHYS_64BIT
/* Bank 1 declares the memory available in the DDR high region */
gd->bd->bi_dram[1].start = CONFIG_SYS_SDRAM_BASE1;
- gd->bd->bi_dram[1].size = 0x37fffffff;
- gd->ram_size = 0x400000000;
+ gd->bd->bi_dram[1].size = 0x17fffffff;
+ gd->ram_size = 0x200000000;
#endif
return 0;
--
2.17.1
diff --git a/utils/perf_stats/src/app_perf_stats_freertos.c b/utils/perf_stats/src/app_perf_stats_freertos.c
index 2c63699..cd6805a 100644
--- a/utils/perf_stats/src/app_perf_stats_freertos.c
+++ b/utils/perf_stats/src/app_perf_stats_freertos.c
@@ -88,7 +88,7 @@
#if defined(SOC_J721E) || defined(SOC_AM62A)
#define APP_PERF_NUM_DDR_INSTANCES (1u)
#elif defined (SOC_J721S2)
-#define APP_PERF_NUM_DDR_INSTANCES (2u)
+#define APP_PERF_NUM_DDR_INSTANCES (1u)
#elif defined (SOC_J784S4)
#define APP_PERF_NUM_DDR_INSTANCES (4u)
#endif
@@ -631,7 +631,7 @@ void appPerfStatsDdrStatsReadCounters(uint32_t *val0, uint32_t *val1, uint32_t *
cnt3[0] = (volatile uint32_t *)0x02980110;
#endif
- #if defined(SOC_J721S2) || defined(SOC_J784S4)
+ #if defined(SOC_J784S4)
cnt_sel[1] = (volatile uint32_t *)0x029A0100;
cnt0[1] = (volatile uint32_t *)0x029A0104;
cnt1[1] = (volatile uint32_t *)0x029A0108;
Verification:
Check the u-boot logs as shown below
U-Boot 2021.01-00002-g7f1139c55f
(Apr 26 2023 - 15:38:23 +0530)
SoC: J721S2 SR1.0 GP
Model: Texas Instruments J721S2 EVM
Board: J721S2X-PM1-SOM rev E1
DRAM: 8 GiB
Flash: 0 Bytes
MMC: mmc@4f80000: 0, mmc@4fb0000: 1
In: serial@2880000
2. Change in the clock frequency for the core based on the speed grade or power optimization
Based on the speed grades/ power optimization, there would be changes in the clock frequencies at which the cores would run. One such example is shown in the below table for speed grade T, N and H for J721s2

To change the clock frequency associated with a core, follow the below steps.
1. Identify the clock source/ PLL and the divider associated with that core from the TRM (Clocking Section) of the superset device.
2. Based on the PLL, modify the divider such that the final output clock is as per the speed grade.
Below is an example of how to change the clock for C7x core for TDA4VL21. The PLL is identified to be MAIN_PLL7 HSDIV0.
The changes done are as below.
diff --git a/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c b/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c
index 2122081..7438db5 100644
--- a/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c
+++ b/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c
@@ -5160,7 +5160,7 @@ static const struct clk_data_div_reg clk_data_hsdiv0_16fft_main_6_hsdiv0 = {
static const struct clk_data_div_reg clk_data_hsdiv0_16fft_main_7_hsdiv0 = {
.data_div = {
.n = 128,
- .default_div = 2,
+ .default_div = 4,
},
.reg = 0x00680000UL + (0x1000UL * 7UL) + 0x80UL + (0x4UL * 0UL),
.bit = 0,Here the clock is reduced from 1GHz to 500MHz for C7x core.
The similar could be done for other cores / HWA as per the combination of speed grades and power optimizations.
Verification Command:
k3conf dump clock 8
k3conf dump clock 11
Output:
The C7x cores clock value is 500MHz.
|-----------------------------------------------------------------------------------------------------------------------| | Device ID | Clock ID | Clock Name | Status | Clock Frequency | |-----------------------------------------------------------------------------------------------------------------------| | 8 | 0 | DEV_COMPUTE_CLUSTER0_C71SS0_0_C7X_CLK | CLK_STATE_READY | 500000000 | | 8 | 1 | DEV_COMPUTE_CLUSTER0_C71SS0_0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 | | 8 | 3 | DEV_COMPUTE_CLUSTER0_C71SS0_0_C7X_DIVH_CLK4_OBSCLK_OUT_CLK | CLK_STATE_READY | 0 | |-----------------------------------------------------------------------------------------------------------------------| |-------------------------------------------------------------------------------------------------------| | Device ID | Clock ID | Clock Name | Status | Clock Frequency | |-------------------------------------------------------------------------------------------------------| | 11 | 0 | DEV_COMPUTE_CLUSTER0_C71SS1_0_C7X_CLK | CLK_STATE_READY | 500000000 | | 11 | 1 | DEV_COMPUTE_CLUSTER0_C71SS1_0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 | |-------------------------------------------------------------------------------------------------------|
3. Disabling/removing the additional cores
Subsets such as TDA4AL88 and TDA4VL21 are quad core R5 devices as compared to it superset which is a hexa core device. There are other subsets where there is only 1 C7x core available.
The changes for the same are required in u-boot, linux and vision_apps.
For example, removal of MCU3_0 (or) main_r5fss1 can be done as shown below
diff --git a/arch/arm/dts/k3-j721s2-common-proc-board.dts b/arch/arm/dts/k3-j721s2-common-proc-board.dts
index 5b7e33490f..ffd9c8568b 100644
--- a/arch/arm/dts/k3-j721s2-common-proc-board.dts
+++ b/arch/arm/dts/k3-j721s2-common-proc-board.dts
@@ -32,8 +32,6 @@
remoteproc1 = &mcu_r5fss0_core1;
remoteproc2 = &main_r5fss0_core0;
remoteproc3 = &main_r5fss0_core1;
- remoteproc4 = &main_r5fss1_core0;
- remoteproc5 = &main_r5fss1_core1;
remoteproc6 = &c71_0;
remoteproc7 = &c71_1;
};
diff --git a/arch/arm/dts/k3-j721s2-main.dtsi b/arch/arm/dts/k3-j721s2-main.dtsi
index 18e5113336..d9bf23b1e9 100644
--- a/arch/arm/dts/k3-j721s2-main.dtsi
+++ b/arch/arm/dts/k3-j721s2-main.dtsi
@@ -1152,46 +1152,6 @@
};
};
- main_r5fss1: r5fss@5e00000 {
- compatible = "ti,j721s2-r5fss";
- ti,cluster-mode = <0>;
- #address-cells = <1>;
- #size-cells = <1>;
- ranges = <0x5e00000 0x00 0x5e00000 0x20000>,
- <0x5f00000 0x00 0x5f00000 0x20000>;
- power-domains = <&k3_pds 278 TI_SCI_PD_EXCLUSIVE>;
-
- main_r5fss1_core0: r5f@5e00000 {
- compatible = "ti,j721s2-r5f";
- reg = <0x5e00000 0x00010000>,
- <0x5e10000 0x00010000>;
- reg-names = "atcm", "btcm";
- ti,sci = <&sms>;
- ti,sci-dev-id = <281>;
- ti,sci-proc-ids = <0x08 0xff>;
- resets = <&k3_reset 281 1>;
- firmware-name = "j721s2-main-r5f1_0-fw";
- ti,atcm-enable = <1>;
- ti,btcm-enable = <1>;
- ti,loczrama = <1>;
- };
-
- main_r5fss1_core1: r5f@5f00000 {
- compatible = "ti,j721s2-r5f";
- reg = <0x5f00000 0x00010000>,
- <0x5f10000 0x00010000>;
- reg-names = "atcm", "btcm";
- ti,sci = <&sms>;
- ti,sci-dev-id = <282>;
- ti,sci-proc-ids = <0x09 0xff>;
- resets = <&k3_reset 282 1>;
- firmware-name = "j721s2-main-r5f1_1-fw";
- ti,atcm-enable = <1>;
- ti,btcm-enable = <1>;
- ti,loczrama = <1>;
- };
- };
-
c71_0: dsp@64800000 {
compatible = "ti,j721s2-c71-dsp";
reg = <0x00 0x64800000 0x00 0x00080000>,
diff --git a/arch/arm/dts/k3-j721s2-som-p0.dtsi b/arch/arm/dts/k3-j721s2-som-p0.dtsi
index f3080e948e..c4df1d51bd 100644
--- a/arch/arm/dts/k3-j721s2-som-p0.dtsi
+++ b/arch/arm/dts/k3-j721s2-som-p0.dtsi
@@ -78,30 +78,6 @@
no-map;
};
- main_r5fss1_core0_dma_memory_region: r5f-dma-memory@a4000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa4000000 0x00 0x100000>;
- no-map;
- };
-
- main_r5fss1_core0_memory_region: r5f-memory@a4100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa4100000 0x00 0xf00000>;
- no-map;
- };
-
- main_r5fss1_core1_dma_memory_region: r5f-dma-memory@a5000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa5000000 0x00 0x100000>;
- no-map;
- };
-
- main_r5fss1_core1_memory_region: r5f-memory@a5100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa5100000 0x00 0xf00000>;
- no-map;
- };
-
c71_0_dma_memory_region: c71-dma-memory@a6000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa6000000 0x00 0x100000>;
@@ -251,17 +227,7 @@
};
&mailbox0_cluster2 {
- interrupts = <428>;
-
- mbox_main_r5fss1_core0: mbox-main-r5fss1-core0 {
- ti,mbox-rx = <0 0 0>;
- ti,mbox-tx = <1 0 0>;
- };
-
- mbox_main_r5fss1_core1: mbox-main-r5fss1-core1 {
- ti,mbox-rx = <2 0 0>;
- ti,mbox-tx = <3 0 0>;
- };
+ status = "disabled";
};
&mailbox0_cluster3 {
@@ -382,18 +348,6 @@
<&main_r5fss0_core1_memory_region>;
};
-&main_r5fss1_core0 {
- mboxes = <&mailbox0_cluster2 &mbox_main_r5fss1_core0>;
- memory-region = <&main_r5fss1_core0_dma_memory_region>,
- <&main_r5fss1_core0_memory_region>;
-};
-
-&main_r5fss1_core1 {
- mboxes = <&mailbox0_cluster2 &mbox_main_r5fss1_core1>;
- memory-region = <&main_r5fss1_core1_dma_memory_region>,
- <&main_r5fss1_core1_memory_region>;
-};
-
&c71_0 {
mboxes = <&mailbox0_cluster4 &mbox_c71_0>;
memory-region = <&c71_0_dma_memory_region>,
diff --git a/arch/arm/dts/k3-j721s2-common-proc-board.dts b/arch/arm/dts/k3-j721s2-common-proc-board.dts
index 5b7e33490f..ffd9c8568b 100644
--- a/arch/arm/dts/k3-j721s2-common-proc-board.dts
+++ b/arch/arm/dts/k3-j721s2-common-proc-board.dts
@@ -32,8 +32,6 @@
remoteproc1 = &mcu_r5fss0_core1;
remoteproc2 = &main_r5fss0_core0;
remoteproc3 = &main_r5fss0_core1;
- remoteproc4 = &main_r5fss1_core0;
- remoteproc5 = &main_r5fss1_core1;
remoteproc6 = &c71_0;
remoteproc7 = &c71_1;
};
diff --git a/arch/arm/dts/k3-j721s2-main.dtsi b/arch/arm/dts/k3-j721s2-main.dtsi
index 18e5113336..d9bf23b1e9 100644
--- a/arch/arm/dts/k3-j721s2-main.dtsi
+++ b/arch/arm/dts/k3-j721s2-main.dtsi
@@ -1152,46 +1152,6 @@
};
};
- main_r5fss1: r5fss@5e00000 {
- compatible = "ti,j721s2-r5fss";
- ti,cluster-mode = <0>;
- #address-cells = <1>;
- #size-cells = <1>;
- ranges = <0x5e00000 0x00 0x5e00000 0x20000>,
- <0x5f00000 0x00 0x5f00000 0x20000>;
- power-domains = <&k3_pds 278 TI_SCI_PD_EXCLUSIVE>;
-
- main_r5fss1_core0: r5f@5e00000 {
- compatible = "ti,j721s2-r5f";
- reg = <0x5e00000 0x00010000>,
- <0x5e10000 0x00010000>;
- reg-names = "atcm", "btcm";
- ti,sci = <&sms>;
- ti,sci-dev-id = <281>;
- ti,sci-proc-ids = <0x08 0xff>;
- resets = <&k3_reset 281 1>;
- firmware-name = "j721s2-main-r5f1_0-fw";
- ti,atcm-enable = <1>;
- ti,btcm-enable = <1>;
- ti,loczrama = <1>;
- };
-
- main_r5fss1_core1: r5f@5f00000 {
- compatible = "ti,j721s2-r5f";
- reg = <0x5f00000 0x00010000>,
- <0x5f10000 0x00010000>;
- reg-names = "atcm", "btcm";
- ti,sci = <&sms>;
- ti,sci-dev-id = <282>;
- ti,sci-proc-ids = <0x09 0xff>;
- resets = <&k3_reset 282 1>;
- firmware-name = "j721s2-main-r5f1_1-fw";
- ti,atcm-enable = <1>;
- ti,btcm-enable = <1>;
- ti,loczrama = <1>;
- };
- };
-
c71_0: dsp@64800000 {
compatible = "ti,j721s2-c71-dsp";
reg = <0x00 0x64800000 0x00 0x00080000>,
diff --git a/arch/arm/dts/k3-j721s2-som-p0.dtsi b/arch/arm/dts/k3-j721s2-som-p0.dtsi
index f3080e948e..c4df1d51bd 100644
--- a/arch/arm/dts/k3-j721s2-som-p0.dtsi
+++ b/arch/arm/dts/k3-j721s2-som-p0.dtsi
@@ -78,30 +78,6 @@
no-map;
};
- main_r5fss1_core0_dma_memory_region: r5f-dma-memory@a4000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa4000000 0x00 0x100000>;
- no-map;
- };
-
- main_r5fss1_core0_memory_region: r5f-memory@a4100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa4100000 0x00 0xf00000>;
- no-map;
- };
-
- main_r5fss1_core1_dma_memory_region: r5f-dma-memory@a5000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa5000000 0x00 0x100000>;
- no-map;
- };
-
- main_r5fss1_core1_memory_region: r5f-memory@a5100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa5100000 0x00 0xf00000>;
- no-map;
- };
-
c71_0_dma_memory_region: c71-dma-memory@a6000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa6000000 0x00 0x100000>;
@@ -251,17 +227,7 @@
};
&mailbox0_cluster2 {
- interrupts = <428>;
-
- mbox_main_r5fss1_core0: mbox-main-r5fss1-core0 {
- ti,mbox-rx = <0 0 0>;
- ti,mbox-tx = <1 0 0>;
- };
-
- mbox_main_r5fss1_core1: mbox-main-r5fss1-core1 {
- ti,mbox-rx = <2 0 0>;
- ti,mbox-tx = <3 0 0>;
- };
+ status = "disabled";
};
&mailbox0_cluster3 {
@@ -382,18 +348,6 @@
<&main_r5fss0_core1_memory_region>;
};
-&main_r5fss1_core0 {
- mboxes = <&mailbox0_cluster2 &mbox_main_r5fss1_core0>;
- memory-region = <&main_r5fss1_core0_dma_memory_region>,
- <&main_r5fss1_core0_memory_region>;
-};
-
-&main_r5fss1_core1 {
- mboxes = <&mailbox0_cluster2 &mbox_main_r5fss1_core1>;
- memory-region = <&main_r5fss1_core1_dma_memory_region>,
- <&main_r5fss1_core1_memory_region>;
-};
-
&c71_0 {
mboxes = <&mailbox0_cluster4 &mbox_c71_0>;
memory-region = <&c71_0_dma_memory_region>,
diff --git a/platform/j721s2/rtos/app_mem_map.h b/platform/j721s2/rtos/app_mem_map.h
index 4f1c7f6..e562580 100755
--- a/platform/j721s2/rtos/app_mem_map.h
+++ b/platform/j721s2/rtos/app_mem_map.h
@@ -127,22 +127,6 @@
#define DDR_MCU2_1_DTS_ADDR (0xA4100000u)
#define DDR_MCU2_1_DTS_SIZE (0x01F00000u)
-/* DDR for MCU3_0 for Linux IPC [ size 1024.00 KB ] */
-#define DDR_MCU3_0_IPC_ADDR (0xA6000000u)
-#define DDR_MCU3_0_IPC_SIZE (0x00100000u)
-
-/* DDR for MCU3_0 for all sections, used for reserving memory in DTS file [ size 15.00 MB ] */
-#define DDR_MCU3_0_DTS_ADDR (0xA6100000u)
-#define DDR_MCU3_0_DTS_SIZE (0x00F00000u)
-
-/* DDR for MCU3_1 for Linux IPC [ size 1024.00 KB ] */
-#define DDR_MCU3_1_IPC_ADDR (0xA7000000u)
-#define DDR_MCU3_1_IPC_SIZE (0x00100000u)
-
-/* DDR for MCU3_1 for all sections, used for reserving memory in DTS file [ size 15.00 MB ] */
-#define DDR_MCU3_1_DTS_ADDR (0xA7100000u)
-#define DDR_MCU3_1_DTS_SIZE (0x00F00000u)
-
/* Memory for IPC Vring's. MUST be non-cached or cache-coherent [ size 32.00 MB ] */
#define IPC_VRING_MEM_ADDR (0xA8000000u)
#define IPC_VRING_MEM_SIZE (0x02000000u)
@@ -195,14 +179,6 @@
#define DDR_MCU2_1_LOCAL_HEAP_ADDR (0xDA000000u)
#define DDR_MCU2_1_LOCAL_HEAP_SIZE (0x01000000u)
-/* DDR for MCU3_0 for local heap [ size 8.00 MB ] */
-#define DDR_MCU3_0_LOCAL_HEAP_ADDR (0xDB000000u)
-#define DDR_MCU3_0_LOCAL_HEAP_SIZE (0x00800000u)
-
-/* DDR for MCU3_1 for local heap [ size 8.00 MB ] */
-#define DDR_MCU3_1_LOCAL_HEAP_ADDR (0xDB800000u)
-#define DDR_MCU3_1_LOCAL_HEAP_SIZE (0x00800000u)
-
/* DDR for c7x_1 for Scratch Memory [ size 368.00 MB ] */
#define DDR_C7X_1_SCRATCH_ADDR (0x100000000u)
#define DDR_C7X_1_SCRATCH_SIZE (0x17000000u)
diff --git a/platform/j721s2/rtos/gen_linker_mem_map.py b/platform/j721s2/rtos/gen_linker_mem_map.py
index 56725bc..c19fd69 100755
--- a/platform/j721s2/rtos/gen_linker_mem_map.py
+++ b/platform/j721s2/rtos/gen_linker_mem_map.py
@@ -79,7 +79,7 @@
# This will generate linker command file at below folders
# ./<cpu name>/linker_mem_map.cmd
#
-# Here CPU name is mpu1, c7x_1, c7x_2, mcu1_0, mcu2_0, mcu3_0
+# Here CPU name is mpu1, c7x_1, c7x_2, mcu1_0, mcu2_0
#
#
from ti_psdk_rtos_tools import *
@@ -193,16 +193,6 @@ mcu2_1_ddr_resource_table_addr = mcu2_1_ddr_ipc_addr + linux_ddr_ipc_size;
mcu2_1_ddr_addr = mcu2_1_ddr_resource_table_addr + linux_ddr_resource_table_size;
mcu2_1_ddr_size = 32*MB - (mcu2_1_ddr_addr-mcu2_1_ddr_ipc_addr);
-mcu3_0_ddr_ipc_addr = mcu2_1_ddr_addr + mcu2_1_ddr_size;
-mcu3_0_ddr_resource_table_addr = mcu3_0_ddr_ipc_addr + linux_ddr_ipc_size;
-mcu3_0_ddr_addr = mcu3_0_ddr_resource_table_addr + linux_ddr_resource_table_size;
-mcu3_0_ddr_size = 16*MB - (mcu3_0_ddr_addr-mcu3_0_ddr_ipc_addr);
-
-mcu3_1_ddr_ipc_addr = mcu3_0_ddr_addr + mcu3_0_ddr_size;
-mcu3_1_ddr_resource_table_addr = mcu3_1_ddr_ipc_addr + linux_ddr_ipc_size;
-mcu3_1_ddr_addr = mcu3_1_ddr_resource_table_addr + linux_ddr_resource_table_size;
-mcu3_1_ddr_size = 16*MB - (mcu3_1_ddr_addr-mcu3_1_ddr_ipc_addr);
-
#
# DDR memory allocation for various shared memories
#
@@ -253,10 +243,6 @@ mcu2_0_ddr_local_heap_addr = mcu1_1_ddr_local_heap_addr + mcu1_1_ddr_local_heap
mcu2_0_ddr_local_heap_size = 16*MB;
mcu2_1_ddr_local_heap_addr = mcu2_0_ddr_local_heap_addr + mcu2_0_ddr_local_heap_size;
mcu2_1_ddr_local_heap_size = 16*MB;
-mcu3_0_ddr_local_heap_addr = mcu2_1_ddr_local_heap_addr + mcu2_1_ddr_local_heap_size;
-mcu3_0_ddr_local_heap_size = 8*MB;
-mcu3_1_ddr_local_heap_addr = mcu3_0_ddr_local_heap_addr + mcu3_0_ddr_local_heap_size;
-mcu3_1_ddr_local_heap_size = 8*MB;
c7x_1_ddr_scratch_addr = ddr_mem_addr_hi;
c7x_1_ddr_scratch_size = 368*MB;
@@ -343,26 +329,6 @@ mcu2_1_ddr_total.concat(mcu2_1_ddr_resource_table);
mcu2_1_ddr_total.concat(mcu2_1_ddr);
mcu2_1_ddr_total.setDtsName("vision_apps_main_r5fss0_core1_memory_region", "vision-apps-r5f-memory");
-mcu3_0_ddr_ipc = MemSection("DDR_MCU3_0_IPC", "RWIX", mcu3_0_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for MCU3_0 for Linux IPC");
-mcu3_0_ddr_ipc.setDtsName("vision_apps_main_r5fss1_core0_dma_memory_region", "vision-apps-r5f-dma-memory");
-mcu3_0_ddr_resource_table = MemSection("DDR_MCU3_0_RESOURCE_TABLE", "RWIX", mcu3_0_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for MCU3_0 for Linux resource table");
-mcu3_0_ddr = MemSection("DDR_MCU3_0", "RWIX", mcu3_0_ddr_addr, mcu3_0_ddr_size, "DDR for MCU3_0 for code/data");
-mcu3_0_ddr_local_heap = MemSection("DDR_MCU3_0_LOCAL_HEAP", "RWIX", mcu3_0_ddr_local_heap_addr, mcu3_0_ddr_local_heap_size, "DDR for MCU3_0 for local heap");
-mcu3_0_ddr_total = MemSection("DDR_MCU3_0_DTS", "", 0, 0, "DDR for MCU3_0 for all sections, used for reserving memory in DTS file");
-mcu3_0_ddr_total.concat(mcu3_0_ddr_resource_table);
-mcu3_0_ddr_total.concat(mcu3_0_ddr);
-mcu3_0_ddr_total.setDtsName("vision_apps_main_r5fss1_core0_memory_region", "vision-apps-r5f-memory");
-
-mcu3_1_ddr_ipc = MemSection("DDR_MCU3_1_IPC", "RWIX", mcu3_1_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for MCU3_1 for Linux IPC");
-mcu3_1_ddr_ipc.setDtsName("vision_apps_main_r5fss1_core1_dma_memory_region", "vision-apps-r5f-dma-memory");
-mcu3_1_ddr_resource_table = MemSection("DDR_MCU3_1_RESOURCE_TABLE", "RWIX", mcu3_1_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for MCU3_1 for Linux resource table");
-mcu3_1_ddr = MemSection("DDR_MCU3_1", "RWIX", mcu3_1_ddr_addr, mcu3_1_ddr_size, "DDR for MCU3_1 for code/data");
-mcu3_1_ddr_local_heap = MemSection("DDR_MCU3_1_LOCAL_HEAP", "RWIX", mcu3_1_ddr_local_heap_addr, mcu3_1_ddr_local_heap_size, "DDR for MCU3_1 for local heap");
-mcu3_1_ddr_total = MemSection("DDR_MCU3_1_DTS", "", 0, 0, "DDR for MCU3_1 for all sections, used for reserving memory in DTS file");
-mcu3_1_ddr_total.concat(mcu3_1_ddr_resource_table);
-mcu3_1_ddr_total.concat(mcu3_1_ddr);
-mcu3_1_ddr_total.setDtsName("vision_apps_main_r5fss1_core1_memory_region", "vision-apps-r5f-memory");
-
c7x_2_ddr_ipc = MemSection("DDR_C7x_2_IPC", "RWIX", c7x_2_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for C7x_2 for Linux IPC");
c7x_2_ddr_ipc.setDtsName("vision_apps_c71_1_dma_memory_region", "vision-apps-c71_1-dma-memory");
c7x_2_ddr_resource_table = MemSection("DDR_C7x_2_RESOURCE_TABLE", "RWIX", c7x_2_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for C7x_2 for Linux resource table");
@@ -422,8 +388,6 @@ vision_apps_core_heaps_lo = MemSection("DDR_VISION_APPS_CORE_HEAPS_LO_DTS", "",
vision_apps_core_heaps_lo.concat(mcu1_0_ddr_local_heap);
vision_apps_core_heaps_lo.concat(mcu2_0_ddr_local_heap);
vision_apps_core_heaps_lo.concat(mcu2_1_ddr_local_heap);
-vision_apps_core_heaps_lo.concat(mcu3_0_ddr_local_heap);
-vision_apps_core_heaps_lo.concat(mcu3_1_ddr_local_heap);
vision_apps_core_heaps_lo.setDtsName("vision_apps_core_heaps_lo", "vision-apps-core-heap-memory-lo");
c7x_1_ddr_local_heap_phy = MemSection("DDR_C7X_1_LOCAL_HEAP", "RWIX", ddr_mem_addr_hi_phy, (c7x_1_ddr_scratch_size + c7x_1_ddr_local_heap_size + c7x_2_ddr_scratch_size + c7x_2_ddr_local_heap_size), "DDR for c7x_1, c7x_2 for scratch memory and local heap");
@@ -498,34 +462,6 @@ mcu2_1_mmap.addMemSection( ddr_shared_mem );
mcu2_1_mmap.addMemSection( mcu2_1_main_ocram );
mcu2_1_mmap.checkOverlap();
-mcu3_0_mmap = MemoryMap("mcu3_0");
-mcu3_0_mmap.addMemSection( mcu_r5f_tcma_vecs );
-mcu3_0_mmap.addMemSection( mcu_r5f_tcma );
-mcu3_0_mmap.addMemSection( r5f_tcmb0 );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr_ipc );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr_resource_table );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr );
-mcu3_0_mmap.addMemSection( app_log_mem );
-mcu3_0_mmap.addMemSection( tiovx_obj_desc_mem );
-mcu3_0_mmap.addMemSection( ipc_vring_mem );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr_local_heap );
-mcu3_0_mmap.addMemSection( ddr_shared_mem );
-mcu3_0_mmap.checkOverlap();
-
-mcu3_1_mmap = MemoryMap("mcu3_1");
-mcu3_1_mmap.addMemSection( mcu_r5f_tcma_vecs );
-mcu3_1_mmap.addMemSection( mcu_r5f_tcma );
-mcu3_1_mmap.addMemSection( r5f_tcmb0 );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr_ipc );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr_resource_table );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr );
-mcu3_1_mmap.addMemSection( app_log_mem );
-mcu3_1_mmap.addMemSection( tiovx_obj_desc_mem );
-mcu3_1_mmap.addMemSection( ipc_vring_mem );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr_local_heap );
-mcu3_1_mmap.addMemSection( ddr_shared_mem );
-mcu3_1_mmap.checkOverlap();
-
c7x_1_mmap = MemoryMap("c7x_1");
c7x_1_mmap.addMemSection( c7x_1_l2 );
c7x_1_mmap.addMemSection( c7x_1_l1 );
@@ -585,14 +521,6 @@ html_mmap.addMemSection( mcu2_1_ddr_ipc );
html_mmap.addMemSection( mcu2_1_ddr_resource_table );
html_mmap.addMemSection( mcu2_1_ddr );
html_mmap.addMemSection( mcu2_1_ddr_local_heap );
-html_mmap.addMemSection( mcu3_0_ddr_ipc );
-html_mmap.addMemSection( mcu3_0_ddr_resource_table );
-html_mmap.addMemSection( mcu3_0_ddr );
-html_mmap.addMemSection( mcu3_0_ddr_local_heap );
-html_mmap.addMemSection( mcu3_1_ddr_ipc );
-html_mmap.addMemSection( mcu3_1_ddr_resource_table );
-html_mmap.addMemSection( mcu3_1_ddr );
-html_mmap.addMemSection( mcu3_1_ddr_local_heap );
html_mmap.addMemSection( c7x_1_ddr_ipc );
html_mmap.addMemSection( c7x_1_ddr_resource_table );
html_mmap.addMemSection( c7x_1_ddr_boot );
@@ -628,16 +556,12 @@ c_header_mmap.addMemSection( mcu1_0_ddr_ipc );
c_header_mmap.addMemSection( mcu1_1_ddr_ipc );
c_header_mmap.addMemSection( mcu2_0_ddr_ipc );
c_header_mmap.addMemSection( mcu2_1_ddr_ipc );
-c_header_mmap.addMemSection( mcu3_0_ddr_ipc );
-c_header_mmap.addMemSection( mcu3_1_ddr_ipc );
c_header_mmap.addMemSection( c7x_1_ddr_ipc );
c_header_mmap.addMemSection( c7x_2_ddr_ipc );
c_header_mmap.addMemSection( mcu1_0_ddr_total );
c_header_mmap.addMemSection( mcu1_1_ddr_total );
c_header_mmap.addMemSection( mcu2_0_ddr_total );
c_header_mmap.addMemSection( mcu2_1_ddr_total );
-c_header_mmap.addMemSection( mcu3_0_ddr_total );
-c_header_mmap.addMemSection( mcu3_1_ddr_total );
c_header_mmap.addMemSection( c7x_1_ddr_total );
c_header_mmap.addMemSection( c7x_2_ddr_total );
@@ -645,8 +569,6 @@ c_header_mmap.addMemSection( mcu1_0_ddr_local_heap);
c_header_mmap.addMemSection( mcu1_1_ddr_local_heap);
c_header_mmap.addMemSection( mcu2_0_ddr_local_heap);
c_header_mmap.addMemSection( mcu2_1_ddr_local_heap);
-c_header_mmap.addMemSection( mcu3_0_ddr_local_heap);
-c_header_mmap.addMemSection( mcu3_1_ddr_local_heap);
c_header_mmap.addMemSection( c7x_1_ddr_local_heap);
c_header_mmap.addMemSection( c7x_1_ddr_scratch);
c_header_mmap.addMemSection( c7x_2_ddr_local_heap);
@@ -672,10 +594,6 @@ dts_mmap.addMemSection( mcu2_0_ddr_ipc );
dts_mmap.addMemSection( mcu2_0_ddr_total );
dts_mmap.addMemSection( mcu2_1_ddr_ipc );
dts_mmap.addMemSection( mcu2_1_ddr_total );
-dts_mmap.addMemSection( mcu3_0_ddr_ipc );
-dts_mmap.addMemSection( mcu3_0_ddr_total );
-dts_mmap.addMemSection( mcu3_1_ddr_ipc );
-dts_mmap.addMemSection( mcu3_1_ddr_total );
dts_mmap.addMemSection( c7x_1_ddr_ipc );
dts_mmap.addMemSection( c7x_1_ddr_total );
dts_mmap.addMemSection( c7x_2_ddr_ipc );
@@ -696,8 +614,6 @@ LinkerCmdFile(mcu1_0_mmap, "./mcu1_0/linker_mem_map.cmd").export();
LinkerCmdFile(mcu1_1_mmap, "./mcu1_1/linker_mem_map.cmd").export();
LinkerCmdFile(mcu2_0_mmap, "./mcu2_0/linker_mem_map.cmd").export();
LinkerCmdFile(mcu2_1_mmap, "./mcu2_1/linker_mem_map.cmd").export();
-LinkerCmdFile(mcu3_0_mmap, "./mcu3_0/linker_mem_map.cmd").export();
-LinkerCmdFile(mcu3_1_mmap, "./mcu3_1/linker_mem_map.cmd").export();
HtmlMmapTable(html_mmap, "./system_memory_map.html").export();
diff --git a/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi b/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi
index 86855a6..214590f 100644
--- a/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi
+++ b/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi
@@ -4,7 +4,7 @@
* IMPORTANT NOTE: Follow below instructions to apply the updated memory map to linux dtsi file,
*
* 1. Copy the memory sections, from the generated dts file, to the file shown below under reserved_memory: reserved-memory { ... }
- * ${LINUX_KERNEL_PATH}/arch/arm64/boot/dts/ti/k3-j721s2-rtos-memory-map.dtsi
+ * ${LINUX_KERNEL_PATH}/arch/arm64/boot/dts/ti/k3-j721e-rtos-memory-map.dtsi
*
* 2. Rebuild the dtb, dtbo from PSDK Linux install directory
* make linux-dtbs
@@ -55,26 +55,6 @@
reg = <0x00 0xa4100000 0x00 0x01f00000>;
no-map;
};
- vision_apps_main_r5fss1_core0_dma_memory_region: vision-apps-r5f-dma-memory@a6000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa6000000 0x00 0x00100000>;
- no-map;
- };
- vision_apps_main_r5fss1_core0_memory_region: vision-apps-r5f-memory@a6100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa6100000 0x00 0x00f00000>;
- no-map;
- };
- vision_apps_main_r5fss1_core1_dma_memory_region: vision-apps-r5f-dma-memory@a7000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa7000000 0x00 0x00100000>;
- no-map;
- };
- vision_apps_main_r5fss1_core1_memory_region: vision-apps-r5f-memory@a7100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa7100000 0x00 0x00f00000>;
- no-map;
- };
vision_apps_rtos_ipc_memory_region: vision-apps-rtos-ipc-memory-region@a8000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa8000000 0x00 0x02000000>;
@@ -111,7 +91,7 @@
};
vision_apps_core_heaps_lo: vision-apps-core-heap-memory-lo@d8000000 {
compatible = "shared-dma-pool";
- reg = <0x00 0xd8000000 0x00 0x04000000>;
+ reg = <0x00 0xd8000000 0x00 0x03000000>;
no-map;
};
vision_apps_core_heaps_hi: vision-apps-core-heap-memory-hi@880000000 {
diff --git a/platform/j721s2/rtos/system_memory_map.html b/platform/j721s2/rtos/system_memory_map.html
index 1859f9b..57d49f5 100644
--- a/platform/j721s2/rtos/system_memory_map.html
+++ b/platform/j721s2/rtos/system_memory_map.html
@@ -192,54 +192,6 @@
<td class="tg-kftd">RWIX</td>
<td class="tg-kftd">DDR for MCU2_1 for code/data</td>
</tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_0_IPC</td>
- <td class="tg-6sgx">0xA6000000</td>
- <td class="tg-6sgx">0xA60FFFFF</td>
- <td class="tg-6sgx">1024.00 KB</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_0 for Linux IPC</td>
- </tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_0_RESOURCE_TABLE</td>
- <td class="tg-kftd">0xA6100000</td>
- <td class="tg-kftd">0xA61003FF</td>
- <td class="tg-kftd">1024 B</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_0 for Linux resource table</td>
- </tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_0</td>
- <td class="tg-6sgx">0xA6100400</td>
- <td class="tg-6sgx">0xA6FFFFFF</td>
- <td class="tg-6sgx">15.00 MB</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_0 for code/data</td>
- </tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_1_IPC</td>
- <td class="tg-kftd">0xA7000000</td>
- <td class="tg-kftd">0xA70FFFFF</td>
- <td class="tg-kftd">1024.00 KB</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_1 for Linux IPC</td>
- </tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_1_RESOURCE_TABLE</td>
- <td class="tg-6sgx">0xA7100000</td>
- <td class="tg-6sgx">0xA71003FF</td>
- <td class="tg-6sgx">1024 B</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_1 for Linux resource table</td>
- </tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_1</td>
- <td class="tg-kftd">0xA7100400</td>
- <td class="tg-kftd">0xA7FFFFFF</td>
- <td class="tg-kftd">15.00 MB</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_1 for code/data</td>
- </tr>
<tr>
<td class="tg-6sgx">IPC_VRING_MEM</td>
<td class="tg-6sgx">0xA8000000</td>
@@ -408,22 +360,6 @@
<td class="tg-6sgx">RWIX</td>
<td class="tg-6sgx">DDR for MCU2_1 for local heap</td>
</tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_0_LOCAL_HEAP</td>
- <td class="tg-kftd">0xDB000000</td>
- <td class="tg-kftd">0xDB7FFFFF</td>
- <td class="tg-kftd"> 8.00 MB</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_0 for local heap</td>
- </tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_1_LOCAL_HEAP</td>
- <td class="tg-6sgx">0xDB800000</td>
- <td class="tg-6sgx">0xDBFFFFFF</td>
- <td class="tg-6sgx"> 8.00 MB</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_1 for local heap</td>
- </tr>
<tr>
<td class="tg-kftd">DDR_C7X_1_SCRATCH</td>
<td class="tg-kftd">0x100000000</td>
Verification Command:
cat /proc/interrupts
Output:
The main-r5fss1-core0 interrupt is not seen upon the input of the command
4. Removal of Drivers for the disabled IP (GPU, EDP, CSITX etc..)
There would be requirements for the subset devices to remove few hardware IP.
For example:
a) the subset analytics devices like TDA4AL, the GPU is not available. Hence to remove the GPU support from the SDK, the changes are required on the u-boot and Linux kernel as shown below.
diff --git a/arch/arm/dts/k3-j721s2.dtsi b/arch/arm/dts/k3-j721s2.dtsi index c25d0c2aff..d7c4f95f21 100644 --- a/arch/arm/dts/k3-j721s2.dtsi +++ b/arch/arm/dts/k3-j721s2.dtsi @@ -122,7 +122,6 @@ <0x00 0x70000000 0x00 0x70000000 0x00 0x00400000>, /* MSMC RAM */ <0x00 0x30000000 0x00 0x30000000 0x00 0x0c400000>, /* MAIN NAVSS */ <0x41 0x00000000 0x41 0x00000000 0x01 0x00000000>, /* PCIe1 DAT1 */ - <0x4e 0x20000000 0x4e 0x20000000 0x00 0x00080000>, /* GPU */ /* MCUSS_WKUP Range */ <0x00 0x28380000 0x00 0x28380000 0x00 0x03880000>,
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
index 69216fe05..8ee1a470e 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
@@ -288,16 +288,6 @@
power-domains = <&k3_pds 358 TI_SCI_PD_EXCLUSIVE>;
};
- gpu: gpu@4e20000000 {
- compatible = "ti,j721s2-pvr", "img,pvr-bxs64";
- reg = <0x4e 0x20000000 0x00 0x80000>;
- interrupts = <GIC_SPI 24 IRQ_TYPE_LEVEL_HIGH>;
- power-domains = <&k3_pds 130 TI_SCI_PD_EXCLUSIVE>,
- <&k3_pds 373 TI_SCI_PD_EXCLUSIVE>;
- power-domain-names = "gpu_0", "gpucore_0";
- clocks = <&k3_clks 130 1>;
- };
-
main_gpio0: gpio@600000 {
compatible = "ti,j721e-gpio", "ti,keystone-gpio";
reg = <0x00 0x00600000 0x00 0x100>;
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2.dtsi b/arch/arm64/boot/dts/ti/k3-j721s2.dtsi
index 75bc8dfac..dd2f0ebc8 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-j721s2.dtsi
@@ -122,7 +122,6 @@
<0x00 0x70000000 0x00 0x70000000 0x00 0x00400000>, /* MSMC RAM */
<0x00 0x30000000 0x00 0x30000000 0x00 0x0c400000>, /* MAIN NAVSS */
<0x41 0x00000000 0x41 0x00000000 0x01 0x00000000>, /* PCIe1 DAT1 */
- <0x4e 0x20000000 0x4e 0x20000000 0x00 0x00080000>, /* GPU */
/* MCUSS_WKUP Range */
<0x00 0x28380000 0x00 0x28380000 0x00 0x03880000>,
Verification Command:
devmem2 0x4E20000018
Output:
Kernel Crash
b) For some subset analytics devices like TDA4AL88, the EDP support is not available. Hence to remove the EDP support from the SDK, the changes are required on the Linux kernel as shown below.
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts b/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
index b6158a27f..a8ad37a9a 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
+++ b/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
@@ -148,19 +148,6 @@
regulator-always-on;
};
- dp0: dp0-connector {
- compatible = "dp-connector";
- label = "DP0";
- type = "full-size";
- dp-pwr-supply = <&dp0_pwr_3v3>;
-
- port {
- dp0_connector_in: endpoint {
- remote-endpoint = <&dp0_out>;
- };
- };
- };
-
panel {
compatible = "ti,panel-edp";
power-supply = <&dp1_pwr_3v3>;
@@ -626,13 +613,6 @@
#address-cells = <1>;
#size-cells = <0>;
- port@0 {
- reg = <0>;
- dpi0_out: endpoint {
- remote-endpoint = <&dp0_in>;
- };
- };
-
port@2 {
reg = <2>;
dpi2_out: endpoint {
@@ -673,31 +653,6 @@
};
};
-&mhdp {
- pinctrl-names = "default";
- pinctrl-0 = <&dp0_pins_default>;
- cdns,no-hpd;
-};
-
-&dp0_ports {
- #address-cells = <1>;
- #size-cells = <0>;
-
- port@0 {
- reg = <0>;
- dp0_in: endpoint {
- remote-endpoint = <&dpi0_out>;
- };
- };
-
- port@4 {
- reg = <4>;
- dp0_out: endpoint {
- remote-endpoint = <&dp0_connector_in>;
- };
- };
-};
-
&main_mcan0 {
status = "disabled";
};
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
index 69216fe05..8ee1a470e 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
@@ -1493,32 +1443,6 @@
power-domains = <&k3_pds 346 TI_SCI_PD_EXCLUSIVE>;
};
- mhdp: dp-bridge@a000000 {
- compatible = "ti,j721e-mhdp8546";
- /*
- * Note: we do not map DPTX PHY area, as that is handled by
- * the PHY driver.
- */
- reg = <0x0 0xa000000 0x0 0x30a00>, /* DSS_EDP0_V2A_CORE_VP_REGS_APB */
- <0x0 0x4f40000 0x0 0x20>; /* DSS_EDP0_INTG_CFG_VP */
- reg-names = "mhdptx", "j721e-intg";
-
- clocks = <&k3_clks 156 19>;
-
- phys = <&torrent_phy_dp>;
- phy-names = "dpphy";
-
- interrupt-parent = <&gic500>;
- interrupts = <GIC_SPI 614 IRQ_TYPE_LEVEL_HIGH>;
-
- power-domains = <&k3_pds 156 TI_SCI_PD_EXCLUSIVE>;
-
- dp0_ports: ports {
- #address-cells = <1>;
- #size-cells = <0>;
- };
- };
-
dphy0: phy@4480000 {
compatible = "ti,j721e-dphy";
reg = <0x0 0x04480000 0x0 0x1000>;
Verification Command:
devmem2 0x04F4001C
Output:
Kernel Crash
SBL Boot flow
For SBL boot flow, users are required to refer the below modifications for SDK 8.6
1. Reduction in the number of DDR Instances
Some of the subset devices of J721s2 such as TDA4AL88, TDA4VL21 etc has only 1 DDR instance as compared to its superset device (which has 2). Hence the below modification shall be made in-order to make SDK compatible for 1 DDR instance.
Note: The DDR register related changes are done in SBL whereas the configuration of DDR size should be done on Linux. Only a slight modification required on vision_apps
diff --git a/packages/ti/board/src/j721s2_evm/board_clock.c b/packages/ti/board/src/j721s2_evm/board_clock.c
index b7e6faf..1d5524b 100644
--- a/packages/ti/board/src/j721s2_evm/board_clock.c
+++ b/packages/ti/board/src/j721s2_evm/board_clock.c
@@ -98,9 +98,7 @@ uint32_t gBoardClkModuleMcuIDDeinitGroupl[] = {
uint32_t gBoardClkModuleMainIDInitGroup1[] = {
TISCI_DEV_DDR0,
- TISCI_DEV_DDR1,
TISCI_DEV_EMIF_DATA_0_VD,
- TISCI_DEV_EMIF_DATA_1_VD,
TISCI_DEV_MMCSD0,
TISCI_DEV_MMCSD1,
TISCI_DEV_GPIO4,
diff --git a/packages/ti/board/src/j721s2_evm/include/board_ddr.h b/packages/ti/board/src/j721s2_evm/include/board_ddr.h
index 60213e0..b75c22e 100644
--- a/packages/ti/board/src/j721s2_evm/include/board_ddr.h
+++ b/packages/ti/board/src/j721s2_evm/include/board_ddr.h
@@ -86,7 +86,7 @@ extern "C" {
#define BOARD_DDR_INSTANCE_0 (0U)
#define BOARD_DDR_INSTANCE_1 (1U)
-#define BOARD_DDR_INSTANCE_MAX (2U)
+#define BOARD_DDR_INSTANCE_MAX (1U)
#define BOARD_DDR_LOCK0 (0x115008U)
#define BOARD_DDR_LOCK1 (0x11500CU)
diff --git a/packages/ti/board/src/j721s2_evm/include/board_ddrRegInit.h b/packages/ti/board/src/j721s2_evm/include/board_ddrRegInit.h
index feec6d6..ddd2b4f 100644
--- a/packages/ti/board/src/j721s2_evm/include/board_ddrRegInit.h
+++ b/packages/ti/board/src/j721s2_evm/include/board_ddrRegInit.h
@@ -45,7 +45,7 @@
#define MULTI_DDR_CFG_INTRLV_SIZE 11
#define MULTI_DDR_CFG_ECC_ENABLE 0
#define MULTI_DDR_CFG_HYBRID_SELECT 0
-#define MULTI_DDR_CFG_EMIFS_ACTIVE 3
+#define MULTI_DDR_CFG_EMIFS_ACTIVE 1
uint32_t DDRSS0_ctlReg[] = {
0x00000B00U,
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2-som-p0.dtsi b/arch/arm64/boot/dts/ti/k3-j721s2-som-p0.dtsi
index db1219b2b..725bc4481 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2-som-p0.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-j721s2-som-p0.dtsi
@@ -13,9 +13,9 @@
/ {
memory@80000000 {
device_type = "memory";
- /* 16 GB RAM */
+ /* 8 GB RAM */
reg = <0x00 0x80000000 0x00 0x80000000>,
- <0x08 0x80000000 0x03 0x80000000>;
+ <0x08 0x80000000 0x01 0x80000000>;
};
/* Reserving memory regions still pending */
@@ -469,3 +469,228 @@
};
};
};
diff --git a/utils/perf_stats/src/app_perf_stats_freertos.c b/utils/perf_stats/src/app_perf_stats_freertos.c
index 2c63699..cd6805a 100644
--- a/utils/perf_stats/src/app_perf_stats_freertos.c
+++ b/utils/perf_stats/src/app_perf_stats_freertos.c
@@ -88,7 +88,7 @@
#if defined(SOC_J721E) || defined(SOC_AM62A)
#define APP_PERF_NUM_DDR_INSTANCES (1u)
#elif defined (SOC_J721S2)
-#define APP_PERF_NUM_DDR_INSTANCES (2u)
+#define APP_PERF_NUM_DDR_INSTANCES (1u)
#elif defined (SOC_J784S4)
#define APP_PERF_NUM_DDR_INSTANCES (4u)
#endif
@@ -631,7 +631,7 @@ void appPerfStatsDdrStatsReadCounters(uint32_t *val0, uint32_t *val1, uint32_t *
cnt3[0] = (volatile uint32_t *)0x02980110;
#endif
- #if defined(SOC_J721S2) || defined(SOC_J784S4)
+ #if defined(SOC_J784S4)
cnt_sel[1] = (volatile uint32_t *)0x029A0100;
cnt0[1] = (volatile uint32_t *)0x029A0104;
cnt1[1] = (volatile uint32_t *)0x029A0108;
Builds Required
cd ${PSDKLA}/
make linux-dtbs
Assuming the SOC is J721s2 (SDK 8.6)
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/build/
make pdk_libs_clean BOARD=j721s2_evm
make pdk_libs BOARD=j721s2_evm
Assuming the SOC is J721s2 (SDK 8.6), Default SBL with MMCSD boot media
For custom SBL and different boot media, please adapt the build commands accordingly
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/build/
make sbl_lib_mmcsd_hlos_clean BOARD=j721s2_evm
make sbl_mmcsd_img_hlos_clean BOARD=j721s2_evm
make sbl_lib_mmcsd_hlos BOARD=j721s2_evm
make sbl_mmcsd_img_hlos BOARD=j721s2_evm
Assuming SOC as J721s2 (SDK 8.6)
To Build vision_apps
=====================
cd ${PSDKRA}/vision_apps
make vision_apps_scrub
make vision_apps
To Build combined_app image
============================
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/boot/sbl/tools/combined_appimage/
make clean BOARD=j721s2_evm
make BOARD=j721s2_evm HLOS_BOOT=optimized
Verification Command
root@j721s2-evm:~# grep MemTotal /proc/meminfo
MemTotal: 6418836 kB
root@j721s2-evm:~# free
total used free shared buff/cache available
Mem: 6418836 79556 6145748 9276 193532 6175444
Swap: 0 0 0
root@j721s2-evm:~#
2. Change in the clock frequency for the core based on the speed grade or power optimization
Based on the speed grades/ power optimization, there would be changes in the clock frequencies at which the cores would run. One such example is shown in the below table for speed grade T, N and H for J721s2

To change the clock frequency associated with a core, follow the below steps.
1. Identify the clock source/ PLL and the divider associated with that core from the TRM (Clocking Section) of the superset device.
2. Based on the PLL, modify the divider such that the final output clock is as per the speed grade.
Below is an example of how to change the clock for C7x core for TDA4VL21. The PLL is identified to be MAIN_PLL7 HSDIV0.
The changes done are as below.
diff --git a/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c b/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c
index 2122081..7438db5 100644
--- a/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c
+++ b/packages/ti/drv/sciclient/src/rm_pm_hal/pm/soc/j721s2/clocks.c
@@ -5160,7 +5160,7 @@ static const struct clk_data_div_reg clk_data_hsdiv0_16fft_main_6_hsdiv0 = {
static const struct clk_data_div_reg clk_data_hsdiv0_16fft_main_7_hsdiv0 = {
.data_div = {
.n = 128,
- .default_div = 2,
+ .default_div = 4,
},
.reg = 0x00680000UL + (0x1000UL * 7UL) + 0x80UL + (0x4UL * 0UL),
.bit = 0,
Here the clock is reduced from 1GHz to 500MHz for C7x core.
Builds Required
Assuming the SOC is J721s2 (SDK 8.6)
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/build/
make pdk_libs_clean BOARD=j721s2_evm
make pdk_libs BOARD=j721s2_evm
Assuming SOC as J721s2 (SDK 8.6). DM is assumed to be ipc_echo_testb_freertos.
If a different DM is used, please use the command to rebuild that DM.
To Build DM
============
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/build
make ipc_echo_testb_freertos_clean BOARD=j721s2_evm CORE=mcu1_0
make ipc_echo_testb_freertos BOARD=j721s2_evm CORE=mcu1_0
To Build combined_app image
============================
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/boot/sbl/tools/combined_appimage/
make clean BOARD=j721s2_evm
make BOARD=j721s2_evm HLOS_BOOT=optimized
Verification Command:
k3conf dump clock 8
k3conf dump clock 11
Output:
The C7x cores clock value is 500MHz.
|-----------------------------------------------------------------------------------------------------------------------| | Device ID | Clock ID | Clock Name | Status | Clock Frequency | |-----------------------------------------------------------------------------------------------------------------------| | 8 | 0 | DEV_COMPUTE_CLUSTER0_C71SS0_0_C7X_CLK | CLK_STATE_READY | 500000000 | | 8 | 1 | DEV_COMPUTE_CLUSTER0_C71SS0_0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 | | 8 | 3 | DEV_COMPUTE_CLUSTER0_C71SS0_0_C7X_DIVH_CLK4_OBSCLK_OUT_CLK | CLK_STATE_READY | 0 | |-----------------------------------------------------------------------------------------------------------------------| |-------------------------------------------------------------------------------------------------------| | Device ID | Clock ID | Clock Name | Status | Clock Frequency | |-------------------------------------------------------------------------------------------------------| | 11 | 0 | DEV_COMPUTE_CLUSTER0_C71SS1_0_C7X_CLK | CLK_STATE_READY | 500000000 | | 11 | 1 | DEV_COMPUTE_CLUSTER0_C71SS1_0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 | |-------------------------------------------------------------------------------------------------------|
Below is an example of how to change the clock for A72 core for Speed Grade "H" (i.e., from 2GHz to 1.2 GHz)
diff --git a/packages/ti/boot/sbl/soc/k3/sbl_soc_cfg.h b/packages/ti/boot/sbl/soc/k3/sbl_soc_cfg.h index 53800ea..01e2f26 100755 --- a/packages/ti/boot/sbl/soc/k3/sbl_soc_cfg.h +++ b/packages/ti/boot/sbl/soc/k3/sbl_soc_cfg.h @@ -653,12 +653,12 @@ extern uint16_t sblMapOtpVidToMilliVolts[256]; #define SBL_PROC_ID_MPU1_CPU0 (SCICLIENT_PROC_ID_A72SS0_CORE0) #define SBL_DEV_ID_MPU1_CPU0 (TISCI_DEV_A72SS0_CORE0) #define SBL_CLK_ID_MPU1_CPU0 (TISCI_DEV_A72SS0_CORE0_ARM_CLK_CLK) -#define SBL_MPU1_CPU0_FREQ_HZ (2000000000) +#define SBL_MPU1_CPU0_FREQ_HZ (1200000000) #define SBL_PROC_ID_MPU1_CPU1 (SCICLIENT_PROC_ID_A72SS0_CORE1) #define SBL_DEV_ID_MPU1_CPU1 (TISCI_DEV_A72SS0_CORE1) #define SBL_CLK_ID_MPU1_CPU1 (TISCI_DEV_A72SS0_CORE1_ARM_CLK_CLK) -#define SBL_MPU1_CPU1_FREQ_HZ (2000000000) +#define SBL_MPU1_CPU1_FREQ_HZ (1200000000)
Builds Required
Assuming the SOC is J721s2 (SDK 8.6), Default SBL with MMCSD boot media
For custom SBL and different boot media, please adapt the build commands accordingly
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/build/
make sbl_lib_mmcsd_hlos_clean BOARD=j721s2_evm
make sbl_mmcsd_img_hlos_clean BOARD=j721s2_evm
make sbl_lib_mmcsd_hlos BOARD=j721s2_evm
make sbl_mmcsd_img_hlos BOARD=j721s2_evm
Verification Command:
k3conf dump clock 202
k3conf dump clock 203
Output:
root@j721s2-evm:~# k3conf dump clock 202
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-88-g982f5c2 built Wed Mar 1 18:42:41 UTC 2023) |
| SoC | J721S2 SR1.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
|-----------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|-----------------------------------------------------------------------------------------|
| 202 | 0 | DEV_A72SS0_CORE0_ARM_CLK_CLK | CLK_STATE_READY | 1200000000 |
|-----------------------------------------------------------------------------------------|
root@j721s2-evm:~# k3conf dump clock 203
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-88-g982f5c2 built Wed Mar 1 18:42:41 UTC 2023) |
| SoC | J721S2 SR1.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0008 '8.6.3--v08.06.03 (Chill Capybar)') |
|--------------------------------------------------------------------------------|
|-----------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|-----------------------------------------------------------------------------------------|
| 203 | 0 | DEV_A72SS0_CORE1_ARM_CLK_CLK | CLK_STATE_READY | 1200000000 |
|-----------------------------------------------------------------------------------------|
The similar could be done for other cores / HWA as per the combination of speed grades and power optimizations.
3. Disabling/removing the additional cores
Subsets such as TDA4AL88 and TDA4VL21 are quad core R5 devices as compared to it superset which is a hexa core device. There are other subsets where there is only 1 C7x core available.
The changes for the same are required in u-boot, linux and vision_apps.
For example, removal of MCU3_0 (or) main_r5fss1 can be done as shown below
diff --git a/arch/arm/dts/k3-j721s2-common-proc-board.dts b/arch/arm/dts/k3-j721s2-common-proc-board.dts
index 5b7e33490f..ffd9c8568b 100644
--- a/arch/arm/dts/k3-j721s2-common-proc-board.dts
+++ b/arch/arm/dts/k3-j721s2-common-proc-board.dts
@@ -32,8 +32,6 @@
remoteproc1 = &mcu_r5fss0_core1;
remoteproc2 = &main_r5fss0_core0;
remoteproc3 = &main_r5fss0_core1;
- remoteproc4 = &main_r5fss1_core0;
- remoteproc5 = &main_r5fss1_core1;
remoteproc6 = &c71_0;
remoteproc7 = &c71_1;
};
diff --git a/arch/arm/dts/k3-j721s2-main.dtsi b/arch/arm/dts/k3-j721s2-main.dtsi
index 18e5113336..d9bf23b1e9 100644
--- a/arch/arm/dts/k3-j721s2-main.dtsi
+++ b/arch/arm/dts/k3-j721s2-main.dtsi
@@ -1152,46 +1152,6 @@
};
};
- main_r5fss1: r5fss@5e00000 {
- compatible = "ti,j721s2-r5fss";
- ti,cluster-mode = <0>;
- #address-cells = <1>;
- #size-cells = <1>;
- ranges = <0x5e00000 0x00 0x5e00000 0x20000>,
- <0x5f00000 0x00 0x5f00000 0x20000>;
- power-domains = <&k3_pds 278 TI_SCI_PD_EXCLUSIVE>;
-
- main_r5fss1_core0: r5f@5e00000 {
- compatible = "ti,j721s2-r5f";
- reg = <0x5e00000 0x00010000>,
- <0x5e10000 0x00010000>;
- reg-names = "atcm", "btcm";
- ti,sci = <&sms>;
- ti,sci-dev-id = <281>;
- ti,sci-proc-ids = <0x08 0xff>;
- resets = <&k3_reset 281 1>;
- firmware-name = "j721s2-main-r5f1_0-fw";
- ti,atcm-enable = <1>;
- ti,btcm-enable = <1>;
- ti,loczrama = <1>;
- };
-
- main_r5fss1_core1: r5f@5f00000 {
- compatible = "ti,j721s2-r5f";
- reg = <0x5f00000 0x00010000>,
- <0x5f10000 0x00010000>;
- reg-names = "atcm", "btcm";
- ti,sci = <&sms>;
- ti,sci-dev-id = <282>;
- ti,sci-proc-ids = <0x09 0xff>;
- resets = <&k3_reset 282 1>;
- firmware-name = "j721s2-main-r5f1_1-fw";
- ti,atcm-enable = <1>;
- ti,btcm-enable = <1>;
- ti,loczrama = <1>;
- };
- };
-
c71_0: dsp@64800000 {
compatible = "ti,j721s2-c71-dsp";
reg = <0x00 0x64800000 0x00 0x00080000>,
diff --git a/arch/arm/dts/k3-j721s2-som-p0.dtsi b/arch/arm/dts/k3-j721s2-som-p0.dtsi
index f3080e948e..c4df1d51bd 100644
--- a/arch/arm/dts/k3-j721s2-som-p0.dtsi
+++ b/arch/arm/dts/k3-j721s2-som-p0.dtsi
@@ -78,30 +78,6 @@
no-map;
};
- main_r5fss1_core0_dma_memory_region: r5f-dma-memory@a4000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa4000000 0x00 0x100000>;
- no-map;
- };
-
- main_r5fss1_core0_memory_region: r5f-memory@a4100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa4100000 0x00 0xf00000>;
- no-map;
- };
-
- main_r5fss1_core1_dma_memory_region: r5f-dma-memory@a5000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa5000000 0x00 0x100000>;
- no-map;
- };
-
- main_r5fss1_core1_memory_region: r5f-memory@a5100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa5100000 0x00 0xf00000>;
- no-map;
- };
-
c71_0_dma_memory_region: c71-dma-memory@a6000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa6000000 0x00 0x100000>;
@@ -251,17 +227,7 @@
};
&mailbox0_cluster2 {
- interrupts = <428>;
-
- mbox_main_r5fss1_core0: mbox-main-r5fss1-core0 {
- ti,mbox-rx = <0 0 0>;
- ti,mbox-tx = <1 0 0>;
- };
-
- mbox_main_r5fss1_core1: mbox-main-r5fss1-core1 {
- ti,mbox-rx = <2 0 0>;
- ti,mbox-tx = <3 0 0>;
- };
+ status = "disabled";
};
&mailbox0_cluster3 {
@@ -382,18 +348,6 @@
<&main_r5fss0_core1_memory_region>;
};
-&main_r5fss1_core0 {
- mboxes = <&mailbox0_cluster2 &mbox_main_r5fss1_core0>;
- memory-region = <&main_r5fss1_core0_dma_memory_region>,
- <&main_r5fss1_core0_memory_region>;
-};
-
-&main_r5fss1_core1 {
- mboxes = <&mailbox0_cluster2 &mbox_main_r5fss1_core1>;
- memory-region = <&main_r5fss1_core1_dma_memory_region>,
- <&main_r5fss1_core1_memory_region>;
-};
-
&c71_0 {
mboxes = <&mailbox0_cluster4 &mbox_c71_0>;
memory-region = <&c71_0_dma_memory_region>,
diff --git a/platform/j721s2/rtos/app_mem_map.h b/platform/j721s2/rtos/app_mem_map.h
index 4f1c7f6..e562580 100755
--- a/platform/j721s2/rtos/app_mem_map.h
+++ b/platform/j721s2/rtos/app_mem_map.h
@@ -127,22 +127,6 @@
#define DDR_MCU2_1_DTS_ADDR (0xA4100000u)
#define DDR_MCU2_1_DTS_SIZE (0x01F00000u)
-/* DDR for MCU3_0 for Linux IPC [ size 1024.00 KB ] */
-#define DDR_MCU3_0_IPC_ADDR (0xA6000000u)
-#define DDR_MCU3_0_IPC_SIZE (0x00100000u)
-
-/* DDR for MCU3_0 for all sections, used for reserving memory in DTS file [ size 15.00 MB ] */
-#define DDR_MCU3_0_DTS_ADDR (0xA6100000u)
-#define DDR_MCU3_0_DTS_SIZE (0x00F00000u)
-
-/* DDR for MCU3_1 for Linux IPC [ size 1024.00 KB ] */
-#define DDR_MCU3_1_IPC_ADDR (0xA7000000u)
-#define DDR_MCU3_1_IPC_SIZE (0x00100000u)
-
-/* DDR for MCU3_1 for all sections, used for reserving memory in DTS file [ size 15.00 MB ] */
-#define DDR_MCU3_1_DTS_ADDR (0xA7100000u)
-#define DDR_MCU3_1_DTS_SIZE (0x00F00000u)
-
/* Memory for IPC Vring's. MUST be non-cached or cache-coherent [ size 32.00 MB ] */
#define IPC_VRING_MEM_ADDR (0xA8000000u)
#define IPC_VRING_MEM_SIZE (0x02000000u)
@@ -195,14 +179,6 @@
#define DDR_MCU2_1_LOCAL_HEAP_ADDR (0xDA000000u)
#define DDR_MCU2_1_LOCAL_HEAP_SIZE (0x01000000u)
-/* DDR for MCU3_0 for local heap [ size 8.00 MB ] */
-#define DDR_MCU3_0_LOCAL_HEAP_ADDR (0xDB000000u)
-#define DDR_MCU3_0_LOCAL_HEAP_SIZE (0x00800000u)
-
-/* DDR for MCU3_1 for local heap [ size 8.00 MB ] */
-#define DDR_MCU3_1_LOCAL_HEAP_ADDR (0xDB800000u)
-#define DDR_MCU3_1_LOCAL_HEAP_SIZE (0x00800000u)
-
/* DDR for c7x_1 for Scratch Memory [ size 368.00 MB ] */
#define DDR_C7X_1_SCRATCH_ADDR (0x100000000u)
#define DDR_C7X_1_SCRATCH_SIZE (0x17000000u)
diff --git a/platform/j721s2/rtos/gen_linker_mem_map.py b/platform/j721s2/rtos/gen_linker_mem_map.py
index 56725bc..c19fd69 100755
--- a/platform/j721s2/rtos/gen_linker_mem_map.py
+++ b/platform/j721s2/rtos/gen_linker_mem_map.py
@@ -79,7 +79,7 @@
# This will generate linker command file at below folders
# ./<cpu name>/linker_mem_map.cmd
#
-# Here CPU name is mpu1, c7x_1, c7x_2, mcu1_0, mcu2_0, mcu3_0
+# Here CPU name is mpu1, c7x_1, c7x_2, mcu1_0, mcu2_0
#
#
from ti_psdk_rtos_tools import *
@@ -193,16 +193,6 @@ mcu2_1_ddr_resource_table_addr = mcu2_1_ddr_ipc_addr + linux_ddr_ipc_size;
mcu2_1_ddr_addr = mcu2_1_ddr_resource_table_addr + linux_ddr_resource_table_size;
mcu2_1_ddr_size = 32*MB - (mcu2_1_ddr_addr-mcu2_1_ddr_ipc_addr);
-mcu3_0_ddr_ipc_addr = mcu2_1_ddr_addr + mcu2_1_ddr_size;
-mcu3_0_ddr_resource_table_addr = mcu3_0_ddr_ipc_addr + linux_ddr_ipc_size;
-mcu3_0_ddr_addr = mcu3_0_ddr_resource_table_addr + linux_ddr_resource_table_size;
-mcu3_0_ddr_size = 16*MB - (mcu3_0_ddr_addr-mcu3_0_ddr_ipc_addr);
-
-mcu3_1_ddr_ipc_addr = mcu3_0_ddr_addr + mcu3_0_ddr_size;
-mcu3_1_ddr_resource_table_addr = mcu3_1_ddr_ipc_addr + linux_ddr_ipc_size;
-mcu3_1_ddr_addr = mcu3_1_ddr_resource_table_addr + linux_ddr_resource_table_size;
-mcu3_1_ddr_size = 16*MB - (mcu3_1_ddr_addr-mcu3_1_ddr_ipc_addr);
-
#
# DDR memory allocation for various shared memories
#
@@ -253,10 +243,6 @@ mcu2_0_ddr_local_heap_addr = mcu1_1_ddr_local_heap_addr + mcu1_1_ddr_local_heap
mcu2_0_ddr_local_heap_size = 16*MB;
mcu2_1_ddr_local_heap_addr = mcu2_0_ddr_local_heap_addr + mcu2_0_ddr_local_heap_size;
mcu2_1_ddr_local_heap_size = 16*MB;
-mcu3_0_ddr_local_heap_addr = mcu2_1_ddr_local_heap_addr + mcu2_1_ddr_local_heap_size;
-mcu3_0_ddr_local_heap_size = 8*MB;
-mcu3_1_ddr_local_heap_addr = mcu3_0_ddr_local_heap_addr + mcu3_0_ddr_local_heap_size;
-mcu3_1_ddr_local_heap_size = 8*MB;
c7x_1_ddr_scratch_addr = ddr_mem_addr_hi;
c7x_1_ddr_scratch_size = 368*MB;
@@ -343,26 +329,6 @@ mcu2_1_ddr_total.concat(mcu2_1_ddr_resource_table);
mcu2_1_ddr_total.concat(mcu2_1_ddr);
mcu2_1_ddr_total.setDtsName("vision_apps_main_r5fss0_core1_memory_region", "vision-apps-r5f-memory");
-mcu3_0_ddr_ipc = MemSection("DDR_MCU3_0_IPC", "RWIX", mcu3_0_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for MCU3_0 for Linux IPC");
-mcu3_0_ddr_ipc.setDtsName("vision_apps_main_r5fss1_core0_dma_memory_region", "vision-apps-r5f-dma-memory");
-mcu3_0_ddr_resource_table = MemSection("DDR_MCU3_0_RESOURCE_TABLE", "RWIX", mcu3_0_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for MCU3_0 for Linux resource table");
-mcu3_0_ddr = MemSection("DDR_MCU3_0", "RWIX", mcu3_0_ddr_addr, mcu3_0_ddr_size, "DDR for MCU3_0 for code/data");
-mcu3_0_ddr_local_heap = MemSection("DDR_MCU3_0_LOCAL_HEAP", "RWIX", mcu3_0_ddr_local_heap_addr, mcu3_0_ddr_local_heap_size, "DDR for MCU3_0 for local heap");
-mcu3_0_ddr_total = MemSection("DDR_MCU3_0_DTS", "", 0, 0, "DDR for MCU3_0 for all sections, used for reserving memory in DTS file");
-mcu3_0_ddr_total.concat(mcu3_0_ddr_resource_table);
-mcu3_0_ddr_total.concat(mcu3_0_ddr);
-mcu3_0_ddr_total.setDtsName("vision_apps_main_r5fss1_core0_memory_region", "vision-apps-r5f-memory");
-
-mcu3_1_ddr_ipc = MemSection("DDR_MCU3_1_IPC", "RWIX", mcu3_1_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for MCU3_1 for Linux IPC");
-mcu3_1_ddr_ipc.setDtsName("vision_apps_main_r5fss1_core1_dma_memory_region", "vision-apps-r5f-dma-memory");
-mcu3_1_ddr_resource_table = MemSection("DDR_MCU3_1_RESOURCE_TABLE", "RWIX", mcu3_1_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for MCU3_1 for Linux resource table");
-mcu3_1_ddr = MemSection("DDR_MCU3_1", "RWIX", mcu3_1_ddr_addr, mcu3_1_ddr_size, "DDR for MCU3_1 for code/data");
-mcu3_1_ddr_local_heap = MemSection("DDR_MCU3_1_LOCAL_HEAP", "RWIX", mcu3_1_ddr_local_heap_addr, mcu3_1_ddr_local_heap_size, "DDR for MCU3_1 for local heap");
-mcu3_1_ddr_total = MemSection("DDR_MCU3_1_DTS", "", 0, 0, "DDR for MCU3_1 for all sections, used for reserving memory in DTS file");
-mcu3_1_ddr_total.concat(mcu3_1_ddr_resource_table);
-mcu3_1_ddr_total.concat(mcu3_1_ddr);
-mcu3_1_ddr_total.setDtsName("vision_apps_main_r5fss1_core1_memory_region", "vision-apps-r5f-memory");
-
c7x_2_ddr_ipc = MemSection("DDR_C7x_2_IPC", "RWIX", c7x_2_ddr_ipc_addr, linux_ddr_ipc_size, "DDR for C7x_2 for Linux IPC");
c7x_2_ddr_ipc.setDtsName("vision_apps_c71_1_dma_memory_region", "vision-apps-c71_1-dma-memory");
c7x_2_ddr_resource_table = MemSection("DDR_C7x_2_RESOURCE_TABLE", "RWIX", c7x_2_ddr_resource_table_addr, linux_ddr_resource_table_size, "DDR for C7x_2 for Linux resource table");
@@ -422,8 +388,6 @@ vision_apps_core_heaps_lo = MemSection("DDR_VISION_APPS_CORE_HEAPS_LO_DTS", "",
vision_apps_core_heaps_lo.concat(mcu1_0_ddr_local_heap);
vision_apps_core_heaps_lo.concat(mcu2_0_ddr_local_heap);
vision_apps_core_heaps_lo.concat(mcu2_1_ddr_local_heap);
-vision_apps_core_heaps_lo.concat(mcu3_0_ddr_local_heap);
-vision_apps_core_heaps_lo.concat(mcu3_1_ddr_local_heap);
vision_apps_core_heaps_lo.setDtsName("vision_apps_core_heaps_lo", "vision-apps-core-heap-memory-lo");
c7x_1_ddr_local_heap_phy = MemSection("DDR_C7X_1_LOCAL_HEAP", "RWIX", ddr_mem_addr_hi_phy, (c7x_1_ddr_scratch_size + c7x_1_ddr_local_heap_size + c7x_2_ddr_scratch_size + c7x_2_ddr_local_heap_size), "DDR for c7x_1, c7x_2 for scratch memory and local heap");
@@ -498,34 +462,6 @@ mcu2_1_mmap.addMemSection( ddr_shared_mem );
mcu2_1_mmap.addMemSection( mcu2_1_main_ocram );
mcu2_1_mmap.checkOverlap();
-mcu3_0_mmap = MemoryMap("mcu3_0");
-mcu3_0_mmap.addMemSection( mcu_r5f_tcma_vecs );
-mcu3_0_mmap.addMemSection( mcu_r5f_tcma );
-mcu3_0_mmap.addMemSection( r5f_tcmb0 );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr_ipc );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr_resource_table );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr );
-mcu3_0_mmap.addMemSection( app_log_mem );
-mcu3_0_mmap.addMemSection( tiovx_obj_desc_mem );
-mcu3_0_mmap.addMemSection( ipc_vring_mem );
-mcu3_0_mmap.addMemSection( mcu3_0_ddr_local_heap );
-mcu3_0_mmap.addMemSection( ddr_shared_mem );
-mcu3_0_mmap.checkOverlap();
-
-mcu3_1_mmap = MemoryMap("mcu3_1");
-mcu3_1_mmap.addMemSection( mcu_r5f_tcma_vecs );
-mcu3_1_mmap.addMemSection( mcu_r5f_tcma );
-mcu3_1_mmap.addMemSection( r5f_tcmb0 );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr_ipc );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr_resource_table );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr );
-mcu3_1_mmap.addMemSection( app_log_mem );
-mcu3_1_mmap.addMemSection( tiovx_obj_desc_mem );
-mcu3_1_mmap.addMemSection( ipc_vring_mem );
-mcu3_1_mmap.addMemSection( mcu3_1_ddr_local_heap );
-mcu3_1_mmap.addMemSection( ddr_shared_mem );
-mcu3_1_mmap.checkOverlap();
-
c7x_1_mmap = MemoryMap("c7x_1");
c7x_1_mmap.addMemSection( c7x_1_l2 );
c7x_1_mmap.addMemSection( c7x_1_l1 );
@@ -585,14 +521,6 @@ html_mmap.addMemSection( mcu2_1_ddr_ipc );
html_mmap.addMemSection( mcu2_1_ddr_resource_table );
html_mmap.addMemSection( mcu2_1_ddr );
html_mmap.addMemSection( mcu2_1_ddr_local_heap );
-html_mmap.addMemSection( mcu3_0_ddr_ipc );
-html_mmap.addMemSection( mcu3_0_ddr_resource_table );
-html_mmap.addMemSection( mcu3_0_ddr );
-html_mmap.addMemSection( mcu3_0_ddr_local_heap );
-html_mmap.addMemSection( mcu3_1_ddr_ipc );
-html_mmap.addMemSection( mcu3_1_ddr_resource_table );
-html_mmap.addMemSection( mcu3_1_ddr );
-html_mmap.addMemSection( mcu3_1_ddr_local_heap );
html_mmap.addMemSection( c7x_1_ddr_ipc );
html_mmap.addMemSection( c7x_1_ddr_resource_table );
html_mmap.addMemSection( c7x_1_ddr_boot );
@@ -628,16 +556,12 @@ c_header_mmap.addMemSection( mcu1_0_ddr_ipc );
c_header_mmap.addMemSection( mcu1_1_ddr_ipc );
c_header_mmap.addMemSection( mcu2_0_ddr_ipc );
c_header_mmap.addMemSection( mcu2_1_ddr_ipc );
-c_header_mmap.addMemSection( mcu3_0_ddr_ipc );
-c_header_mmap.addMemSection( mcu3_1_ddr_ipc );
c_header_mmap.addMemSection( c7x_1_ddr_ipc );
c_header_mmap.addMemSection( c7x_2_ddr_ipc );
c_header_mmap.addMemSection( mcu1_0_ddr_total );
c_header_mmap.addMemSection( mcu1_1_ddr_total );
c_header_mmap.addMemSection( mcu2_0_ddr_total );
c_header_mmap.addMemSection( mcu2_1_ddr_total );
-c_header_mmap.addMemSection( mcu3_0_ddr_total );
-c_header_mmap.addMemSection( mcu3_1_ddr_total );
c_header_mmap.addMemSection( c7x_1_ddr_total );
c_header_mmap.addMemSection( c7x_2_ddr_total );
@@ -645,8 +569,6 @@ c_header_mmap.addMemSection( mcu1_0_ddr_local_heap);
c_header_mmap.addMemSection( mcu1_1_ddr_local_heap);
c_header_mmap.addMemSection( mcu2_0_ddr_local_heap);
c_header_mmap.addMemSection( mcu2_1_ddr_local_heap);
-c_header_mmap.addMemSection( mcu3_0_ddr_local_heap);
-c_header_mmap.addMemSection( mcu3_1_ddr_local_heap);
c_header_mmap.addMemSection( c7x_1_ddr_local_heap);
c_header_mmap.addMemSection( c7x_1_ddr_scratch);
c_header_mmap.addMemSection( c7x_2_ddr_local_heap);
@@ -672,10 +594,6 @@ dts_mmap.addMemSection( mcu2_0_ddr_ipc );
dts_mmap.addMemSection( mcu2_0_ddr_total );
dts_mmap.addMemSection( mcu2_1_ddr_ipc );
dts_mmap.addMemSection( mcu2_1_ddr_total );
-dts_mmap.addMemSection( mcu3_0_ddr_ipc );
-dts_mmap.addMemSection( mcu3_0_ddr_total );
-dts_mmap.addMemSection( mcu3_1_ddr_ipc );
-dts_mmap.addMemSection( mcu3_1_ddr_total );
dts_mmap.addMemSection( c7x_1_ddr_ipc );
dts_mmap.addMemSection( c7x_1_ddr_total );
dts_mmap.addMemSection( c7x_2_ddr_ipc );
@@ -696,8 +614,6 @@ LinkerCmdFile(mcu1_0_mmap, "./mcu1_0/linker_mem_map.cmd").export();
LinkerCmdFile(mcu1_1_mmap, "./mcu1_1/linker_mem_map.cmd").export();
LinkerCmdFile(mcu2_0_mmap, "./mcu2_0/linker_mem_map.cmd").export();
LinkerCmdFile(mcu2_1_mmap, "./mcu2_1/linker_mem_map.cmd").export();
-LinkerCmdFile(mcu3_0_mmap, "./mcu3_0/linker_mem_map.cmd").export();
-LinkerCmdFile(mcu3_1_mmap, "./mcu3_1/linker_mem_map.cmd").export();
HtmlMmapTable(html_mmap, "./system_memory_map.html").export();
diff --git a/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi b/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi
index 86855a6..214590f 100644
--- a/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi
+++ b/platform/j721s2/rtos/k3-j721s2-rtos-memory-map.dtsi
@@ -4,7 +4,7 @@
* IMPORTANT NOTE: Follow below instructions to apply the updated memory map to linux dtsi file,
*
* 1. Copy the memory sections, from the generated dts file, to the file shown below under reserved_memory: reserved-memory { ... }
- * ${LINUX_KERNEL_PATH}/arch/arm64/boot/dts/ti/k3-j721s2-rtos-memory-map.dtsi
+ * ${LINUX_KERNEL_PATH}/arch/arm64/boot/dts/ti/k3-j721e-rtos-memory-map.dtsi
*
* 2. Rebuild the dtb, dtbo from PSDK Linux install directory
* make linux-dtbs
@@ -55,26 +55,6 @@
reg = <0x00 0xa4100000 0x00 0x01f00000>;
no-map;
};
- vision_apps_main_r5fss1_core0_dma_memory_region: vision-apps-r5f-dma-memory@a6000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa6000000 0x00 0x00100000>;
- no-map;
- };
- vision_apps_main_r5fss1_core0_memory_region: vision-apps-r5f-memory@a6100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa6100000 0x00 0x00f00000>;
- no-map;
- };
- vision_apps_main_r5fss1_core1_dma_memory_region: vision-apps-r5f-dma-memory@a7000000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa7000000 0x00 0x00100000>;
- no-map;
- };
- vision_apps_main_r5fss1_core1_memory_region: vision-apps-r5f-memory@a7100000 {
- compatible = "shared-dma-pool";
- reg = <0x00 0xa7100000 0x00 0x00f00000>;
- no-map;
- };
vision_apps_rtos_ipc_memory_region: vision-apps-rtos-ipc-memory-region@a8000000 {
compatible = "shared-dma-pool";
reg = <0x00 0xa8000000 0x00 0x02000000>;
@@ -111,7 +91,7 @@
};
vision_apps_core_heaps_lo: vision-apps-core-heap-memory-lo@d8000000 {
compatible = "shared-dma-pool";
- reg = <0x00 0xd8000000 0x00 0x04000000>;
+ reg = <0x00 0xd8000000 0x00 0x03000000>;
no-map;
};
vision_apps_core_heaps_hi: vision-apps-core-heap-memory-hi@880000000 {
diff --git a/platform/j721s2/rtos/system_memory_map.html b/platform/j721s2/rtos/system_memory_map.html
index 1859f9b..57d49f5 100644
--- a/platform/j721s2/rtos/system_memory_map.html
+++ b/platform/j721s2/rtos/system_memory_map.html
@@ -192,54 +192,6 @@
<td class="tg-kftd">RWIX</td>
<td class="tg-kftd">DDR for MCU2_1 for code/data</td>
</tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_0_IPC</td>
- <td class="tg-6sgx">0xA6000000</td>
- <td class="tg-6sgx">0xA60FFFFF</td>
- <td class="tg-6sgx">1024.00 KB</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_0 for Linux IPC</td>
- </tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_0_RESOURCE_TABLE</td>
- <td class="tg-kftd">0xA6100000</td>
- <td class="tg-kftd">0xA61003FF</td>
- <td class="tg-kftd">1024 B</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_0 for Linux resource table</td>
- </tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_0</td>
- <td class="tg-6sgx">0xA6100400</td>
- <td class="tg-6sgx">0xA6FFFFFF</td>
- <td class="tg-6sgx">15.00 MB</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_0 for code/data</td>
- </tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_1_IPC</td>
- <td class="tg-kftd">0xA7000000</td>
- <td class="tg-kftd">0xA70FFFFF</td>
- <td class="tg-kftd">1024.00 KB</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_1 for Linux IPC</td>
- </tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_1_RESOURCE_TABLE</td>
- <td class="tg-6sgx">0xA7100000</td>
- <td class="tg-6sgx">0xA71003FF</td>
- <td class="tg-6sgx">1024 B</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_1 for Linux resource table</td>
- </tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_1</td>
- <td class="tg-kftd">0xA7100400</td>
- <td class="tg-kftd">0xA7FFFFFF</td>
- <td class="tg-kftd">15.00 MB</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_1 for code/data</td>
- </tr>
<tr>
<td class="tg-6sgx">IPC_VRING_MEM</td>
<td class="tg-6sgx">0xA8000000</td>
@@ -408,22 +360,6 @@
<td class="tg-6sgx">RWIX</td>
<td class="tg-6sgx">DDR for MCU2_1 for local heap</td>
</tr>
- <tr>
- <td class="tg-kftd">DDR_MCU3_0_LOCAL_HEAP</td>
- <td class="tg-kftd">0xDB000000</td>
- <td class="tg-kftd">0xDB7FFFFF</td>
- <td class="tg-kftd"> 8.00 MB</td>
- <td class="tg-kftd">RWIX</td>
- <td class="tg-kftd">DDR for MCU3_0 for local heap</td>
- </tr>
- <tr>
- <td class="tg-6sgx">DDR_MCU3_1_LOCAL_HEAP</td>
- <td class="tg-6sgx">0xDB800000</td>
- <td class="tg-6sgx">0xDBFFFFFF</td>
- <td class="tg-6sgx"> 8.00 MB</td>
- <td class="tg-6sgx">RWIX</td>
- <td class="tg-6sgx">DDR for MCU3_1 for local heap</td>
- </tr>
<tr>
<td class="tg-kftd">DDR_C7X_1_SCRATCH</td>
<td class="tg-kftd">0x100000000</td>
Builds Required
cd ${PSDKLA}/
make linux-dtbs
Assuming SOC as J721s2 (SDK 8.6)
To Build vision_apps
=====================
cd ${PSDKRA}/vision_apps
make vision_apps_scrub
make vision_apps
To Build combined_app image
============================
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/boot/sbl/tools/combined_appimage/
make clean BOARD=j721s2_evm
make BOARD=j721s2_evm HLOS_BOOT=optimized
Verification Command:
cat /proc/interrupts
Output:
The main-r5fss1-core0 interrupt is not seen upon the input of the command
4. Removal of Drivers for the disabled IP (GPU, EDP, CSITX etc..)
There would be requirements for the subset devices to remove few hardware IP.
For example:
a) the subset analytics devices like TDA4AL, the GPU is not available. Hence to remove the GPU support from the SDK, the changes are required on the u-boot and Linux kernel as shown below.
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
index 69216fe05..8ee1a470e 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
@@ -288,16 +288,6 @@
power-domains = <&k3_pds 358 TI_SCI_PD_EXCLUSIVE>;
};
- gpu: gpu@4e20000000 {
- compatible = "ti,j721s2-pvr", "img,pvr-bxs64";
- reg = <0x4e 0x20000000 0x00 0x80000>;
- interrupts = <GIC_SPI 24 IRQ_TYPE_LEVEL_HIGH>;
- power-domains = <&k3_pds 130 TI_SCI_PD_EXCLUSIVE>,
- <&k3_pds 373 TI_SCI_PD_EXCLUSIVE>;
- power-domain-names = "gpu_0", "gpucore_0";
- clocks = <&k3_clks 130 1>;
- };
-
main_gpio0: gpio@600000 {
compatible = "ti,j721e-gpio", "ti,keystone-gpio";
reg = <0x00 0x00600000 0x00 0x100>;
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2.dtsi b/arch/arm64/boot/dts/ti/k3-j721s2.dtsi
index 75bc8dfac..dd2f0ebc8 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-j721s2.dtsi
@@ -122,7 +122,6 @@
<0x00 0x70000000 0x00 0x70000000 0x00 0x00400000>, /* MSMC RAM */
<0x00 0x30000000 0x00 0x30000000 0x00 0x0c400000>, /* MAIN NAVSS */
<0x41 0x00000000 0x41 0x00000000 0x01 0x00000000>, /* PCIe1 DAT1 */
- <0x4e 0x20000000 0x4e 0x20000000 0x00 0x00080000>, /* GPU */
/* MCUSS_WKUP Range */
<0x00 0x28380000 0x00 0x28380000 0x00 0x03880000>,
Builds Required
cd ${PSDKLA}/
make linux-dtbs
Assuming SOC as J721s2 (SDK 8.6)
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/boot/sbl/tools/combined_appimage/
make clean BOARD=j721s2_evm
make BOARD=j721s2_evm HLOS_BOOT=optimized
Verification Command:
devmem2 0x4E20000018
Output:
Kernel Crash
b) For some subset analytics devices like TDA4AL88, the EDP support is not available. Hence to remove the EDP support from the SDK, the changes are required on the Linux kernel as shown below.
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts b/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
index b6158a27f..a8ad37a9a 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
+++ b/arch/arm64/boot/dts/ti/k3-j721s2-common-proc-board.dts
@@ -148,19 +148,6 @@
regulator-always-on;
};
- dp0: dp0-connector {
- compatible = "dp-connector";
- label = "DP0";
- type = "full-size";
- dp-pwr-supply = <&dp0_pwr_3v3>;
-
- port {
- dp0_connector_in: endpoint {
- remote-endpoint = <&dp0_out>;
- };
- };
- };
-
panel {
compatible = "ti,panel-edp";
power-supply = <&dp1_pwr_3v3>;
@@ -626,13 +613,6 @@
#address-cells = <1>;
#size-cells = <0>;
- port@0 {
- reg = <0>;
- dpi0_out: endpoint {
- remote-endpoint = <&dp0_in>;
- };
- };
-
port@2 {
reg = <2>;
dpi2_out: endpoint {
@@ -673,31 +653,6 @@
};
};
-&mhdp {
- pinctrl-names = "default";
- pinctrl-0 = <&dp0_pins_default>;
- cdns,no-hpd;
-};
-
-&dp0_ports {
- #address-cells = <1>;
- #size-cells = <0>;
-
- port@0 {
- reg = <0>;
- dp0_in: endpoint {
- remote-endpoint = <&dpi0_out>;
- };
- };
-
- port@4 {
- reg = <4>;
- dp0_out: endpoint {
- remote-endpoint = <&dp0_connector_in>;
- };
- };
-};
-
&main_mcan0 {
status = "disabled";
};
diff --git a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
index 69216fe05..8ee1a470e 100644
--- a/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-j721s2-main.dtsi
@@ -1493,32 +1443,6 @@
power-domains = <&k3_pds 346 TI_SCI_PD_EXCLUSIVE>;
};
- mhdp: dp-bridge@a000000 {
- compatible = "ti,j721e-mhdp8546";
- /*
- * Note: we do not map DPTX PHY area, as that is handled by
- * the PHY driver.
- */
- reg = <0x0 0xa000000 0x0 0x30a00>, /* DSS_EDP0_V2A_CORE_VP_REGS_APB */
- <0x0 0x4f40000 0x0 0x20>; /* DSS_EDP0_INTG_CFG_VP */
- reg-names = "mhdptx", "j721e-intg";
-
- clocks = <&k3_clks 156 19>;
-
- phys = <&torrent_phy_dp>;
- phy-names = "dpphy";
-
- interrupt-parent = <&gic500>;
- interrupts = <GIC_SPI 614 IRQ_TYPE_LEVEL_HIGH>;
-
- power-domains = <&k3_pds 156 TI_SCI_PD_EXCLUSIVE>;
-
- dp0_ports: ports {
- #address-cells = <1>;
- #size-cells = <0>;
- };
- };
-
dphy0: phy@4480000 {
compatible = "ti,j721e-dphy";
reg = <0x0 0x04480000 0x0 0x1000>;
diff --git a/packages/ti/board/src/j721s2_evm/board_clock.c b/packages/ti/board/src/j721s2_evm/board_clock.c
index b7e6faf..7250703 100644
--- a/packages/ti/board/src/j721s2_evm/board_clock.c
+++ b/packages/ti/board/src/j721s2_evm/board_clock.c
@@ -211,7 +209,6 @@ uint32_t gBoardClkModuleMainIDGroup2[] = {
TISCI_DEV_DPHY_RX1,
TISCI_DEV_DSS_DSI0,
TISCI_DEV_DSS_DSI1,
- TISCI_DEV_DSS_EDP0,
TISCI_DEV_DSS0,
TISCI_DEV_DPHY_TX0,
TISCI_DEV_DPHY_TX1
diff --git a/platform/j721s2/rtos/common/app_cfg_mcu2_0.h b/platform/j721s2/rtos/common/app_cfg_mcu2_0.h
index 78e57f3..0fdfc7f 100755
--- a/platform/j721s2/rtos/common/app_cfg_mcu2_0.h
+++ b/platform/j721s2/rtos/common/app_cfg_mcu2_0.h
@@ -84,12 +84,12 @@
* - When ENABLE_DSS_SINGLE is defined, only one of ENABLE_DSS_HDMI or ENABLE_DSS_EDP should be defined
* - When ENABLE_DSS_DUAL is defined, ENABLE_DSS_HDMI and ENABLE_DSS_EDP are not used, both EDP and HDMI are enabled unconditionally
*/
- #define ENABLE_DSS_SINGLE
+ #undef ENABLE_DSS_SINGLE
#undef ENABLE_DSS_DUAL
/* define below to enable eDP display,
make sure to undef ENABLE_DSS_HDMI & ENABLE_DSS_DSI as well */
- #define ENABLE_DSS_EDP
+ #undef ENABLE_DSS_EDP
/* define below to enable HDMI display,
make sure to undef ENABLE_DSS_EDP & ENABLE_DSS_DSI as well */
#undef ENABLE_DSS_HDMI
Builds Required
cd ${PSDKLA}/
make linux-dtbs
Assuming the SOC is J721s2 (SDK 8.6)
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/build/
make pdk_libs_clean BOARD=j721s2_evm
make pdk_libs BOARD=j721s2_evm
Assuming the SOC is J721s2 (SDK 8.6), Default SBL with MMCSD boot media
For custom SBL and different boot media, please adapt the build commands accordingly
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/build/
make sbl_lib_mmcsd_hlos_clean BOARD=j721s2_evm
make sbl_mmcsd_img_hlos_clean BOARD=j721s2_evm
make sbl_lib_mmcsd_hlos BOARD=j721s2_evm
make sbl_mmcsd_img_hlos BOARD=j721s2_evm
Assuming SOC as J721s2 (SDK 8.6)
To Build vision_apps
=====================
cd ${PSDKRA}/vision_apps
make vision_apps_scrub
make vision_apps
To Build combined_app image
============================
cd ${PSDKRA}/pdk_j721s2_08_06_00_31/packages/ti/boot/sbl/tools/combined_appimage/
make clean BOARD=j721s2_evm
make BOARD=j721s2_evm HLOS_BOOT=optimized
Verification Command:
devmem2 0x04F4001C
Output:
Kernel Crash