This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM6x to DP83867IR: How to read/write register values in DP83867 with addresses above 0x001F?

Part Number: DP83867IR


Problem Statement:

Hi Expert,

How to read/write register values in DP83867 with addresses above 0x001F?

Regards

  • Solution:

    Addresses above 0x001F falls under extended register set and they are accessed using indirect addressing via registers REGCR(0x000D) and ADDAR(0x000E).

    REGCR: Register Control Register [0x000D]

    BIT

    BIT NAME

    DEFAULT

    DESCRIPTION

    15:14

    Function

    0, RW

    00 = Address

    01 = Data, no post increment

    10 = Data, post increment on read and write

    11 = Data, post increment on write only

    13:5

    RESERVED

    0, RO

    RESERVED: Writes ignored, read as 0

    4:0

    DEVAD

    0, RW

    Device Address:  bits [4:0], directs any accesses of ADDAR register (0x000E) to appropriate MMD. DP83867 uses vendor specific DEVAD [4:0] = 1111 for accesses.

    All accesses through registers REGCR and ADDAR should use this DEVAD. Transactions with other DEVAD are ignored.

    ADDAR: Address or Data Register [0x000E]

    BIT

    BIT NAME

    DEFAULT

    DESCRIPTION

    15:0

    Address/Data

    0, RW

    If REGCR register 15:14 = 00, holds MMD DEVAD’s address register, otherwise holds MMD DEVAD’s data register.

    Bit setting of REGCR defines the working of ADDAR register as containing address value or data value.

    • If value contained in REGCR = 0x001F -> ADDAR will contain address of the targeted register.
    • If value contained in REGCR = 0x401F -> ADDAR will contain value at the targeted register address.

    Steps to follow for editing these register values:

    {E.g. : Assigning value 0x0480 to address location 0x0025}

    S.No.

    Step

    Respective Command

    1.

    Set REGCR = 0x001F

    phytool ethX/0x0/0x000D 0x001F

     

    2.

    Set ADDAR to point to address of targeted register = 0x0025

    phytool ethX/0x0/0x000E 0x0025

     

    3.

    Set REGCR = 0x401F

    phytool ethX/0x0/0x000D 0x401F

     

    4.

    Set ADDAR to value to be assigned to the location previously pointed by ADDAR

     

    phytol ethX/0x0/0x000E 0x0480

     

    To read the value of a register in extended register set:

    S.No.

    Step

    Respective Command

    1.

    Set REGCR = 0x001F [ADDAR address mode]

     

    phytool ethX/0x0/0x000D 0x001F

    2.

    ADDAR = 0x0025 (pointing to address of the register to be read)

    phytool ethX/0x0/0x000E 0x0025

     

    3.

    Set REGCR = 0x401F [ADDAR data mode]

     

    phytool ethX/0x0/0x000D 0x401F

     

    4.

    Read ADDAR

    phytool read ethX/0x0/0x000E.

     

    Thanks & Regards

    Rimika