Other Parts Discussed in Thread: SYSCONFIG
Hi,
Can you please recommend how should I perform memory placement of various SW components when using Profinet - TSN on the AM64x processor.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please recommend how should I perform memory placement of various SW components when using Profinet - TSN on the AM64x processor.
Hi,
This document explains the MCU+ SDK and Profinet component placement recommendation on different memory controller (DDR/MSMC/TCM) for Sitara AM64x platform.
| Component | Sub Component | Description | Alignment | MPU Settings | Section | Comments |
| ENET | ENET_DMA_RING_M EMPOOL |
This is DMA ring accelerator memory pool. Each ring contains four memory spaces on the VBUSM target bus for access, each of which is 512 bytes long, with a total of 4 kB per ring. Each ring space starts immediately after the preceding ring. |
128U - Cache alignm ent |
Cacheable: 1 Bufferable: 1 Shareable: 0 |
.bss | Note: the memory alignment described here is the default configuration and part of sysconfig generated file ti_enet_config.c. Refer below macro. ENETDMA_CACHELINE_ALIGNMENT UDMA_CACHELINE_ALIGNMENT |
| ENET_DMA_DESC_M EMPOOL |
This is DMA descriptor memory pool. |
32U - Cache alignm ent |
Cacheable: 1 Bufferable: 1 Shareable: 0 |
.bss | This subcomponent can be placed in MSMC/DDR target memory and MPU settings should be strictly followed. | |
| ENET_DMA_PKT_ME MPOOL |
Large/medium/small packet memory pools. This is application packet memory pool contains actual eth packets. |
32U - Cache alignm ent |
Cacheable: 1 Bufferable: 1 Shareable: 0 |
.bss | ||
| ICSSG | Firmware - icssfw | ICSSG Firmware headers - for switch and DUAL MAC |
128U | Cacheable: 1 Bufferable: 1 Shareable: 0 |
.rodata | This subcomponent has to be placed in MSMC target memory. |
| host buffer pool | Host buffer pool memory |
64U |
Cacheable: 1 >> NOLOAD |
.bss | Note: the memory alignment described here is the default configuration and part of sysconfig generated file ti_enet_config.c Refer below macro: ICSSG_CACHELINE_ALIGNMENT This subcomponent has to be placed in MSMC target memory. |
|
| host queue memory pool |
Host egress queue memory |
64U |
Cacheable: 1 >> NOLOAD |
.bss | Note: the memory alignment described here is the default configuration and part of sysconfig generated file ti_enet_config.c Refer below macro: ICSSG_CACHELINE_ALIGNMENT This subcomponent has to be placed in MSMC target memory. |
|
| Port buffer pool | Port buffer pool memory |
64U |
Cacheable: 1 >> NOLOAD |
.bss | Note: the memory alignment described here is the default configuration and part of sysconfig generated file ti_enet_config.c Refer below macro: ICSSG_CACHELINE_ALIGNMENT. This subcomponent has to be placed in MSMC target memory. |
|
| Scratch buffer | Scratch buffer used for error and large size frames. |
64U |
Cacheable: 1 >> NOLOAD |
.bss | Note: the memory alignment described here is the default configuration and part of sysconfig generated file ti_enet_config.c Refer below macro: ICSSG_CACHELINE_ALIGNMENT. This subcomponent has to be placed in MSMC target memory. | |
| Profinet - PPM buffers |
PPM buffer and TRPD list |
PPM buffers - application buffer for storing IO data. PPM TRPD list - BCDMA block copy transfer request descriptors |
128U |
Cacheable: 1 >> NOLOAD |
.bss | PPM buffers = Max AR * Max PPM buffer size Refer: rt_msmc_mem in linkercmd file |
| freeRTOS | Boot code | GROUP: hwi, cache, mpu, boot: freeRTOS IRQ handlers, hardware interrupt module and boot code |
8 |
Cacheable: 1 |
.text | |
| R5F entry table and vector |
R5F HWIP |
8 |
Cacheable: 1 |
.vectors | ||
| ARM | IRQ, FIQ, SVC, ABORT and UNDEFINED stack |
GROUP: All the arm r5f stacks for different modes |
8 |
Cacheable: 1 |
||
| SBL |
Boot loader: 0-512KB (2 |
- |
|
In this bank .text or .rodata cannot be placed. Otherwise, this region can also be used for application stack, heap or firmware buffers (refer ICSSG component and buffer pool sub component) | ||
|
Rest of code, initialized/uninitialized data, uninitialized global variables, |
GROUP: All the un-initialized global variables |
8 |
Cacheable: 1 |
.bss |
These subcomponents can be placed in MSMC/DDR target memory and MPU settings should be strictly followed. |
|
| GROUP: Heap and stack |
8 |
Cacheable: 1 |
.system .stack |
|||
| GROUP: Text and read only data |
8 |
Cacheable: 1 |
.text .rodata |
|||
| GROUP: data - initialized data |
8 |
Cacheable: 1 |
.data |
| Memory | Region Name | Region Start | Length | MPU Settings | Description |
| MSRAM (Multicore Shared Memory Controller) | MSMC_cached | 0x70000000 | 0x1e0000 | Cacheable: 1 Bufferable: 1 Shareable: 0 |
|
| MSMC_uncached | 0x701e0000 | 0x0C0000 | Cacheable: 0 Bufferable: 1 Shareable: 1 |
||
| DDR4 | DDR_cached | 0x86000000 | 0x01800000 | Cacheable: 1 Bufferable: 1 Shareable: 0 |
|
| DDR_uncached | 0x87800000 | 0x00400000 | Cacheable: 0 Bufferable: 1 Shareable: 1 |
||
| Flash | 0x60100000 | 0x80000 | Cacheable: 1 Bufferable: 1 Shareable: 1 |
This section can be used to put XIP section of the application in flash, make sure this does not overlap with other CPUs. Also make sure to add a MPU entry for this section and mark it as cached and code executable. Note: This memory is not used in PN TSN application - TI unit test. |
|
| R5F TCM | R5F_VECS | 0x00000000 | 0x00000040 | Cacheable: 1 Bufferable: 1 Shareable: 0 |
|
| R5F_TCMA | 0x00000040 | 0x00007FC0 | Cacheable: 1 Bufferable: 1 Shareable: 0 |
||
| R5F_TCMB0 | 0x41010000 | 0x00008000 | Cacheable: 1 Bufferable: 1 Shareable: 0 |
Best Regards