Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM
While using DFU boot on SK-TDA4VM the dfu device disappear after flashing tisp.bin.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In order to make the DFU to work on SK-TDA4VM, we need to set the usb mode as peripheral instead of host.
USB0 is connected to the TYPEC interface so we need to make dr_mode as peripheral in the USB0 node.


we need to make the below changes in the dtsi and need to recompile the U-BOOT
diff --git a/arch/arm/dts/k3-j721e-sk-u-boot.dtsi b/arch/arm/dts/k3-j721e-sk-u-boot.dtsi
index 9731094a..024a5987 100644
--- a/arch/arm/dts/k3-j721e-sk-u-boot.dtsi
+++ b/arch/arm/dts/k3-j721e-sk-u-boot.dtsi
@@ -143,7 +143,7 @@
};
&usb0 {
- dr_mode = "host";
+ dr_mode = "peripheral";
bootph-pre-ram;
};
Regards
Diwakar