Part Number: TDA4VH-Q1
Tool/software:
In the SBL bootflow, using BootApp, how to print ATF logs on MCU_UART or WKUP_UART?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VH-Q1
Tool/software:
In the SBL bootflow, using BootApp, how to print ATF logs on MCU_UART or WKUP_UART?
Initially, you would create the binaries required for BootApp referring the below steps "Booting Linux via MMCSD"
If you are loading vision_apps binaries, then you could refer the below FAQ instead
On the EVM, you would see the logs of SBL on MCU_UART 0 and ATF, OPTEE and Linux logs on Main UART 8
Any change in the custom board UART would require a rebuild of the firmwares with the specific UART port
This FAQ focused on changing the UART instance to MCU_UART for ATF
Step 1: Change the K3_USART_BASE and K3_USART_CLK_SPEED in ${PSDKLA}/board-support/trusted-firmware-a-2.10+git/plat/ti/k3/include/platform_def.h
For mcu uart, it would be K3_USART_BASE 0x40a00000 and K3_USART_CLK_SPEED 96000000
Step 2: Rebuild the ATF firmware using the below command removing optee
make CROSS_COMPILE="${PSDKLA}/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/aarch64-oe-linux/aarch64-oe-linux-" ARCH=aarch64 PLAT=k3 TARGET_BOARD=j784s4
Step 3: Copy the generated b31.bin to ${PSDKLA}/board-support/prebuilt-images
Step 4: Replace the below file "atf_optee.lds" in ${PSDKRA}/mcusw/mcuss_demos/boot_app_mcu_rtos/main_domain_apps/scripts/hlos/linux/atf_optee.lds
/cfs-file/__key/communityserver-discussions-components-files/791/atf_5F00_optee.lds
Step 5: Follow the "Steps to generate Linux related images" in the below FAQ
Step 6: Replace the generated atf_optee.appimage in the SD Card and boot the same.
Now the ATF logs would be seen on the MCU_UART
Regards,
Nikhil