Part Number: TDA4VL-Q1
I would like to turn off DebugSS, but TISCI API is not turning this off. How can I turn this subsystem off?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VL-Q1
I would like to turn off DebugSS, but TISCI API is not turning this off. How can I turn this subsystem off?
Below is a series of Linux commands for register writes as a proof-of-concept, which should be translatable to other OS. User can attempt to connect JTAG to confirm if JTAG is not accessible after the register writes.
#set next state in MDCTL register to Disable for LPSC_DEBUG2DMSC devmem2 0x42000a08 w 0x80000102 #set PTCMD to GO devmem2 0x42000120 w 0xFFFFFFFF #[optional] check state. Least significant hex value should be 0x2 devmem2 0x42000808 #set next state in MDCTL register to Disable for LPSC_main_debug devmem2 0x00400a34 w 0x80000102 #set psc_PTCMD_j to GO and reflect MDCTL change devmem2 0x00400120 w 0xFFFFFFFF #[optional] check state. Least significant hex value should be 0x2 devmem2 0x00400834 #[optional] See if DEBUGSS is active. 0x1 is active, 0x0 is non-active. Expectation is 0x0 after register writes were done devmem2 0x43014300
For some context, there is no device ID associated with LPSC_DEBUG2DMSC and LPSC_main_debug. Hence reads through the TISCI API (Sciclient_pmGetModuleState) does not actually give the status of the DebugSS as the TISCI API tracks power state associated to device ID.
Regards,
Takuma