Part Number: TIDA-00961 Other Parts Discussed in Thread: TMS320F280049 What are the benefits of using TMS320F280049 in the implementation of high density power solutions using GaN?
Part Number: TIDA-01599 Other Parts Discussed in Thread: TPS27S100 , What are the benefits of using TPS27S100 (Single-Channel High-Side Switch) in the implementation of safe torque off functionality in Variable Speed Drives?
Part Number: TIDA-01599 Other Parts Discussed in Thread: ISO1212 , What are the benefits of using ISO1212 (Isolated 24-V to 60-V Digital Input Receiver) in the implementation of safe torque off functionality in Variable Speed Drives?
Part Number: TPS650250 Other Parts Discussed in Thread: TPS54340-Q1 ,
Hi team,
Could you give me advise on following customer request? What document or material should the customer refer to?
<Customer request>
Could you tell me how to estimate…
Part Number: TPS2372
Hello,
I'm understand the concept of demotion but I don't understand the Table 3 on the datasheet for TPS2372. On page 16 we can see Table 3. It states that a PSE type 3-4 can just allocate 12.95w on a type 4-8 PD. If a Type…
Need to update your time zone for your TI E2E Community account?
Browse to "Settings" ( as shown below )
Found in the drop-down clicking on your E2E avatar in the top right
Visit your "Settings" directly here ( when already signed in )
…
Other Parts Discussed in Thread: SN74LVC1G34 , SN74LVC1G79 FAQ: Logic and Voltage Translation > Timing Parameters >> Current FAQ
** NOTE **
This FAQ is in reference to push-pull output devices. Open-drain outputs will
inherently have slower operating…
Part Number: IWR1443
Hello,
I am Yin.
The website can only see the SDk vesion 2.1.0.4,That is only for IWR1443 ES 3.0. But It seems that my EVM is ES2.0.
I wonder if there any way to let the SDk 2.1.0.4 could match my EVM? I found that there few…
FAQ: Logic and Voltage Translation > Output Parameters >> Current FAQ
There are circumstances where you might want to know a VOH or VOL Value that is not given. I will describe two cases:
If you want VOH for a supply voltage that is not given (for…