Part Number: AM2434
The tables below highlight the working configurations of custom OSPI and QSPI serial NOR/NAND Flash Parts
Note: After using the values for the Flash part present in the below tables, run the OSPI Flash IO example to verify if Flash…
Part Number: AM2434 Other Parts Discussed in Thread: UNIFLASH , SYSCONFIG
uart_uniflash.py allows to flash binaries to the flash on a EVM. UART is used as the transport or interface to send the file to flash to the EVM. When the uart_uniflash.py script…
Part Number: AM2434
Facing issues while running the loadJSFile command from the CCS scripting console.
Please refer image below.
I am using the CCS v20.4.0.
Part Number: AM62P-Q1 Other Parts Discussed in Thread: AM62P
Hi Team,
we need to use PWM channels but i’d like to ask, are we able to set the ePWM period to 1 second in AM62P?
I noticed that the PWM input clock is 250 MHz. Is this adjustable? I…
Part Number: AM6441
While running the default Sciclient CCS Init binary on the AM6441 SOC, below error is coming.
[MAIN_Cortex_R5_0_0] DMSC Firmware Version 11.0.6--v11.00.06 (Fancy Rat) DMSC Firmware revision 0xb DMSC ABI revision 4.0
[SCICLIENT…
Part Number: AM2434
To enable Quad operations when using QSPI Flash, a QE bit has to be set from the OSPI Controller. Different flash parts have different QE bit configurations.
Part Number: TDA4VH-Q1
UFS 2.1 devices are growing more difficult to purchase, as UFS 2.1 was implemented in 2016.
I have a UFS 3.0+ device, and I would like to replace the UFS 2.1 device in my design. How do I go about doing that? Are there any changes…
Part Number: AM6442 Other Parts Discussed in Thread: TMDS64EVM
AM64x boot ROM supports booting from parallel GPMC-NAND. From "4.4.10 GPMC NAND Boot" in AM64x TRM "AM64x ROM only supports boot from ONFI 1.0 compatible 8 bit parallel NAND memory up to…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: UNIFLASH , AUDIO-AM275-EVM
The ENETFOTA example demonstrates how Ethernet can be used to transfer a new application image from a host PC to an AM275x device that is currently running an older application…