Part Number: TLV320AIC3254
Hi Team,
I used the tlv320aic3254evm-m evaluation board to test it. During the test, I burned the internal program. Then I couldn't identify the evaluation board. I didn't know what happened after a long day of tossing.…
I would like an easy way to be sure that my Power over Ethernet (PoE) equipment is inter-operable. I want to avoid the potential issues outlined in the TI blog linked here -->
Part Number: OPT3101 For the following questions please refer to the answer below.
What is the measurement accuracy?
How long can you measure from the shortest to the longest?
Is output accuracy different depending on the distance?
Is output…
Hello
UCD90xxx Sequencer Training portal is online. please go to below link to learn how to use Fusion Digital Power Designer Tool to configure.
https://training.ti.com/fusion-digital-power-designer
Regards
Yihe
Part Number: TPS2372
Hi Team,
Customer want to see the specification of 802.3bt. since we already had the bt ready chips, Can you please support this document. thanks.
FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ
This question is really about the input structure of a logic device.
There are primarily two types of CMOS input structures - one with a positive clamping diode, and one without…
FAQ: Logic and Voltage Translation > Power and Thermals >> Current FAQ
Some datasheets do not specify what should be done with the thermal pad, such as in the image below:
The thermal pad is recommended to be soldered to the PCB and electrically…
Other Parts Discussed in Thread: TL431 , TL431LI Frequently Asked Questions
1. Oscillation on A/TL431, TLV/H431, A/TL431LI
One common question always regards oscillation and stability of '431 like devices. The architecture of the TL431 was designed…