Part Number: F29H859TU-Q1 Other Parts Discussed in Thread: SYSCONFIG
The multi-core project can run normally in HS-FS device, the CPU3 can be boot successfully.
But now if I run the multi-core project in HS-SE device, the CPU3 can't boot, CPU1 will…
Part Number: AM62A7
I am using AM6x or TDA4x family of devices. The TRM interrupt table shows a different interrupt number than whats provided in the device tree for my device. Why is that the case?
Part Number: AM2754-Q1 Other Parts Discussed in Thread: AM62P , SYSCONFIG , AUDIO-AM275-EVM
Sitara Audio: Where can I find audio software debugging guides and example codes for McASP and audio applications, apart from what is included in the MCU+ SDK…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG
AM275x: How to use 32-bit audio on McASP with the AASRC , which supports only up to 24-bit samples?
The default aasrc_multichannel_playback example of the AM275x SDK is configured for…
Part Number: AM2754-Q1
How to handle loss and recovery of an external McASP clock (for example A2B) when the McASP Rx feeds an AASRC, without a DSP reset?
In my system one McASP receives audio on an external clock (for example from an A2B transceiver…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG
How to detect McASP external clock (frame sync) loss and recovery using eCAP? My McASP runs as a slave on an external frame sync and bit clock, and the external source can go away and…
Part Number: AM2754-Q1 Other Parts Discussed in Thread: SYSCONFIG
How to build an AASRC application with only 2 buffers in ping-pong style and add audio processing to it?
The aasrc_multichannel_playback example in the AM275x FreeRTOS SDK allocates…
Part Number: AWR2944 Other Parts Discussed in Thread: SYSCONFIG
Where to get a list of the supported flash variants by mmwaveradar devices
You can refer to the following flash application note
Flash Variants Supported by the mmWave Sensor (Rev…