Part Number: TDA4VM-Q1 Tool/software: On custom boards where UART instances are limited, how can I route debug output from my application running in one domain to a UART instance available in different domain? Specially, I want to enable cross-domain…
Part Number: EDGE-AI-STUDIO
Tool/software:
Model importing in TI has two sets of tools due to historical reasons. These two sets has developed in parallel for a long time. Here is an explanation of the similarity and difference of the two tools. …
FAQ: Isolation >> Electromagnetic Compatibility
Digital Isolators
Isolated Interfaces
Signal Isolators
with Integrated
Power
Opto-Emulators
Electromagnetic
Compatibility
Part Recommendations
and Technical Training…
Part Number: AUDIO-AM62D-EVM Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
1. While configuring McASP through sysConfig, I found that when the num of slots set as 2, the active slot bitmask can only below 3. What is this active slot bitmask…
Part Number: AUDIO-AM275-EVM
Tool/software:
I am not able to return from infinity loop in C7x core by changing the loop variable from the Variables tab in CCS. In the following code - void loop_forever()
{
volatile uint32_t loop = 1U;
while(loop…
Part Number: BQ24800EVM Other Parts Discussed in Thread: BQ24800
Tool/software:
The quiescent current stated on the BQ24800 data sheet applies only to the IC itself and not the EVM. Other components on the EVM board can also draw small amounts of…