Part Number: TLV320AIC3262
Dear Sir:
Our system block diagram as below picture , If we want to mix 2 I2S input signal from HDMI RX and through I2S output , We have 2 question as below:
1.If same sample rate , can I used MUX to switch either one…
This thread contains E2E search tips and tricks. This should help users take better advantage of the capabilities that are available in the E2E Search feature.
Part Number: TPS65311-Q1
Hi,
When 5V is supplied to EXTSUP pin, how the VREG FET does operate(as regulator or Power SW)?
I would like to know if "VREGDROP(=200mV[max])" is I*R drop.
Best Regards,
Kuramochi
Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models
Some of the LDO models that were recently released work fine in PSpice, but give a missing subcircuit warning when imported into other tools. How do I fix this?
Other Parts Discussed in Thread: TPS53647 , TPS53667 , TPS53681 , TPS53622 , TPS53659 , TPS53679 Q1: How to properly turn off phases if you don’t need the max phase number?
Pull the appropriate CSP line up to the controller supply voltage V3R3 to select…
Part Number: TPS51200
General Questions:
Q: What types of DDR does TPS51200 support?
A: TPS51200 supports DDR, DDR2, DDR3, DDR3L, LP DDR3 (Low power DDR3) and DDR4.
Q: How to calculate the power dissipation on TPS51200.
A: TPS51200 is a linear…
Part Number: TPS51206
General Questions:
Q: What types of DDR does TPS51206 support?
A: TPS51206 supports DDR2, DDR3, DDR3L, LP DDR3 (Low power DDR3) and DDR4.
Q: How to calculate the power dissipation on TPS51206.
A: TPS51206 is a linear…
Part Number: LAUNCHXL-F28069M
The XDS100 USB Serial Port on some LAUNCHXL-F28069M boards may not be configured correctly. A symptom of this condition is that the USB Serial Port will not be identified by Windows. Below is a snapshot of an XDS100 USB…
Part Number: DLP2000
Hello DLP® LightCrafter™ Display 2000 users!
We have recently pushed a new code update to the BeagleBone Black Debian distribution for this EVM. This update provides some reference code and a program to enable structured light…