Texas Instruments (TI) MSP low-power microcontrollers support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search MSP low-power microcontroller content or ask technical support questions on value line, capacitive sensing, ultrasonic & performance sensing MCUs, as well as other MSP430™ MCUs. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Part Number: MSPM33-SDK
1.Import empty example from SDK as a customer’s project.
2.Build project. Copy the 4 files which Sysconfig created to customer’s project.
3.Copy below files from SDK to the customer’s project. Recommend following the…
Part Number: MSPM0G3507
mcan_application_LP_MSPM0G3507_nortos_ticlang_20260408.zip
mcan_application_LP_MSPM0G3507_nortos_ticlang_20261020.zip
Release note: Add Tx Event FIFO handling, Add unified buffer/fifo API
Here is the mcan application…
Part Number: MSPM0-SDK
This thread is used to update the software or hardware update for application note of Low cost AC motor control solution based on MSPM0 and Triac.
5466.Resource_HW&FW.zip
TI is pleased to announce a new TI Arm Clang Compiler Tools release 3.2.0.LTS which includes the following new features.
New features:
Support for ELF Segment "Blocking" (Alignment and Padding)
Support for OpTI-Flash Smart Placement
Support…
Other Parts Discussed in Thread: MSPM0L1306 Automatically set the LOAD_VALUE into TIMx.CTR via TIMx.CCCTL.LCOND is not work for period capture. It will have influence on "Period Capture" mode and "Combined Pulse Width and Period Time" mode. (Only use…
Other Parts Discussed in Thread: MSPM0L1306 The timeout function on MSPM0G or MSPM0L UART can't reach ms level.
Here is an example to realize it based on 1 UART, 1 Timer, 2 DMA.
Here is the blockdiagram. The key point is that it doesn't use UART R…
Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH , MSPM0-SDK
Important note for early MSPM0 customers
TI recently launched a new family of Arm Cortex-M0+ MCUs , including the MSPM0L series and MSPM0G series . These MCUs are accompanied by a…
Part Number: MSP-EXP430F5529LP Other Parts Discussed in Thread: MSP430F5529 , UNIFLASH , ENERGIA , MSP-FET , MSP-FLASHER , MSP430F5528
Hi everybody,
I have a new MSP-EXP430F5529LP board, but I can't get it to work. Connecting the EVM to the PC via…
Part Number: CCSTUDIO-MSP Other Parts Discussed in Thread: UNIFLASH
By default, CCS will detect the JTAG interface automatically based on the device and the debugger. However, you may want to manually change the interface type to 2-wire SBW or 4-wire…