Part Number: EVM430-FR6047
Tool/software:
Dear Experts
I recently purchased a new EVM430-FR6047. When I click the "Request Update" button to update the parameters using the Ultrasonic Sensing Design Center (Water Mode), the following error message is displayed.

However, when I reconnect the Ultrasonic Sensing Design Center (Water Mode) to the previously purchased evaluation board, the parameter update works fine. Additionally, although the parameter update cannot be performed, flow measurement is still possible.
Is there any setting required, or is a firmware update needed for the evaluation board or the Ultrasonic Sensing Design Center?