Part Number: TPS65070
I'm using the TPS65070 as Power-Manager of an IIoT-System. As power-supply I use LiPo or/and AC. After booting the TSP EN_DCDC1 is high and in the CON_CTRL1-Register there is the default setting “01111111” This means after pulling…
Part Number: ADS1282
Hi all,
For unipolar mode (AVDD=5V, AVSS=0V, VREFP=5V, VREFN=0V), ADS1282 full-scale input voltage is from 0V to 2.5V. Am i right?
Also data code is range from 00000000h to 7FFFFFFFh for FIR filter. Am i right?
Most of…
Part Number: TIDM-THREEPHASEMETER-F6779 Other Parts Discussed in Thread: MSP430F6779
With Reference to the reference design:
SLAA577G–January 2013–Revised August 2015 Implementation of a Three-Phase Electronic Watt-Hour Meter Using the MSP430F677x…
Part Number: MSP430F5528
Hi,
Can someone clarify what temperature range the TLV ADC gain and offset parameters were intended for? Were these TLV parameters optimized from -40C to 85C or
at room temperature only?
-Kelvin
Dear MSP community,
The complexity of applications is increasing, and the integration of functions on a single chip is also increasing. Therefore it is natural that dedicated functions sometimes do not work as a developer expects.
In such cases…
Part Number: BOOSTXL-DRV8323RS BOOSTXL-DRV8323RH Other Parts Discussed in Thread: DRV832X , MOTORWARE , LAUNCHXL-F28027F , , LAUNCHXL-F28069M , BOOSTXL-DRV8323RH
We are not planning to revise MotorWare from the current v18. However, many of our customers…
Part Number: DLPLIGHTCRAFTER
Getting the DLP® LightCrafter™ EVM to work with Windows 10
In order for the DLP LightCrafter EVM to work with Windows 10 the default driver needs to be replaced. Below is one driver that can be used for successful operation…
Part Number: DLPDLCR2000EVM
All,
We would like to present a brief tutorial on how to get your DLP® LightCrafter™ Display 2000 EVM up and running on a BeagleBone Black. This tutorial will assume limited Linux/Debian experience. For more general information…
Part Number: DLPDLCR2000EVM
All,
We would like to present a straightforward modification to the DLPDLCR2000EVM’s optical engine that will result in a focus lever that is more resistant to adjustment. To implement this you will need:
1x Steel Phillips…
Other Parts Discussed in Thread: C2000WARE Question: Where can I find information to get started with software? Where are the peripheral examples, Math, DSP, or DigitalPower examples?